You are viewing documentation for version:3.0.12Public Attributes#uint8_tname_lenName length. int8_tnameArray which consists name of the local device. Public Attribute Documentation#name_len#uint8_t rsi_bt_resp_get_local_name_s::name_lenName length. name#int8_t rsi_bt_resp_get_local_name_s::name[RSI_DEV_NAME_LEN]Array which consists name of the local device. The maximum size of this array is 50