Public Attributes#
maxtxoctets Preferred maximum number of payload octets that the local Controller should include in a single Link Layer packet on this connection.
maxtxtime Preferred maximum number of microseconds that the local Controller should use to transmit a single Link Layer packet on this connection
maxrxoctets Maximum number of payload octets that the local Controller supports for reception of a single Link Layer packet on a data connection
maxrxtime Maximum time, in microseconds, that the local Controller supports for reception of a single Link Layer packet on a data connection.
Public Attribute Documentation#
maxtxoctets#
uint16_t rsi_ble_resp_read_max_data_length_s::maxtxoctets
maxtxoctets Preferred maximum number of payload octets that the local Controller should include in a single Link Layer packet on this connection.
892
of file components/si91x/ble/inc/rsi_ble_apis.h
maxtxtime#
uint16_t rsi_ble_resp_read_max_data_length_s::maxtxtime
maxtxtime Preferred maximum number of microseconds that the local Controller should use to transmit a single Link Layer packet on this connection
896
of file components/si91x/ble/inc/rsi_ble_apis.h
maxrxoctets#
uint16_t rsi_ble_resp_read_max_data_length_s::maxrxoctets
maxrxoctets Maximum number of payload octets that the local Controller supports for reception of a single Link Layer packet on a data connection
900
of file components/si91x/ble/inc/rsi_ble_apis.h
maxrxtime#
uint16_t rsi_ble_resp_read_max_data_length_s::maxrxtime
maxrxtime Maximum time, in microseconds, that the local Controller supports for reception of a single Link Layer packet on a data connection.
904
of file components/si91x/ble/inc/rsi_ble_apis.h