Public Attributes#
Remote device Bluetooth Address.
TX PHY Rate 0x01 The transmitter PHY for the connection is LE 1M 0x02 The transmitter PHY for the connection is LE 2M 0x03 The transmitter PHY for the connection is LE Coded All other values Reserved for future use.
RX PHY Rate 0x01 The receiver PHY for the connection is LE 1M 0x02 The receiver PHY for the connection is LE 2M 0x03 The receiver PHY for the connection is LE Coded All other values Reserved for future use.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_resp_read_phy_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device Bluetooth Address.
872
of file components/si91x/ble/inc/rsi_ble_apis.h
tx_phy#
uint8_t rsi_ble_resp_read_phy_s::tx_phy
TX PHY Rate 0x01 The transmitter PHY for the connection is LE 1M 0x02 The transmitter PHY for the connection is LE 2M 0x03 The transmitter PHY for the connection is LE Coded All other values Reserved for future use.
878
of file components/si91x/ble/inc/rsi_ble_apis.h
rx_phy#
uint8_t rsi_ble_resp_read_phy_s::rx_phy
RX PHY Rate 0x01 The receiver PHY for the connection is LE 1M 0x02 The receiver PHY for the connection is LE 2M 0x03 The receiver PHY for the connection is LE Coded All other values Reserved for future use.
884
of file components/si91x/ble/inc/rsi_ble_apis.h