Wi-Fi performance profile.
Public Attributes#
Performance profile.
uint8_t
Set DTIM alignment required. si91x_dtim_alignment_types.
uint8_t
Default value to be used is 0.
uint16_t
Listen interval.
sl_wifi_twt_request_t
twt request.
Public Attribute Documentation#
profile#
sl_performance_profile_t sl_wifi_performance_profile_t::profile
Performance profile.
Definition at line
943
of file components/si91x/inc/sl_wifi_device.h
dtim_aligned_type#
uint8_t sl_wifi_performance_profile_t::dtim_aligned_type
Set DTIM alignment required. si91x_dtim_alignment_types.
Definition at line
944
of file components/si91x/inc/sl_wifi_device.h
num_of_dtim_skip#
uint8_t sl_wifi_performance_profile_t::num_of_dtim_skip
Default value to be used is 0.
Definition at line
945
of file components/si91x/inc/sl_wifi_device.h
listen_interval#
uint16_t sl_wifi_performance_profile_t::listen_interval
Listen interval.
Definition at line
946
of file components/si91x/inc/sl_wifi_device.h
twt_request#
sl_wifi_twt_request_t sl_wifi_performance_profile_t::twt_request
twt request.
Definition at line
947
of file components/si91x/inc/sl_wifi_device.h