Wi-Fi Access Point configuration.

Public Attributes#

Optional flags for AP configuration.

ID of secure credentials.

uint8_t

Keep alive type of the access point.

uint16_t

Beacon interval of the access point in milliseconds.

uint32_t

Duration in milliseconds to kick idle client.

uint16_t

How many beacons per DTIM.

uint8_t

Maximum number of associated clients.

Public Attribute Documentation#

ssid#

sl_wifi_ssid_t sl_wifi_ap_configuration_t::ssid

SSID.


Definition at line 91 of file components/protocol/wifi/inc/sl_wifi_types.h

security#

sl_wifi_security_t sl_wifi_ap_configuration_t::security

Security mode.


Definition at line 92 of file components/protocol/wifi/inc/sl_wifi_types.h

encryption#

sl_wifi_encryption_t sl_wifi_ap_configuration_t::encryption

Encryption mode.


Definition at line 93 of file components/protocol/wifi/inc/sl_wifi_types.h

channel#

sl_wifi_channel_t sl_wifi_ap_configuration_t::channel

Channel.


Definition at line 94 of file components/protocol/wifi/inc/sl_wifi_types.h

rate_protocol#

sl_wifi_rate_protocol_t sl_wifi_ap_configuration_t::rate_protocol

Rate protocol.


Definition at line 95 of file components/protocol/wifi/inc/sl_wifi_types.h

options#

sl_wifi_ap_flag_t sl_wifi_ap_configuration_t::options

Optional flags for AP configuration.


Definition at line 96 of file components/protocol/wifi/inc/sl_wifi_types.h

credential_id#

sl_wifi_credential_id_t sl_wifi_ap_configuration_t::credential_id

ID of secure credentials.


Definition at line 97 of file components/protocol/wifi/inc/sl_wifi_types.h

keepalive_type#

uint8_t sl_wifi_ap_configuration_t::keepalive_type

Keep alive type of the access point.


Definition at line 98 of file components/protocol/wifi/inc/sl_wifi_types.h

beacon_interval#

uint16_t sl_wifi_ap_configuration_t::beacon_interval

Beacon interval of the access point in milliseconds.


Definition at line 99 of file components/protocol/wifi/inc/sl_wifi_types.h

client_idle_timeout#

uint32_t sl_wifi_ap_configuration_t::client_idle_timeout

Duration in milliseconds to kick idle client.


Definition at line 100 of file components/protocol/wifi/inc/sl_wifi_types.h

dtim_beacon_count#

uint16_t sl_wifi_ap_configuration_t::dtim_beacon_count

How many beacons per DTIM.


Definition at line 101 of file components/protocol/wifi/inc/sl_wifi_types.h

maximum_clients#

uint8_t sl_wifi_ap_configuration_t::maximum_clients

Maximum number of associated clients.


Definition at line 102 of file components/protocol/wifi/inc/sl_wifi_types.h