uint16_t beacon_interval parameter in rsi_wlan_ap_start()
| uint16_t sl_wifi_ap_configuration_t :: beacon_interval
| API parameter in v2.x API is mapped to struct member in v3.x. |
uint8_t rsi_opermode_t :: ble_ext_feature_bit_map[4]
| uint32_t sl_si91x_boot_configuration_t :: ble_ext_feature_bit_map
| |
uint8_t rsi_opermode_t :: ble_feature_bit_map[4]
| uint32_t sl_si91x_boot_configuration_t :: ble_feature_bit_map
| |
uint16_t coex_mode parameter in rsi_wireless_init()
| uint16_t sl_si91x_boot_configuration_t :: coex_mode
| API parameter in v2.x API is mapped to struct member in v3.x. |
uint8_t channel parameter in rsi_wlan_ap_start()
| sl_wifi_channel_t sl_wifi_ap_configuration_t :: channel
| API parameter in v2.x API is mapped to struct member in v3.x. |
uint8_t rsi_opermode_t :: config_feature_bit_map[4]
| uint32_t sl_si91x_boot_configuration_t :: config_feature_bit_map
| |
uint8_t dtim_period parameter in rsi_wlan_ap_start()
| uint16_t sl_wifi_ap_configuration_t :: dtim_beacon_count
| API parameter in v2.x API is mapped to struct member in v3.x. |
rsi_encryption_mode_t encryption_mode parameter in rsi_wlan_ap_start()
| sl_wifi_encryption_t sl_wifi_ap_configuration_t :: encryption
| API parameter in v2.x API is mapped to struct member in v3.x. |
uint8_t twt_user_params_t :: implicit_twt
| uint8_t sl_wifi_twt_request_t :: implicit_twt
| |
uint8_t *ip_addr, uint8_t *mask, uint8_t *gw parameters in rsi_config_ipaddress()
| union { sl_net_ipv4_setting_t v4; sl_net_ipv6_setting_t v6; } sl_net_ip_configuration_t :: ip
| All three v2.x function parameters are set in v3.x using a struct member. |
uint8_t mode parameter in rsi_config_ipaddress()
| sl_ip_management_t sl_net_ip_configuration_t :: mode
| API parameter in v2.x API is mapped to struct member in v3.x. |
uint16_t oper_mode parameter in rsi_wireless_init()
| uint16_t sl_si91x_boot_configuration_t :: oper_mode
| API parameter in v2.x API is mapped to struct member in v3.x. |
uint8_t rsi_eap_credentials_t :: password[128]
| uint8_t sl_wifi_eap_credential_t :: password[SL_EAP_PASSWORD_LENGTH]
| |
uint8_t twt_user_params_t :: restrict_tx_outside_tsp
| uint8_t sl_wifi_twt_request_t :: restrict_tx_outside_tsp
| |
uint8_t twt_user_params_t :: req_type
| uint8_t sl_wifi_twt_request_t :: req_type
| |
RSI_CUSTOM_FEATURE_BIT_MAP
| uint32_t sl_si91x_boot_configuration_t :: custom_feature_bit_map
| Macro in v2.x API is mapped to struct member in v3.x. |
RSI_EXT_CUSTOM_FEATURE_BIT_MAP
| uint32_t sl_si91x_boot_configuration_t :: ext_custom_feature_bit_map
| Macro in v2.x API is mapped to struct member in v3.x. |
RSI_EXT_TCPIP_FEATURE_BITMAP
| uint32_t sl_si91x_boot_configuration_t :: ext_tcp_ip_feature_bit_map
| Macro in v2.x API is mapped to struct member in v3.x. |
RSI_FEATURE_BIT_MAP
| uint32_t sl_si91x_boot_configuration_t :: feature_bit_map
| Macro in v2.x API is mapped to struct member in v3.x. |
RSI_TCP_IP_FEATURE_BIT_MAP
| uint32_t sl_si91x_boot_configuration_t :: tcp_ip_feature_bit_map
| Macro in v2.x API is mapped to struct member in v3.x. |
rsi_security_mode_t sec_type parameter in rsi_wla_connect()
| sl_wifi_security_t sl_wifi_client_configuration_t :: security
| API parameter in v2.x API is mapped to struct member in v3.x. |
int8_t *ssid parameter in rsi_wlan_connect()
| sl_wifi_ssid_t sl_wifi_client_configuration_t :: ssid
| API parameter in v2.x API is mapped to struct member in v3.x. |
uint8_t twt_user_params_t :: triggered_twt
| uint8_t sl_wifi_twt_request_t :: triggered_twt
| |
uint8_t twt_user_params_t :: twt_channel
| uint8_t sl_wifi_twt_request_t :: twt_channel
| |
uint8_t twt_enable parameter in rsi_wlan_twt_config()
| uint8_t sl_wifi_twt_request_t :: twt_enable
| API parameter in v2.x API is mapped to struct member in v3.x. |
uint8_t twt_flow_id parameter in rsi_wlan_twt_config()
| uint8_t sl_wifi_twt_request_t :: twt_flow_id
| API parameter in v2.x API is mapped to struct member in v3.x. |
uint8_t twt_user_params_t :: twt_retry_limit
| uint8_t sl_wifi_twt_request_t :: twt_retry_limit
| |
uint8_t twt_user_params_t :: twt_retry_interval
| uint8_t sl_wifi_twt_request_t :: twt_retry_interval
| |
uint8_t twt_user_params_t :: twt_protection
| uint8_t sl_wifi_twt_request_t :: twt_protection
| |
uint8_t twt_user_params_t :: un_announced_twt
| uint8_t sl_wifi_twt_request_t :: un_announced_twt
| |
uint8_t rsi_eap_credentials_t :: username[64]
| uint8_t sl_wifi_eap_credential_t :: username[SL_EAP_USER_NAME_LENGTH]
| |
rsi_ip_version_t version parameter in rsi_config_ipaddress()
| sl_ip_address_type_t sl_net_ip_configuration_t :: type
| API parameter in v2.x API is mapped to struct member in v3.x. |
uint8_t twt_user_params_t :: wake_duration
| uint8_t sl_wifi_twt_request_t :: wake_duration
| |
uint8_t twt_user_params_t :: wake_duration_tol
| uint8_t sl_wifi_twt_request_t :: wake_duration_tol
| |
uint8_t twt_user_params_t :: wake_duration_unit
| uint8_t sl_wifi_twt_request_t :: wake_duration_unit
| |
uint8_t twt_user_params_t :: wake_int_exp
| uint8_t sl_wifi_twt_request_t :: wake_int_exp
| |
uint8_t twt_user_params_t :: wake_int_exp_tol
| uint8_t sl_wifi_twt_request_t :: wake_int_exp_tol
| |
uint16_t twt_user_params_t :: wake_int_mantissa
| uint16_t sl_wifi_twt_request_t :: wake_int_mantissa
| |
uint16_t twt_user_params_t :: wake_int_mantissa_tol
| uint16_t sl_wifi_twt_request_t :: wake_int_mantissa_tol
| |