Modules#
sl_mqtt_client_last_will_message_t
sl_mqtt_client_configuration_t
sl_mqtt_client_topic_subscription_info_t
Types#
This section provides a reference to the MQTT API data types.
Typedefs#
Handler for MQTT client Events.
Handler for MQTT client RX message.
Typedef Documentation#
sl_mqtt_client_event_handler#
typedef void(* sl_mqtt_client_event_handler) (void *client, sl_mqtt_client_event_t event, void *event_data, void *context) )(void *client, sl_mqtt_client_event_t event, void *event_data, void *context)
Handler for MQTT client Events.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [out] | client | Client on which the event occurred. | |
| [out] | event | Event occurred. | |
| [out] | event_data | Event data for the data. This parameter would be non-null only for MQTT_CLIENT_MESSAGED_RECEIVED and MQTT_CLIENT_ERROR. | |
| [out] | context | Context provided by user at the time of API call. The caller must ensure that the lifecycle of the context is retained until the callback is invoked. The deallocation of context is also the responsibility of the caller. |
sl_mqtt_client_message_received#
typedef void(* sl_mqtt_client_message_received) (void *client, sl_mqtt_client_message_t *message_to_be_published, void *context) )(void *client, sl_mqtt_client_message_t *message_to_be_published, void *context)
Handler for MQTT client RX message.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [out] | client | Client which has received message. | |
| [out] | message | Message received. | |
| [out] | context | Context provided by user at the time of Subscribe API call. The caller must ensure that the lifecycle of the context is retained until the callback is invoked. The deallocation of context is also the responsibility of the caller. |
Note
Due to the constraints from the firmware, is_retained, qos_level, packet_identifer, duplicate_message of sl_mqtt_client_message_t are not populated and shall be ignored while processing the message.