Performance Management#
Functions#
Set Wi-Fi performance profile.
Get Wi-Fi performance profile.
Function Documentation#
sl_wifi_set_performance_profile#
sl_status_t sl_wifi_set_performance_profile (const sl_wifi_performance_profile_t * profile)
Set Wi-Fi performance profile.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_wifi_performance_profile_t * | [in] | profile | Wi-Fi performance profile as indicated by sl_wifi_performance_profile_t |
sl_wifi_init should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.
Note
For SI91x chips Enhanced MAX PSP is supported when profile is set to ASSOCIATED_POWER_SAVE_LOW_LATENCY and SL_SI91X_ENABLE_ENHANCED_MAX_PSP bit is enabled in config feature bitmap
sl_wifi_get_performance_profile#
sl_status_t sl_wifi_get_performance_profile (sl_wifi_performance_profile_t * profile)
Get Wi-Fi performance profile.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_wifi_performance_profile_t * | [out] | profile | Wi-Fi performance profile as indicated by sl_wifi_performance_profile_t |
sl_wifi_init should be called before this API.
Returns
sl_status_t. See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.