Public Attributes#

uint8_t

Command ID Takes per BLE_RECEIVE_CMD_ID of value 0x14.

uint8_t

Enables/disables the ble per receive mode 1 PER Receive Enable 0 PER Receive Disable.

uint8_t

Access address with which packets are received.

uint8_t

Phy rate at which packets are received 1 1Mbps 2 2 Mbps 4 125 Kbps Coded 8 500 Kbps Coded.

uint8_t

Rx channel number (0 - 39)

uint8_t

Tx channel number (0 - 39)

uint8_t

Initial seed to be used for whitening.

uint8_t

LE channel type (data or advertise channel) 0x00 Advertise Channel 0x01 Data Channel (to be used by Default)

uint8_t

Frequency hopping type to be used 0 No Hopping 1 Fixed Hopping 2 Random Hopping (rx_chnl_num, tx_chnl_num parameters are unused in this mode)

uint8_t

Select the antenna to be used.

uint8_t

pll_mode type to be used 0 PLL_MODE0 (to be used by Default) 1 PLL_MODE1

uint8_t

Selection of RF type (internal/external) 0 BT_EXTERNAL_RF 1 BT_INTERNAL_RF (to be used by Default)

uint8_t

Selection of RF Chain (HP/LP) to be used 2 BT_HP_CHAIN 3 BT_LP_CHAIN.

uint8_t

This field enables/disables the extended data length 0 Extended Data length disabled 1 Extended Data length enabled.

uint8_t

This field defines the loopback to be enable or disable 0 LOOP_BACK_MODE_DISABLE 1 LOOP_BACK_MODE_ENABLE.

uint8_t

This field enables/disables the duty cycling 0 Duty Cycling Disabled (to be used by Default) 1 Duty Cycling Enabled.

Public Attribute Documentation#

cmd_ix#

uint8_t rsi_ble_per_receive_s::cmd_ix

Command ID Takes per BLE_RECEIVE_CMD_ID of value 0x14.


receive_enable#

uint8_t rsi_ble_per_receive_s::receive_enable

Enables/disables the ble per receive mode 1 PER Receive Enable 0 PER Receive Disable.


access_addr#

uint8_t rsi_ble_per_receive_s::access_addr[4]

Access address with which packets are received.


phy_rate#

uint8_t rsi_ble_per_receive_s::phy_rate

Phy rate at which packets are received 1 1Mbps 2 2 Mbps 4 125 Kbps Coded 8 500 Kbps Coded.


rx_chnl_num#

uint8_t rsi_ble_per_receive_s::rx_chnl_num

Rx channel number (0 - 39)


tx_chnl_num#

uint8_t rsi_ble_per_receive_s::tx_chnl_num

Tx channel number (0 - 39)


scrambler_seed#

uint8_t rsi_ble_per_receive_s::scrambler_seed

Initial seed to be used for whitening.

It should be set to 0 in order to disable whitening. In order to enable, one should give the scrambler seed value which is used on the transmit side


le_chnl_type#

uint8_t rsi_ble_per_receive_s::le_chnl_type

LE channel type (data or advertise channel) 0x00 Advertise Channel 0x01 Data Channel (to be used by Default)


freq_hop_en#

uint8_t rsi_ble_per_receive_s::freq_hop_en

Frequency hopping type to be used 0 No Hopping 1 Fixed Hopping 2 Random Hopping (rx_chnl_num, tx_chnl_num parameters are unused in this mode)


ant_sel#

uint8_t rsi_ble_per_receive_s::ant_sel

Select the antenna to be used.

Refer to the datasheet for your hardware to check whether or not it contains an onboard antenna. 2 ONBOARD_ANT_SEL 3 EXT_ANT_SEL


pll_mode#

uint8_t rsi_ble_per_receive_s::pll_mode

pll_mode type to be used 0 PLL_MODE0 (to be used by Default) 1 PLL_MODE1


rf_type#

uint8_t rsi_ble_per_receive_s::rf_type

Selection of RF type (internal/external) 0 BT_EXTERNAL_RF 1 BT_INTERNAL_RF (to be used by Default)

Note

  • The above macros are applicable for both BT and BLE


rf_chain#

uint8_t rsi_ble_per_receive_s::rf_chain

Selection of RF Chain (HP/LP) to be used 2 BT_HP_CHAIN 3 BT_LP_CHAIN.

Note

  • The above macros are applicable for both BT and BLE


ext_data_len_indication#

uint8_t rsi_ble_per_receive_s::ext_data_len_indication

This field enables/disables the extended data length 0 Extended Data length disabled 1 Extended Data length enabled.


loop_back_mode#

uint8_t rsi_ble_per_receive_s::loop_back_mode

This field defines the loopback to be enable or disable 0 LOOP_BACK_MODE_DISABLE 1 LOOP_BACK_MODE_ENABLE.


duty_cycling_en#

uint8_t rsi_ble_per_receive_s::duty_cycling_en

This field enables/disables the duty cycling 0 Duty Cycling Disabled (to be used by Default) 1 Duty Cycling Enabled.