Getting Started with the WiSeConnect™ SDK v3.x#

To get started with using the WiSeConnect™ SDK v3.x, download the latest version of Simplicity Studio and select one of the getting started guides in this section:

  • System-on-chip (SoC) mode - both the application and connectivity stack run on the SiWx91x™ chipset. See the Getting Started with SoC Mode section.

  • Network co-processor (NCP) mode - application runs on external microcontroller unit (MCU) host, connectivity stack runs on the SiWx91x chipset. See the Getting Started with EFx32 in NCP Mode section.

    Note: Only EFx32 hosts are supported in NCP mode at this time.