Public Attributes#
Device input output capability 0x00 - Display Only 0x01 - Display Yes/No 0x02 - Keyboard Only 0x03 - No Input No Output 0x04 - Keyboard Display.
oob_data_flag 0 - disable 1 - enable
Authentication Request contains bonding type MITM Request - BIT(2) Secure Connections - BIT(3) Keypress - BIT(4) CT2 - BIT(5)
Supported Encryption key size 7 to 16 bytes.
Initiator generates/requires the no .of keys after successful paring BIT(0) - EncKey: Initiator distributes the LTK followed by EDIV and Rand BIT(1) - IdKey : Initiator distributes the IRK followed by its address BIT(2) - Sign : Initiator distributes the CSRK BIT(3) - BIT(7): Reserved for future use.
Responder generates/requires the no .of keys after successful paring BIT(0) - EncKey: Responder distributes the LTK followed by EDIV and Rand BIT(1) - IdKey : Responder distributes the IRK followed by its address BIT(2) - Sign : Responder distributes the CSRK BIT(3) - BIT(7): Reserved for future use.
Public Attribute Documentation#
io_capability#
uint8_t rsi_ble_set_smp_pairing_capabilty_data::io_capability
Device input output capability 0x00 - Display Only 0x01 - Display Yes/No 0x02 - Keyboard Only 0x03 - No Input No Output 0x04 - Keyboard Display.
oob_data_flag#
uint8_t rsi_ble_set_smp_pairing_capabilty_data::oob_data_flag
oob_data_flag 0 - disable 1 - enable
auth_req#
uint8_t rsi_ble_set_smp_pairing_capabilty_data::auth_req
Authentication Request contains bonding type MITM Request - BIT(2) Secure Connections - BIT(3) Keypress - BIT(4) CT2 - BIT(5)
enc_key_size#
uint8_t rsi_ble_set_smp_pairing_capabilty_data::enc_key_size
Supported Encryption key size 7 to 16 bytes.
ini_key_distribution#
uint8_t rsi_ble_set_smp_pairing_capabilty_data::ini_key_distribution
Initiator generates/requires the no .of keys after successful paring BIT(0) - EncKey: Initiator distributes the LTK followed by EDIV and Rand BIT(1) - IdKey : Initiator distributes the IRK followed by its address BIT(2) - Sign : Initiator distributes the CSRK BIT(3) - BIT(7): Reserved for future use.
rsp_key_distribution#
uint8_t rsi_ble_set_smp_pairing_capabilty_data::rsp_key_distribution
Responder generates/requires the no .of keys after successful paring BIT(0) - EncKey: Responder distributes the LTK followed by EDIV and Rand BIT(1) - IdKey : Responder distributes the IRK followed by its address BIT(2) - Sign : Responder distributes the CSRK BIT(3) - BIT(7): Reserved for future use.