Import Updated Code into Studio#

  1. When you have updated your code for WiSeConnectâ„¢ SDK v3.x, either copy it into the existing app.c file in your Simplicity Studio project or organize it into multiple source files and add them to your Simplicity Studio project.

  2. To add files to your Simplicty Studio project:

    • Open your project in Simplicity Studio.

    • Right-click on the project folder in the Project Explorer window, and select New > File.

    Project ExplorerProject Explorer

    • In the Create New File wizard, select the project folder in which you wish to add the file.

    • Click Advanced>>.

    Create New FileCreate New File

    • Select Link to fie in the file system

    • Click Browse

    • Locate and select the file you wish to add.

    • Click Finish to add the file to your project.

    Link to file in the file systemLink to file in the file system

    • The added file will appear in the project structure in your Project Explorer window.

    File added to file systemFile added to file system