Public Attributes#

uint16_t

Packet count of CRC fails (Cyclic Redundancy Check (CRC))

uint16_t

Packet count of CRC fails (Cyclic Redundancy Check (CRC))

uint16_t

Packet count of aborted Tx.

uint16_t

Packet count of dropped Rx.

uint16_t

Packet count of CCA Idle (Clear Channel Assessment (CCA))

uint16_t

Packet count of Rx start.

uint16_t

Packet count of aborted Rx.

uint16_t

Packet count of successful transmissions.

int8_t

Received Signal Strength Indicator of the packet.

uint16_t

Packet count of ID packets received.

uint16_t

Dummy array of length 5.

Public Attribute Documentation#

crc_fail_cnt#

uint16_t rsi_bt_per_stats_s::crc_fail_cnt

Packet count of CRC fails (Cyclic Redundancy Check (CRC))


Definition at line 321 of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h

crc_pass_cnt#

uint16_t rsi_bt_per_stats_s::crc_pass_cnt

Packet count of CRC fails (Cyclic Redundancy Check (CRC))


Definition at line 323 of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h

tx_abort_cnt#

uint16_t rsi_bt_per_stats_s::tx_abort_cnt

Packet count of aborted Tx.


Definition at line 325 of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h

rx_drop_cnt#

uint16_t rsi_bt_per_stats_s::rx_drop_cnt

Packet count of dropped Rx.


Definition at line 327 of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h

rx_cca_idle_cnt#

uint16_t rsi_bt_per_stats_s::rx_cca_idle_cnt

Packet count of CCA Idle (Clear Channel Assessment (CCA))


Definition at line 329 of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h

rx_start_idle_cnt#

uint16_t rsi_bt_per_stats_s::rx_start_idle_cnt

Packet count of Rx start.


Definition at line 331 of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h

rx_abrt_cnt#

uint16_t rsi_bt_per_stats_s::rx_abrt_cnt

Packet count of aborted Rx.


Definition at line 333 of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h

tx_dones#

uint16_t rsi_bt_per_stats_s::tx_dones

Packet count of successful transmissions.


Definition at line 335 of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h

rssi#

int8_t rsi_bt_per_stats_s::rssi

Received Signal Strength Indicator of the packet.


Definition at line 337 of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h

id_pkts_rcvd#

uint16_t rsi_bt_per_stats_s::id_pkts_rcvd

Packet count of ID packets received.


Definition at line 339 of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h

dummy#

uint16_t rsi_bt_per_stats_s::dummy[5]

Dummy array of length 5.


Definition at line 341 of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h