Attestation#
This section provides a reference to the Crypto API functions for device attestation.
Functions#
sl_status_t
sl_si91x_attestation_get_token(uint8_t *token, uint16_t length, uint32_t *nonce)
\Process the nonce for attestation token
Function Documentation#
sl_si91x_attestation_get_token#
sl_status_t sl_si91x_attestation_get_token (uint8_t * token, uint16_t length, uint32_t * nonce)
\Process the nonce for attestation token
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t * | [in] | token | |
| uint16_t | [in] | length | |
| uint32_t * | [out] | nonce |
Returns
return sl_status code