Additional Status Codes#
This section provides a reference to the additional status codes returned by the WiSeConnect™ SDK v3.x which are not included in the list of Silicon Labs standard status codes.
Macros#
OS operation failed.
Bootup options not saved.
Bootup options checksum failed.
Bootloader version mismatch.
Waiting for board ready.
Invalid firmware.
Invalid option.
SPI busy.
Card ready not received.
Firmware upgrade timed out.
Does not exist.
Not authenticated.
Not keyed.
IOCTL fail.
Buffer unavailable temporarily.
Buffer unavailable permanently.
WPS PBC overlap.
Connection lost.
Cannot add extra event handler.
Error manipulating a semaphore.
Packet retrieval cancelled due to flow control.
Packet retrieval cancelled due to lack of bus credits.
Packet retrieval cancelled due to no pending packets.
Core disabled due to no clock.
Core disabled - in reset.
Unsupported function.
Error writing to WLAN register.
SDIO bus failed to come up.
Join not finished yet.
Specified network was not found.
Join status error.
Unknown interface specified.
Error during SDIO receive.
Hardware tag header corrupt.
Failed to allocate a buffer to receive into.
Error reading a bus hardware register.
Failed to create a new thread.
Error manipulating a queue.
Error moving the current pointer of a buffer.
Error setting size of packet buffer.
Null stack pointer passed when non null was required.
Error deleting a thread.
Failed to put a thread to sleep.
Failed to allocate a packet buffer.
Requested interface is not active.
Requested delay is too long.
Duty cycle is outside limit 0 to 0.
Returned pmk was the wrong length.
AP security type was unknown.
AP not allowed to use WEP - use Open instead.
WPA / WPA2 key length must be between 8 & 64 bytes.
Specified filter id not found.
Failed to read 0xfeedbead SPI id from chip.
Mismatch in sizes between SPI and SDPCM header.
Attempt to register a multicast address twice.
SDIO transfer failed too many times.
Null Pointer argument passed to function.
Error deleting a thread.
Semaphore/Mutex wait has been aborted.
Unaligned message in the queue.
Error while Mutex operation.
Error while decryption over secure link.
Error while renegotiation of key over secure link.
Invalid opermode provided.
Invalid security encryption method provided.
TRNG duplicate elements error.
Return when parameter passed to Crypto SAPI is invalid.
Return in AEAD (CCM, GCM, Chachapoly) decryption function, when MAC generated during decryption does not match the MAC passed.
Scan command issued while device is already associated with an access point.
No AP found.
Wrong PSK is issued while the device client tries to join an access point with WEP security enabled.
Invalid band.
Association not done or in unassociated state.
De-authentication received from AP.
Failed to associate to access point during "Join".
Invalid channel.
Authentication failure during "Join". Unable to find AP during join which was found during scan.
Missed beacon from AP during join.
Non-existent MAC address supplied in "Disassociate" command.
EAP configuration is not done.
Memory allocation failed or Store configuration check sum failed.
Information is wrong or insufficient in join command.
Not an AP interface.
Push button command given before the expiry of previous push button command.
Access point not found. Rejoin failure.
Frequency not supported.
Invalid opermode.
EAP configuration failed.
P2P configuration failed.
Unable to start Group Owner negotiation.
Join timeout.
Command given in incorrect state.
Query GO parameters issued in incorrect operating mode.
Unable to form access point.
Wrong scan input parameters supplied to "Scan" command.
Command issued during re-join in progress.
Wrong parameters the command request.
Provision discovery failed in P2P.
PSK length less than 8 bytes or more than 63 bytes.
Failed to clear or to set the Enterprise Certificate (Set Certificate).
P2P Go negotiation failed.
Association between nodes failed in P2P WPS mode due to timeout.
If a command is issued by the Host when the device is internally executing auto-join or auto-create.
WEP key is of wrong length.
ICMP request timeout error.
ICMP data size exceeds maximum limit.
Send data packet exceeded the limit or length that is mentioned (or) MQTT publish data and publish data length mismatched (or) MQTT Send data packet exceeded the limit.
ARP cache entry not found.
UART command timeout happened.
Fixed data rate is not supported by connecting AP.
Maximum length exceeded of username/password/client_id/topic in MQTT.
Wrong WPS PIN.
Wrong WPS PIN length.
Wrong PMK length.
SSID not present for PMK generation.
SSID incorrect for PMK generation(more than 32 bytes).
Band not supported.
User store configuration invalid length.
Error in length of the command (Exceeds number of characters is mentioned in the PRM).
Data packet dropped.
WEP key not given.
Error in length of store config profile.
PSK or PMK not given.
Security mode given in join command is invalid.
Beacon miscount reaches max beacon miscount (De-authentication due to beacon miss).
De-authentication received from supplicant.
De-authentication received from AP after channel switching.
Synchronization missed.
Authentication timeout occurred.
Association timeout.
BG scan in given channels is not allowed.
Scanned SSID and SSID given in join are not matching.
Given number of clients exceeded max number of stations supported.
Given HT capabilities are not supported.
UART Flow control not supported.
ZB/BT/BLE packet received and protocol is not enabled.
MGMT pkt dropped.
Invalid RF current mode.
Power save support is not present for a given interface.
Concurrent AP in connected state.
Connected AP or Station channel mismatch.
IAP co processor error.
WPS not supported in current operating mode.
Concurrent AP doesn't have same channel as connected station channel.
PBC session overlap error.
BT feature bit map invalid.
4/4 confirmation of 4 way handshake failed.
MAC address not present in MAC based join.
Concurrent mode, both AP and client should be up, to enable configuration.
Certificate load not allowed in flash.
Certificate load not allowed in RAM.
Certificate load failed due to wrong index.
AP HT caps not enabled.
Address family not supported by protocol.
Invalid beacon interval or DTIM period provided.
Invalid range of the configuration provided.
RTS THRESHOLD Config type is invalid.
Error with MQTT command.
listen interval in power save is greater than that of join.
WLAN radio deregistered.
SAE failure due to multiple confirm frames from AP.
AP does not support the EC-group set by station.
Occurs when HE_PARAMS_SUPPORT and SLI_SI91X_ENABLE_TWT_FEATURE macros are not enabled.
Occurs when user tries to give TWT config command when there is an already active TWT session.
Occurs when TWT teardown command is given with a flow ID that does not match existing session flow ID.
Occurs when teardown command is given while there is no active session.
This error code indicates that TWT session is not feasible. It is thrown only when TWT Auto Selection API is used.
AP does not support TWT information frame reception.
No active TWT agreement corresponding to given flow id.
Suspend or resume TWT action is in progress.
TWT information frame packet creation failed in firmware.
Invalid station TSF error returned when station is not connected or atleast one beacon is not received.
The Server does not support the level of the MQTT protocol requested by the Client.
The Client identifier is correct UTF-8 but not allowed by the Server.
The Network Connection has been made but the MQTT service is unavailable.
The data in the user name or password is malformed.
The Client is not authorized to connect.
Disconnection due to SA Query Timeout.
Duplicate entry exists in DNS server table.
Memory error: No memory available.
Invalid characters in JSON object.
Update commands: No such key found.
No such file found: Re-check filename.
No corresponding web page exists with same filename.
Space unavailable for new file.
Invalid input data, Re-check filename, lengths, etc.
Space unavailable for new file.
Existing file overwrite: Exceeds size of previous file. Use erase and try again.
No such file found. Re-check filename.
Memory Error: No memory available.
Received more web page data than the total length initially specified.
Error in set region command.
Web page current chunk length is incorrect.
Error in AP set region command.
Error in AP set region command parameters.
Region code not supported.
Error in extracting country region from beacon.
Device does not have selected region support.
SSL/TLS context create failed.
SSL/TLS handshake failed. Socket will be closed.
SSL/TLS max sockets reached.
FTP client is not connected.
Cipher set failure.
HTTP credentials maximum length exceeded.
Feature not supported.
Unable to write to flash OR flash data verification failed.
Calibration data verification failed.
SNMP internal error.
SNMP invalid IP protocol error.
No data received or receive timeout.
Insufficient data for converting NTP time to mm-dd-yy time format.
Invalid SNTP server address.
SNTP client not started.
SNTP server not available. Client will not get any time update service from current server.
SNTP server authentication failed.
Internal error.
Entry not found for multicast IP address.
No more entries found for multicast.
IP address error.
Socket already bound.
Port not available.
Socket is not created.
ICMP request failed.
Maximum listen sockets reached.
DHCP duplicate listen.
Port not in closed state.
Socket is closed or in process of closing.
Process in progress.
Trying to connect non-existing TCP server socket.
Error in length of the command ('Exceeds number of characters' is mentioned in the PRM).
Wrong packet info.
Socket is still bound.
No free port.
Invalid port.
Feature not supported.
Socket is not in connected state. Disconnected from server. In case of FTP, user need to give destroy command after receiving this error.
POP3 session creation failed / POP3 session got terminated.
DHCPv6 handshake failure.
DHCP invalid IP response.
SMTP authentication error.
No DNS server was specified, SMTP over size mail data.
SMTP invalid server reply.
DNS query failed, SMTP internal error.
Bad DNS address, SMTP server error code received.
SMTP invalid parameters.
SMTP packet allocation failed.
SMTP Greet reply failed.
Parameter error, SMTP hello reply error.
SMTP mail reply error.
SMTP RCPT reply error.
SMTP message reply error.
SMTP data reply error.
SMTP authentication reply error.
SMTP server error reply.
DNS duplicate entry.
SMTP oversize server reply.
SMTP client not initialized.
DNS IPv6 not supported.
Invalid mail index for POP3 mail retrieve command.
SSL/TLS handshake failed.
FTP client is not connected or disconnected with the FTP server.
FTP client is not disconnected.
FTP file is not opened.
SSL/TLS handshake timeout or FTP file is not closed.
Expected [1XX response from FTP server but not received].
Expected [2XX response from FTP server but not received].
Expected [22X response from FTP server but not received].
Expected [23X response from FTP server but not received].
Expected [3XX response from FTP server but not received].
Expected [33X response from FTP server but not received].
HTTP timeout.
HTTP failed.
HTTP timeout for HTTP PUT client.
Authentication error.
Invalid packet length. Content length and received data length is mismatching.
Server responds before HTTP client request is complete.
HTTP/HTTPS password is too long.
MQTT ping time out error.
MQTT command sent in incorrect state.
MQTT ACK time out error.
POP3 error for invalid mail index.
Listening TCP socket in device is not connected to the remote peer, or the LTCP socket is not yet opened in the device.
Sockets not available. The error comes if the host tries to open more than 10 sockets.
HTTP OTAF invalid packet.
TCP_IP initialization failed.
Cannot create IP in same interface in concurrent mode.
HTTP OTAF incomplete packet.
Store configuration profile type mismatch or invalid profile type.
MQTT remote terminate error.
Byte stuffing error in AT mode.
Invalid command (e.g. parameters insufficient or invalid in the command). Invalid operation (e.g. power save command with the same mode given twice, accessing wrong socket, creating more than allowed sockets ).
HTTP OTAF no packet.
TCP socket is not connected.
Station count exceeded max station supported.
Unable to send TCP data.
Socket buffer too small.
Invalid content in the DNS response to the DNS resolution query.
DNS class error in response to the DNS resolution query.
DNS count error in response to the DNS resolution query.
DNS return code error in the response to the DNS resolution query.
DNS Opcode error in the response to the DNS resolution query.
DNS id mismatch between DNS resolution request and response.
An invalid input to the DNS resolution query.
DNS response was timed out.
ARP request failure.
Unable to update TCP window.
DHCP lease time expired.
DHCP handshake failure.
This error is issued when WebSocket creation failed.
This error is issued when device tried to connect to a non-existent TCP server socket on the remote side.
This error is issued when tried to close non-existent socket. or invalid socket descriptor.
Invalid socket parameters.
Feature not supported.
Socket already open.
Attempt to open more than the maximum allowed number of sockets.
Data length exceeds mss.
DUT unable to configure IP address due to IP conflict.
Feature not enabled.
DHCP server not set in AP mode.
Error in AP set region command parameters.
SSL/TLS not supported.
JSON not supported.
Invalid operating mode.
Invalid socket configuration parameters.
Web socket creation timeout.
Parameter maximum allowed value is exceeded.
Socket read timeout.
Invalid command in sequence.
DNS response timed out.
HTTP socket creation failed.
HTTP GET command is in progress.
TCP socket close command is issued before getting the response of the previous close command.
'Wait On Host' feature not enabled.
Store configuration checksum validation failed.
TCP keep alive timed out.
TCP ACK failed for TCP SYN-ACK.
Memory limit exceeded in a given operating mode.
Memory limit exceeded in an operating mode during auto join/create.
PUF operation is blocked.
PUF activation code invalid.
PUF input parameters invalid.
PUF in error state.
PUF operation not allowed.
PUF operation failed.
Auto join or user store configuration going on.
Improper RSNIE from AP to station.
Reached maximum SNTP invalid attempts.
Frequency offset sent is zero.
Frequency offset specified goes beyond upper or lower limits and indicates that frequency offset cannot be changed further.
Macro Definition Documentation#
SL_STATUS_OS_OPERATION_FAILURE#
#define SL_STATUS_OS_OPERATION_FAILUREValue:
((sl_status_t)0x0051)
OS operation failed.
SL_STATUS_BOOTUP_OPTIONS_NOT_SAVED#
#define SL_STATUS_BOOTUP_OPTIONS_NOT_SAVEDValue:
((sl_status_t)0x0052)
Bootup options not saved.
SL_STATUS_BOOTUP_OPTIONS_CHECKSUM_FAILURE#
#define SL_STATUS_BOOTUP_OPTIONS_CHECKSUM_FAILUREValue:
((sl_status_t)0x0053)
Bootup options checksum failed.
SL_STATUS_BOOTLOADER_VERSION_MISMATCH#
#define SL_STATUS_BOOTLOADER_VERSION_MISMATCHValue:
((sl_status_t)0x0054)
Bootloader version mismatch.
SL_STATUS_WAITING_FOR_BOARD_READY#
#define SL_STATUS_WAITING_FOR_BOARD_READYValue:
((sl_status_t)0x0055)
Waiting for board ready.
SL_STATUS_VALID_FIRMWARE_NOT_PRESENT#
#define SL_STATUS_VALID_FIRMWARE_NOT_PRESENTValue:
((sl_status_t)0x0056)
Invalid firmware.
SL_STATUS_CARD_READY_TIMEOUT#
#define SL_STATUS_CARD_READY_TIMEOUTValue:
((sl_status_t)0x0059)
Card ready not received.
SL_STATUS_FW_LOAD_OR_UPGRADE_TIMEOUT#
#define SL_STATUS_FW_LOAD_OR_UPGRADE_TIMEOUTValue:
((sl_status_t)0x005A)
Firmware upgrade timed out.
SL_STATUS_WIFI_DOES_NOT_EXIST#
#define SL_STATUS_WIFI_DOES_NOT_EXISTValue:
((sl_status_t)0x0B21)
Does not exist.
SL_STATUS_WIFI_NOT_AUTHENTICATED#
#define SL_STATUS_WIFI_NOT_AUTHENTICATEDValue:
((sl_status_t)0x0B22)
Not authenticated.
SL_STATUS_WIFI_BUFFER_UNAVAILABLE_TEMPORARY
#define SL_STATUS_WIFI_BUFFER_UNAVAILABLE_TEMPORARYValue:
((sl_status_t)0x0B25)
Buffer unavailable temporarily.
SL_STATUS_WIFI_BUFFER_UNAVAILABLE_PERMANENT
#define SL_STATUS_WIFI_BUFFER_UNAVAILABLE_PERMANENTValue:
((sl_status_t)0x0B26)
Buffer unavailable permanently.
SL_STATUS_WIFI_WPS_PBC_OVERLAP#
#define SL_STATUS_WIFI_WPS_PBC_OVERLAPValue:
((sl_status_t)0x0B27)
WPS PBC overlap.
SL_STATUS_WIFI_CONNECTION_LOST#
#define SL_STATUS_WIFI_CONNECTION_LOSTValue:
((sl_status_t)0x0B28)
Connection lost.
SL_STATUS_WIFI_OUT_OF_EVENT_HANDLER_SPACE#
#define SL_STATUS_WIFI_OUT_OF_EVENT_HANDLER_SPACEValue:
((sl_status_t)0x0B29)
Cannot add extra event handler.
SL_STATUS_WIFI_SEMAPHORE_ERROR#
#define SL_STATUS_WIFI_SEMAPHORE_ERRORValue:
((sl_status_t)0x0B2A)
Error manipulating a semaphore.
SL_STATUS_WIFI_FLOW_CONTROLLED#
#define SL_STATUS_WIFI_FLOW_CONTROLLEDValue:
((sl_status_t)0x0B2B)
Packet retrieval cancelled due to flow control.
SL_STATUS_WIFI_NO_CREDITS#
#define SL_STATUS_WIFI_NO_CREDITSValue:
((sl_status_t)0x0B2C)
Packet retrieval cancelled due to lack of bus credits.
SL_STATUS_WIFI_NO_PACKET_TO_SEND#
#define SL_STATUS_WIFI_NO_PACKET_TO_SENDValue:
((sl_status_t)0x0B2D)
Packet retrieval cancelled due to no pending packets.
SL_STATUS_WIFI_CORE_CLOCK_NOT_ENABLED#
#define SL_STATUS_WIFI_CORE_CLOCK_NOT_ENABLEDValue:
((sl_status_t)0x0B2E)
Core disabled due to no clock.
SL_STATUS_WIFI_CORE_IN_RESET#
#define SL_STATUS_WIFI_CORE_IN_RESETValue:
((sl_status_t)0x0B2F)
Core disabled - in reset.
SL_STATUS_WIFI_UNSUPPORTED#
#define SL_STATUS_WIFI_UNSUPPORTEDValue:
((sl_status_t)0x0B30)
Unsupported function.
SL_STATUS_WIFI_BUS_WRITE_REGISTER_ERROR#
#define SL_STATUS_WIFI_BUS_WRITE_REGISTER_ERRORValue:
((sl_status_t)0x0B31)
Error writing to WLAN register.
SL_STATUS_WIFI_SDIO_BUS_UP_FAIL#
#define SL_STATUS_WIFI_SDIO_BUS_UP_FAILValue:
((sl_status_t)0x0B32)
SDIO bus failed to come up.
SL_STATUS_WIFI_JOIN_IN_PROGRESS#
#define SL_STATUS_WIFI_JOIN_IN_PROGRESSValue:
((sl_status_t)0x0B33)
Join not finished yet.
SL_STATUS_WIFI_NETWORK_NOT_FOUND#
#define SL_STATUS_WIFI_NETWORK_NOT_FOUNDValue:
((sl_status_t)0x0B34)
Specified network was not found.
SL_STATUS_WIFI_INVALID_JOIN_STATUS#
#define SL_STATUS_WIFI_INVALID_JOIN_STATUSValue:
((sl_status_t)0x0B35)
Join status error.
SL_STATUS_WIFI_UNKNOWN_INTERFACE#
#define SL_STATUS_WIFI_UNKNOWN_INTERFACEValue:
((sl_status_t)0x0B36)
Unknown interface specified.
SL_STATUS_WIFI_SDIO_RX_FAIL#
#define SL_STATUS_WIFI_SDIO_RX_FAILValue:
((sl_status_t)0x0B37)
Error during SDIO receive.
SL_STATUS_WIFI_HWTAG_MISMATCH#
#define SL_STATUS_WIFI_HWTAG_MISMATCHValue:
((sl_status_t)0x0B38)
Hardware tag header corrupt.
SL_STATUS_WIFI_RX_BUFFER_ALLOC_FAIL#
#define SL_STATUS_WIFI_RX_BUFFER_ALLOC_FAILValue:
((sl_status_t)0x0B39)
Failed to allocate a buffer to receive into.
SL_STATUS_WIFI_BUS_READ_REGISTER_ERROR#
#define SL_STATUS_WIFI_BUS_READ_REGISTER_ERRORValue:
((sl_status_t)0x0B3A)
Error reading a bus hardware register.
SL_STATUS_WIFI_THREAD_CREATE_FAILED#
#define SL_STATUS_WIFI_THREAD_CREATE_FAILEDValue:
((sl_status_t)0x0B3B)
Failed to create a new thread.
SL_STATUS_WIFI_QUEUE_ERROR#
#define SL_STATUS_WIFI_QUEUE_ERRORValue:
((sl_status_t)0x0B3C)
Error manipulating a queue.
SL_STATUS_WIFI_BUFFER_POINTER_MOVE_ERROR#
#define SL_STATUS_WIFI_BUFFER_POINTER_MOVE_ERRORValue:
((sl_status_t)0x0B3D)
Error moving the current pointer of a buffer.
SL_STATUS_WIFI_BUFFER_SIZE_SET_ERROR#
#define SL_STATUS_WIFI_BUFFER_SIZE_SET_ERRORValue:
((sl_status_t)0x0B3E)
Error setting size of packet buffer.
SL_STATUS_WIFI_THREAD_STACK_NULL#
#define SL_STATUS_WIFI_THREAD_STACK_NULLValue:
((sl_status_t)0x0B3F)
Null stack pointer passed when non null was required.
SL_STATUS_WIFI_THREAD_DELETE_FAIL#
#define SL_STATUS_WIFI_THREAD_DELETE_FAILValue:
((sl_status_t)0x0B40)
Error deleting a thread.
SL_STATUS_WIFI_SLEEP_ERROR#
#define SL_STATUS_WIFI_SLEEP_ERRORValue:
((sl_status_t)0x0B41)
Failed to put a thread to sleep.
SL_STATUS_WIFI_BUFFER_ALLOC_FAIL#
#define SL_STATUS_WIFI_BUFFER_ALLOC_FAILValue:
((sl_status_t)0x0B42)
Failed to allocate a packet buffer.
SL_STATUS_WIFI_INTERFACE_NOT_UP#
#define SL_STATUS_WIFI_INTERFACE_NOT_UPValue:
((sl_status_t)0x0B44)
Requested interface is not active.
SL_STATUS_WIFI_DELAY_TOO_LONG#
#define SL_STATUS_WIFI_DELAY_TOO_LONGValue:
((sl_status_t)0x0B45)
Requested delay is too long.
SL_STATUS_WIFI_INVALID_DUTY_CYCLE#
#define SL_STATUS_WIFI_INVALID_DUTY_CYCLEValue:
((sl_status_t)0x0B46)
Duty cycle is outside limit 0 to 0.
SL_STATUS_WIFI_PMK_WRONG_LENGTH#
#define SL_STATUS_WIFI_PMK_WRONG_LENGTHValue:
((sl_status_t)0x0B47)
Returned pmk was the wrong length.
SL_STATUS_WIFI_UNKNOWN_SECURITY_TYPE#
#define SL_STATUS_WIFI_UNKNOWN_SECURITY_TYPEValue:
((sl_status_t)0x0B48)
AP security type was unknown.
SL_STATUS_WIFI_WEP_NOT_ALLOWED#
#define SL_STATUS_WIFI_WEP_NOT_ALLOWEDValue:
((sl_status_t)0x0B49)
AP not allowed to use WEP - use Open instead.
SL_STATUS_WIFI_WPA_KEYLEN_BAD#
#define SL_STATUS_WIFI_WPA_KEYLEN_BADValue:
((sl_status_t)0x0B4A)
WPA / WPA2 key length must be between 8 & 64 bytes.
SL_STATUS_WIFI_FILTER_NOT_FOUND#
#define SL_STATUS_WIFI_FILTER_NOT_FOUNDValue:
((sl_status_t)0x0B4B)
Specified filter id not found.
SL_STATUS_WIFI_SPI_ID_READ_FAIL#
#define SL_STATUS_WIFI_SPI_ID_READ_FAILValue:
((sl_status_t)0x0B4C)
Failed to read 0xfeedbead SPI id from chip.
SL_STATUS_WIFI_SPI_SIZE_MISMATCH#
#define SL_STATUS_WIFI_SPI_SIZE_MISMATCHValue:
((sl_status_t)0x0B4D)
Mismatch in sizes between SPI and SDPCM header.
SL_STATUS_WIFI_ADDRESS_ALREADY_REGISTERED#
#define SL_STATUS_WIFI_ADDRESS_ALREADY_REGISTEREDValue:
((sl_status_t)0x0B4E)
Attempt to register a multicast address twice.
SL_STATUS_WIFI_SDIO_RETRIES_EXCEEDED#
#define SL_STATUS_WIFI_SDIO_RETRIES_EXCEEDEDValue:
((sl_status_t)0x0B4F)
SDIO transfer failed too many times.
SL_STATUS_WIFI_NULL_PTR_ARG#
#define SL_STATUS_WIFI_NULL_PTR_ARGValue:
((sl_status_t)0x0B50)
Null Pointer argument passed to function.
SL_STATUS_WIFI_THREAD_FINISH_FAIL#
#define SL_STATUS_WIFI_THREAD_FINISH_FAILValue:
((sl_status_t)0x0B51)
Error deleting a thread.
SL_STATUS_WIFI_WAIT_ABORTED#
#define SL_STATUS_WIFI_WAIT_ABORTEDValue:
((sl_status_t)0x0B52)
Semaphore/Mutex wait has been aborted.
SL_STATUS_WIFI_QUEUE_MESSAGE_UNALIGNED#
#define SL_STATUS_WIFI_QUEUE_MESSAGE_UNALIGNEDValue:
((sl_status_t)0x0B53)
Unaligned message in the queue.
SL_STATUS_WIFI_MUTEX_ERROR#
#define SL_STATUS_WIFI_MUTEX_ERRORValue:
((sl_status_t)0x0B54)
Error while Mutex operation.
SL_STATUS_WIFI_SECURE_LINK_DECRYPT_ERROR#
#define SL_STATUS_WIFI_SECURE_LINK_DECRYPT_ERRORValue:
((sl_status_t)0x0B57)
Error while decryption over secure link.
SL_STATUS_WIFI_SECURE_LINK_KEY_RENEGOTIATION_ERROR#
#define SL_STATUS_WIFI_SECURE_LINK_KEY_RENEGOTIATION_ERRORValue:
((sl_status_t)0x0B59)
Error while renegotiation of key over secure link.
SL_STATUS_WIFI_INVALID_OPERMODE#
#define SL_STATUS_WIFI_INVALID_OPERMODEValue:
((sl_status_t)0x0B60)
Invalid opermode provided.
SL_STATUS_WIFI_INVALID_ENCRYPTION_METHOD#
#define SL_STATUS_WIFI_INVALID_ENCRYPTION_METHODValue:
((sl_status_t)0x0B61)
Invalid security encryption method provided.
SL_STATUS_TRNG_DUPLICATE_ENTROPY#
#define SL_STATUS_TRNG_DUPLICATE_ENTROPYValue:
((sl_status_t)0x0B62)
TRNG duplicate elements error.
SL_STATUS_CRYPTO_INVALID_PARAMETER#
#define SL_STATUS_CRYPTO_INVALID_PARAMETERValue:
((sl_status_t)0x1CCFE)
Return when parameter passed to Crypto SAPI is invalid.
SL_STATUS_CRYPTO_INVALID_SIGNATURE#
#define SL_STATUS_CRYPTO_INVALID_SIGNATUREValue:
((sl_status_t)0x1CC9A)
Return in AEAD (CCM, GCM, Chachapoly) decryption function, when MAC generated during decryption does not match the MAC passed.
SL_STATUS_SI91X_SCAN_ISSUED_IN_ASSOCIATED_STATE#
#define SL_STATUS_SI91X_SCAN_ISSUED_IN_ASSOCIATED_STATEValue:
((sl_status_t)0x10002)
Scan command issued while device is already associated with an access point.
SL_STATUS_SI91X_NO_AP_FOUND#
#define SL_STATUS_SI91X_NO_AP_FOUNDValue:
((sl_status_t)0x10003)
No AP found.
SL_STATUS_SI91X_INVALID_PSK_IN_WEP_SECURITY#
#define SL_STATUS_SI91X_INVALID_PSK_IN_WEP_SECURITYValue:
((sl_status_t)0x10004)
Wrong PSK is issued while the device client tries to join an access point with WEP security enabled.
SL_STATUS_SI91X_INVALID_BAND#
#define SL_STATUS_SI91X_INVALID_BANDValue:
((sl_status_t)0x10005)
Invalid band.
SL_STATUS_SI91X_UNASSOCIATED#
#define SL_STATUS_SI91X_UNASSOCIATEDValue:
((sl_status_t)0x10006)
Association not done or in unassociated state.
SL_STATUS_SI91X_DEAUTHENTICATION_RECEIVED_FROM_AP#
#define SL_STATUS_SI91X_DEAUTHENTICATION_RECEIVED_FROM_APValue:
((sl_status_t)0x10008)
De-authentication received from AP.
SL_STATUS_SI91X_ASSOCIATION_FAILED#
#define SL_STATUS_SI91X_ASSOCIATION_FAILEDValue:
((sl_status_t)0x10009)
Failed to associate to access point during "Join".
SL_STATUS_SI91X_INVALID_CHANNEL#
#define SL_STATUS_SI91X_INVALID_CHANNELValue:
((sl_status_t)0x1000A)
Invalid channel.
SL_STATUS_SI91X_JOIN_AUTHENTICATION_FAILED#
#define SL_STATUS_SI91X_JOIN_AUTHENTICATION_FAILEDValue:
((sl_status_t)0x1000E)
Authentication failure during "Join". Unable to find AP during join which was found during scan.
SL_STATUS_SI91X_BEACON_MISSED_FROM_AP_DURING_JOIN#
#define SL_STATUS_SI91X_BEACON_MISSED_FROM_AP_DURING_JOINValue:
((sl_status_t)0x1000F)
Missed beacon from AP during join.
SL_STATUS_SI91X_INVALID_MAC_SUPPLIED#
#define SL_STATUS_SI91X_INVALID_MAC_SUPPLIEDValue:
((sl_status_t)0x10013)
Non-existent MAC address supplied in "Disassociate" command.
SL_STATUS_SI91X_EAP_CONFIG_NOT_DONE#
#define SL_STATUS_SI91X_EAP_CONFIG_NOT_DONEValue:
((sl_status_t)0x10014)
EAP configuration is not done.
SL_STATUS_SI91X_MEMORY_FAILED_FROM_MODULE#
#define SL_STATUS_SI91X_MEMORY_FAILED_FROM_MODULEValue:
((sl_status_t)0x10015)
Memory allocation failed or Store configuration check sum failed.
SL_STATUS_SI91X_INSUFFICIENT_INFO#
#define SL_STATUS_SI91X_INSUFFICIENT_INFOValue:
((sl_status_t)0x10016)
Information is wrong or insufficient in join command.
SL_STATUS_SI91X_NOT_AP_INTERFACE#
#define SL_STATUS_SI91X_NOT_AP_INTERFACEValue:
((sl_status_t)0x10017)
Not an AP interface.
SL_STATUS_SI91X_INVALID_PUSH_BUTTON_SEQUENCE
#define SL_STATUS_SI91X_INVALID_PUSH_BUTTON_SEQUENCEValue:
((sl_status_t)0x10018)
Push button command given before the expiry of previous push button command.
SL_STATUS_SI91X_REJOIN_FAILURE#
#define SL_STATUS_SI91X_REJOIN_FAILUREValue:
((sl_status_t)0x10019)
Access point not found. Rejoin failure.
SL_STATUS_SI91X_FREQUENCY_NOT_SUPPORTED#
#define SL_STATUS_SI91X_FREQUENCY_NOT_SUPPORTEDValue:
((sl_status_t)0x1001A)
Frequency not supported.
SL_STATUS_SI91X_INVALID_OPERMODE#
#define SL_STATUS_SI91X_INVALID_OPERMODEValue:
((sl_status_t)0x1001B)
Invalid opermode.
SL_STATUS_SI91X_EAP_CONFIG_FAILED#
#define SL_STATUS_SI91X_EAP_CONFIG_FAILEDValue:
((sl_status_t)0x1001C)
EAP configuration failed.
SL_STATUS_SI91X_P2P_CONFIG_FAILED#
#define SL_STATUS_SI91X_P2P_CONFIG_FAILEDValue:
((sl_status_t)0x1001D)
P2P configuration failed.
SL_STATUS_SI91X_GROUP_OWNER_NEGOTIATION_FAILED#
#define SL_STATUS_SI91X_GROUP_OWNER_NEGOTIATION_FAILEDValue:
((sl_status_t)0x1001E)
Unable to start Group Owner negotiation.
SL_STATUS_SI91X_JOIN_TIMEOUT#
#define SL_STATUS_SI91X_JOIN_TIMEOUTValue:
((sl_status_t)0x10020)
Join timeout.
SL_STATUS_SI91X_COMMAND_GIVEN_IN_INVALID_STATE#
#define SL_STATUS_SI91X_COMMAND_GIVEN_IN_INVALID_STATEValue:
((sl_status_t)0x10021)
Command given in incorrect state.
SL_STATUS_SI91X_INVALID_QUERY_GO_PARAMS#
#define SL_STATUS_SI91X_INVALID_QUERY_GO_PARAMSValue:
((sl_status_t)0x10022)
Query GO parameters issued in incorrect operating mode.
SL_STATUS_SI91X_ACCESS_POINT_FAILED#
#define SL_STATUS_SI91X_ACCESS_POINT_FAILEDValue:
((sl_status_t)0x10023)
Unable to form access point.
SL_STATUS_SI91X_INVALID_SCAN_INFO#
#define SL_STATUS_SI91X_INVALID_SCAN_INFOValue:
((sl_status_t)0x10024)
Wrong scan input parameters supplied to "Scan" command.
SL_STATUS_SI91X_COMMAND_ISSUED_IN_REJOIN_STATE#
#define SL_STATUS_SI91X_COMMAND_ISSUED_IN_REJOIN_STATEValue:
((sl_status_t)0x10025)
Command issued during re-join in progress.
SL_STATUS_SI91X_WRONG_PARAMETERS#
#define SL_STATUS_SI91X_WRONG_PARAMETERSValue:
((sl_status_t)0x10026)
Wrong parameters the command request.
SL_STATUS_SI91X_PROVISION_DISCOVERY_FAILED_IN_P2P#
#define SL_STATUS_SI91X_PROVISION_DISCOVERY_FAILED_IN_P2PValue:
((sl_status_t)0x10027)
Provision discovery failed in P2P.
SL_STATUS_SI91X_INVALID_PSK_LENGTH#
#define SL_STATUS_SI91X_INVALID_PSK_LENGTHValue:
((sl_status_t)0x10028)
PSK length less than 8 bytes or more than 63 bytes.
SL_STATUS_SI91X_FAILED_TO_CLEAR_OR_SET_EAP_CERTIFICATE#
#define SL_STATUS_SI91X_FAILED_TO_CLEAR_OR_SET_EAP_CERTIFICATEValue:
((sl_status_t)0x10029)
Failed to clear or to set the Enterprise Certificate (Set Certificate).
SL_STATUS_SI91X_P2P_GO_NEGOTIATED_FAILED#
#define SL_STATUS_SI91X_P2P_GO_NEGOTIATED_FAILEDValue:
((sl_status_t)0x1002A)
P2P Go negotiation failed.
SL_STATUS_SI91X_ASSOCIATION_TIMEOUT_IN_P2P_WPS_MODE#
#define SL_STATUS_SI91X_ASSOCIATION_TIMEOUT_IN_P2P_WPS_MODEValue:
((sl_status_t)0x1002B)
Association between nodes failed in P2P WPS mode due to timeout.
SL_STATUS_SI91X_COMMAND_ISSUED_WHILE_INTERNAL_OPERATION#
#define SL_STATUS_SI91X_COMMAND_ISSUED_WHILE_INTERNAL_OPERATIONValue:
((sl_status_t)0x1002C)
If a command is issued by the Host when the device is internally executing auto-join or auto-create.
SL_STATUS_SI91X_INVALID_WEP_KEY_LEN#
#define SL_STATUS_SI91X_INVALID_WEP_KEY_LENValue:
((sl_status_t)0x1002D)
WEP key is of wrong length.
SL_STATUS_SI91X_ICMP_REQUEST_TIMEOUT_ERROR#
#define SL_STATUS_SI91X_ICMP_REQUEST_TIMEOUT_ERRORValue:
((sl_status_t)0x1002E)
ICMP request timeout error.
SL_STATUS_SI91X_ICMP_DATA_SIZE_EXCEED_MAX_LIMIT#
#define SL_STATUS_SI91X_ICMP_DATA_SIZE_EXCEED_MAX_LIMITValue:
((sl_status_t)0x1002F)
ICMP data size exceeds maximum limit.
SL_STATUS_SI91X_SEND_DATA_PACKET_EXCEED_LIMIT#
#define SL_STATUS_SI91X_SEND_DATA_PACKET_EXCEED_LIMITValue:
((sl_status_t)0x10030)
Send data packet exceeded the limit or length that is mentioned (or) MQTT publish data and publish data length mismatched (or) MQTT Send data packet exceeded the limit.
SL_STATUS_SI91X_ARP_CACHE_NOT_FOUND#
#define SL_STATUS_SI91X_ARP_CACHE_NOT_FOUNDValue:
((sl_status_t)0x10031)
ARP cache entry not found.
SL_STATUS_SI91X_UART_COMMAND_TIMEOUT#
#define SL_STATUS_SI91X_UART_COMMAND_TIMEOUTValue:
((sl_status_t)0x10032)
UART command timeout happened.
SL_STATUS_SI91X_FIXED_DATA_RATE_NOT_SUPPORTED_BY_AP#
#define SL_STATUS_SI91X_FIXED_DATA_RATE_NOT_SUPPORTED_BY_APValue:
((sl_status_t)0x10033)
Fixed data rate is not supported by connecting AP.
SL_STATUS_SI91X_USERNAME_PASSWORD_CLIENTID_TOPIC_MAX_LEN#
#define SL_STATUS_SI91X_USERNAME_PASSWORD_CLIENTID_TOPIC_MAX_LENValue:
((sl_status_t)0x10036)
Maximum length exceeded of username/password/client_id/topic in MQTT.
SL_STATUS_SI91X_INVALID_WPS_PIN#
#define SL_STATUS_SI91X_INVALID_WPS_PINValue:
((sl_status_t)0x10037)
Wrong WPS PIN.
SL_STATUS_SI91X_INVALID_WPS_PIN_LEN#
#define SL_STATUS_SI91X_INVALID_WPS_PIN_LENValue:
((sl_status_t)0x10038)
Wrong WPS PIN length.
SL_STATUS_SI91X_INVALID_PMK_LEN#
#define SL_STATUS_SI91X_INVALID_PMK_LENValue:
((sl_status_t)0x10039)
Wrong PMK length.
SL_STATUS_SI91X_SSID_NOT_PRESENT_FOR_PMK_GENERATION#
#define SL_STATUS_SI91X_SSID_NOT_PRESENT_FOR_PMK_GENERATIONValue:
((sl_status_t)0x1003A)
SSID not present for PMK generation.
SL_STATUS_SI91X_SSID_INCORRECT_PMK_GENERATION#
#define SL_STATUS_SI91X_SSID_INCORRECT_PMK_GENERATIONValue:
((sl_status_t)0x1003B)
SSID incorrect for PMK generation(more than 32 bytes).
SL_STATUS_SI91X_BAND_NOT_SUPPORTED#
#define SL_STATUS_SI91X_BAND_NOT_SUPPORTEDValue:
((sl_status_t)0x1003C)
Band not supported.
SL_STATUS_SI91X_INVALID_USR_STORE_CONFIGURATION_LEN#
#define SL_STATUS_SI91X_INVALID_USR_STORE_CONFIGURATION_LENValue:
((sl_status_t)0x1003D)
User store configuration invalid length.
SL_STATUS_SI91X_INVALID_COMMAND_LEN#
#define SL_STATUS_SI91X_INVALID_COMMAND_LENValue:
((sl_status_t)0x1003E)
Error in length of the command (Exceeds number of characters is mentioned in the PRM).
SL_STATUS_SI91X_DATA_PACKET_DROPPED#
#define SL_STATUS_SI91X_DATA_PACKET_DROPPEDValue:
((sl_status_t)0x1003F)
Data packet dropped.
SL_STATUS_SI91X_WEP_KEY_NOT_GIVEN#
#define SL_STATUS_SI91X_WEP_KEY_NOT_GIVENValue:
((sl_status_t)0x10040)
WEP key not given.
SL_STATUS_SI91X_INVALID_STORE_CONFIG_PROFILE#
#define SL_STATUS_SI91X_INVALID_STORE_CONFIG_PROFILEValue:
((sl_status_t)0x10041)
Error in length of store config profile.
SL_STATUS_SI91X_MISSING_PSK_OR_PMK#
#define SL_STATUS_SI91X_MISSING_PSK_OR_PMKValue:
((sl_status_t)0x10042)
PSK or PMK not given.
SL_STATUS_SI91X_INVALID_SECURITY_MODE_IN_JOIN_COMMAND#
#define SL_STATUS_SI91X_INVALID_SECURITY_MODE_IN_JOIN_COMMANDValue:
((sl_status_t)0x10043)
Security mode given in join command is invalid.
SL_STATUS_SI91X_MAX_BEACON_MISCOUNT#
#define SL_STATUS_SI91X_MAX_BEACON_MISCOUNTValue:
((sl_status_t)0x10044)
Beacon miscount reaches max beacon miscount (De-authentication due to beacon miss).
SL_STATUS_SI91X_DEAUTH_REQUEST_FROM_SUPPLICANT#
#define SL_STATUS_SI91X_DEAUTH_REQUEST_FROM_SUPPLICANTValue:
((sl_status_t)0x10045)
De-authentication received from supplicant.
SL_STATUS_SI91X_DEAUTH_REQUEST_FROM_FROM_AP#
#define SL_STATUS_SI91X_DEAUTH_REQUEST_FROM_FROM_APValue:
((sl_status_t)0x10046)
De-authentication received from AP after channel switching.
SL_STATUS_SI91X_MISSED_SYNCHRONIZATION#
#define SL_STATUS_SI91X_MISSED_SYNCHRONIZATIONValue:
((sl_status_t)0x10047)
Synchronization missed.
SL_STATUS_SI91X_AUTHENTICATION_TIMEOUT#
#define SL_STATUS_SI91X_AUTHENTICATION_TIMEOUTValue:
((sl_status_t)0x10048)
Authentication timeout occurred.
SL_STATUS_SI91X_ASSOCIATION_TIMEOUT#
#define SL_STATUS_SI91X_ASSOCIATION_TIMEOUTValue:
((sl_status_t)0x10049)
Association timeout.
SL_STATUS_SI91X_BG_SCAN_NOT_ALLOWED#
#define SL_STATUS_SI91X_BG_SCAN_NOT_ALLOWEDValue:
((sl_status_t)0x1004A)
BG scan in given channels is not allowed.
SL_STATUS_SI91X_SSID_MISMATCH#
#define SL_STATUS_SI91X_SSID_MISMATCHValue:
((sl_status_t)0x1004B)
Scanned SSID and SSID given in join are not matching.
SL_STATUS_SI91X_CLIENT_MAX_SUPPORTED_EXCEEDED#
#define SL_STATUS_SI91X_CLIENT_MAX_SUPPORTED_EXCEEDEDValue:
((sl_status_t)0x1004C)
Given number of clients exceeded max number of stations supported.
SL_STATUS_SI91X_HT_CAPABILITIES_NOT_SUPPORTED#
#define SL_STATUS_SI91X_HT_CAPABILITIES_NOT_SUPPORTEDValue:
((sl_status_t)0x1004D)
Given HT capabilities are not supported.
SL_STATUS_SI91X_UART_FLOW_NOT_SUPPORTED#
#define SL_STATUS_SI91X_UART_FLOW_NOT_SUPPORTEDValue:
((sl_status_t)0x1004E)
UART Flow control not supported.
SL_STATUS_SI91X_ZB_BT_BLE_PKT_RECEIVED#
#define SL_STATUS_SI91X_ZB_BT_BLE_PKT_RECEIVEDValue:
((sl_status_t)0x1004F)
ZB/BT/BLE packet received and protocol is not enabled.
SL_STATUS_SI91X_MGMT_PKT_DROPPED#
#define SL_STATUS_SI91X_MGMT_PKT_DROPPEDValue:
((sl_status_t)0x10050)
MGMT pkt dropped.
SL_STATUS_SI91X_INVALID_RF_CURRENT_MODE#
#define SL_STATUS_SI91X_INVALID_RF_CURRENT_MODEValue:
((sl_status_t)0x10051)
Invalid RF current mode.
SL_STATUS_SI91X_POWER_SAVE_NOT_SUPPORTED#
#define SL_STATUS_SI91X_POWER_SAVE_NOT_SUPPORTEDValue:
((sl_status_t)0x10052)
Power save support is not present for a given interface.
SL_STATUS_SI91X_CONCURRENT_AP_IN_CONNECTED_STATE#
#define SL_STATUS_SI91X_CONCURRENT_AP_IN_CONNECTED_STATEValue:
((sl_status_t)0x10053)
Concurrent AP in connected state.
SL_STATUS_SI91X_CONNECTED_AP_OR_STATION_CHANNEL_MISMATCH#
#define SL_STATUS_SI91X_CONNECTED_AP_OR_STATION_CHANNEL_MISMATCHValue:
((sl_status_t)0x10054)
Connected AP or Station channel mismatch.
SL_STATUS_SI91X_IAP_COPROCESSOR_ERROR#
#define SL_STATUS_SI91X_IAP_COPROCESSOR_ERRORValue:
((sl_status_t)0x10055)
IAP co processor error.
SL_STATUS_SI91X_WPS_NOT_SUPPORTED#
#define SL_STATUS_SI91X_WPS_NOT_SUPPORTEDValue:
((sl_status_t)0x10056)
WPS not supported in current operating mode.
SL_STATUS_SI91X_CONCURRENT_AP_CHANNEL_MISMATCH#
#define SL_STATUS_SI91X_CONCURRENT_AP_CHANNEL_MISMATCHValue:
((sl_status_t)0x10057)
Concurrent AP doesn't have same channel as connected station channel.
SL_STATUS_SI91X_PBC_SESSION_OVERLAP#
#define SL_STATUS_SI91X_PBC_SESSION_OVERLAPValue:
((sl_status_t)0x10058)
PBC session overlap error.
SL_STATUS_SI91X_BT_FEATURE_BITMAP_INVALID#
#define SL_STATUS_SI91X_BT_FEATURE_BITMAP_INVALIDValue:
((sl_status_t)0x10059)
BT feature bit map invalid.
SL_STATUS_SI91X_FOUR_WAY_HANDSHAKE_FAILED#
#define SL_STATUS_SI91X_FOUR_WAY_HANDSHAKE_FAILEDValue:
((sl_status_t)0x1005A)
4/4 confirmation of 4 way handshake failed.
SL_STATUS_SI91X_MAC_ADDRESS_NOT_PRESENT_IN_MAC_JOIN#
#define SL_STATUS_SI91X_MAC_ADDRESS_NOT_PRESENT_IN_MAC_JOINValue:
((sl_status_t)0x1005B)
MAC address not present in MAC based join.
SL_STATUS_SI91X_CONCURRENT_MODE_DOWN#
#define SL_STATUS_SI91X_CONCURRENT_MODE_DOWNValue:
((sl_status_t)0x1005C)
Concurrent mode, both AP and client should be up, to enable configuration.
SL_STATUS_SI91X_CERTIFICATE_LOAD_NOT_ALLOWED_IN_FLASH#
#define SL_STATUS_SI91X_CERTIFICATE_LOAD_NOT_ALLOWED_IN_FLASHValue:
((sl_status_t)0x1005D)
Certificate load not allowed in flash.
SL_STATUS_SI91X_CERTIFICATE_LOAD_NOT_ALLOWED_IN_RAM#
#define SL_STATUS_SI91X_CERTIFICATE_LOAD_NOT_ALLOWED_IN_RAMValue:
((sl_status_t)0x1005E)
Certificate load not allowed in RAM.
SL_STATUS_SI91X_WRONG_CERTIFICATE_LOAD_INDEX#
#define SL_STATUS_SI91X_WRONG_CERTIFICATE_LOAD_INDEXValue:
((sl_status_t)0x1005F)
Certificate load failed due to wrong index.
SL_STATUS_SI91X_AP_HT_CAPS_NOT_ENABLED#
#define SL_STATUS_SI91X_AP_HT_CAPS_NOT_ENABLEDValue:
((sl_status_t)0x10060)
AP HT caps not enabled.
SL_STATUS_SI91X_ADDRESS_FAMILY_NOT_SUPPORTED#
#define SL_STATUS_SI91X_ADDRESS_FAMILY_NOT_SUPPORTEDValue:
((sl_status_t)0x10061)
Address family not supported by protocol.
SL_STATUS_SI91X_INVALID_BEACON_INTERVAL_OR_DTM_PERIOD#
#define SL_STATUS_SI91X_INVALID_BEACON_INTERVAL_OR_DTM_PERIODValue:
((sl_status_t)0x10062)
Invalid beacon interval or DTIM period provided.
SL_STATUS_SI91X_INVALID_CONFIG_RANGE_PROVIDED#
#define SL_STATUS_SI91X_INVALID_CONFIG_RANGE_PROVIDEDValue:
((sl_status_t)0x10063)
Invalid range of the configuration provided.
SL_STATUS_SI91X_INVALID_CONFIG_TYPE#
#define SL_STATUS_SI91X_INVALID_CONFIG_TYPEValue:
((sl_status_t)0x10064)
RTS THRESHOLD Config type is invalid.
SL_STATUS_SI91X_ERROR_WITH_MQTT_COMMAND#
#define SL_STATUS_SI91X_ERROR_WITH_MQTT_COMMANDValue:
((sl_status_t)0x10065)
Error with MQTT command.
SL_STATUS_SI91X_HIGHER_LISTEN_INTERVAL#
#define SL_STATUS_SI91X_HIGHER_LISTEN_INTERVALValue:
((sl_status_t)0x10066)
listen interval in power save is greater than that of join.
SL_STATUS_SI91X_WLAN_RADIO_DEREGISTERED#
#define SL_STATUS_SI91X_WLAN_RADIO_DEREGISTEREDValue:
((sl_status_t)0x10067)
WLAN radio deregistered.
SL_STATUS_SI91X_SAE_FAILURE_DUE_TO_MULTIPLE_CONFIRM_FRAMES_FROM_AP#
#define SL_STATUS_SI91X_SAE_FAILURE_DUE_TO_MULTIPLE_CONFIRM_FRAMES_FROM_APValue:
((sl_status_t)0x10069)
SAE failure due to multiple confirm frames from AP.
SL_STATUS_SI91X_EC_GROUP_STATION_UNSUPPORTED_BY_AP#
#define SL_STATUS_SI91X_EC_GROUP_STATION_UNSUPPORTED_BY_APValue:
((sl_status_t)0x1006A)
AP does not support the EC-group set by station.
SL_STATUS_TWT_SUPPORT_NOT_ENABLED_ERR#
#define SL_STATUS_TWT_SUPPORT_NOT_ENABLED_ERRValue:
((sl_status_t)0x10070)
Occurs when HE_PARAMS_SUPPORT and SLI_SI91X_ENABLE_TWT_FEATURE macros are not enabled.
SL_STATUS_TWT_SETUP_ERR_SESSION_ACTIVE#
#define SL_STATUS_TWT_SETUP_ERR_SESSION_ACTIVEValue:
((sl_status_t)0x10071)
Occurs when user tries to give TWT config command when there is an already active TWT session.
SL_STATUS_TWT_TEARDOWN_ERR_FLOWID_NOT_MATCHED#
#define SL_STATUS_TWT_TEARDOWN_ERR_FLOWID_NOT_MATCHEDValue:
((sl_status_t)0x10072)
Occurs when TWT teardown command is given with a flow ID that does not match existing session flow ID.
SL_STATUS_TWT_TEARDOWN_ERR_NOACTIVE_SESS#
#define SL_STATUS_TWT_TEARDOWN_ERR_NOACTIVE_SESSValue:
((sl_status_t)0x10073)
Occurs when teardown command is given while there is no active session.
SL_STATUS_TWT_SESSION_NOT_FEASIBLE#
#define SL_STATUS_TWT_SESSION_NOT_FEASIBLEValue:
((sl_status_t)0x10074)
This error code indicates that TWT session is not feasible. It is thrown only when TWT Auto Selection API is used.
SL_STATUS_SI91X_RESCHEDULE_TWT_NOT_SUPPORTED#
#define SL_STATUS_SI91X_RESCHEDULE_TWT_NOT_SUPPORTEDValue:
((sl_status_t)0x10075)
AP does not support TWT information frame reception.
SL_STATUS_SI91X_RESCHEDULE_TWT_ERR_NOACTIVE_SESS#
#define SL_STATUS_SI91X_RESCHEDULE_TWT_ERR_NOACTIVE_SESSValue:
((sl_status_t)0x10076)
No active TWT agreement corresponding to given flow id.
SL_STATUS_SI91X_TWT_RESCHEDULING_IN_PROGRESS#
#define SL_STATUS_SI91X_TWT_RESCHEDULING_IN_PROGRESSValue:
((sl_status_t)0x10077)
Suspend or resume TWT action is in progress.
SL_STATUS_SI91X_RESCHEDULE_TWT_PACKET_CREATION_FAILED#
#define SL_STATUS_SI91X_RESCHEDULE_TWT_PACKET_CREATION_FAILEDValue:
((sl_status_t)0x10078)
TWT information frame packet creation failed in firmware.
SL_STATUS_SI91X_INVALID_STATION_TSF#
#define SL_STATUS_SI91X_INVALID_STATION_TSFValue:
((sl_status_t)0x10079)
Invalid station TSF error returned when station is not connected or atleast one beacon is not received.
SL_STATUS_SI91X_MQTT_ERROR_UNACCEPTABLE_PROTOCOL#
#define SL_STATUS_SI91X_MQTT_ERROR_UNACCEPTABLE_PROTOCOLValue:
((sl_status_t)0x10081)
The Server does not support the level of the MQTT protocol requested by the Client.
SL_STATUS_SI91X_MQTT_ERROR_IDENTIFIER_REJECTED#
#define SL_STATUS_SI91X_MQTT_ERROR_IDENTIFIER_REJECTEDValue:
((sl_status_t)0x10082)
The Client identifier is correct UTF-8 but not allowed by the Server.
SL_STATUS_SI91X_MQTT_ERROR_SERVER_UNAVAILABLE
#define SL_STATUS_SI91X_MQTT_ERROR_SERVER_UNAVAILABLEValue:
((sl_status_t)0x10083)
The Network Connection has been made but the MQTT service is unavailable.
SL_STATUS_SI91X_MQTT_ERROR_BAD_USERNAME_PASSWORD#
#define SL_STATUS_SI91X_MQTT_ERROR_BAD_USERNAME_PASSWORDValue:
((sl_status_t)0x10084)
The data in the user name or password is malformed.
SL_STATUS_SI91X_MQTT_ERROR_NOT_AUTHORIZED
#define SL_STATUS_SI91X_MQTT_ERROR_NOT_AUTHORIZEDValue:
((sl_status_t)0x10085)
The Client is not authorized to connect.
SL_STATUS_SI91X_SA_QUERY_TIMEOUT#
#define SL_STATUS_SI91X_SA_QUERY_TIMEOUTValue:
((sl_status_t)0x10086)
Disconnection due to SA Query Timeout.
SL_STATUS_SI91X_DUPLICATE_ENTRY_EXISTS_IN_DNS_SERVER_TABLE#
#define SL_STATUS_SI91X_DUPLICATE_ENTRY_EXISTS_IN_DNS_SERVER_TABLEValue:
((sl_status_t)0x100AF)
Duplicate entry exists in DNS server table.
SL_STATUS_SI91X_NO_MEM_AVAILABLE#
#define SL_STATUS_SI91X_NO_MEM_AVAILABLEValue:
((sl_status_t)0x100B1)
Memory error: No memory available.
SL_STATUS_SI91X_INVALID_CHARACTERS_IN_JSON_OBJECT#
#define SL_STATUS_SI91X_INVALID_CHARACTERS_IN_JSON_OBJECTValue:
((sl_status_t)0x100B2)
Invalid characters in JSON object.
SL_STATUS_SI91X_NO_KEY_FOUND#
#define SL_STATUS_SI91X_NO_KEY_FOUNDValue:
((sl_status_t)0x100B3)
Update commands: No such key found.
SL_STATUS_SI91X_NO_FILE_FOUND#
#define SL_STATUS_SI91X_NO_FILE_FOUNDValue:
((sl_status_t)0x100B4)
No such file found: Re-check filename.
SL_STATUS_SI91X_NO_WEB_PAGE_EXISTS_WITH_SAME_FILENAME#
#define SL_STATUS_SI91X_NO_WEB_PAGE_EXISTS_WITH_SAME_FILENAMEValue:
((sl_status_t)0x100B5)
No corresponding web page exists with same filename.
SL_STATUS_SI91X_SPACE_UNAVAILABLE_FOR_NEW_FILE
#define SL_STATUS_SI91X_SPACE_UNAVAILABLE_FOR_NEW_FILEValue:
((sl_status_t)0x100B6)
Space unavailable for new file.
SL_STATUS_SI91X_INVALID_INPUT_DATA#
#define SL_STATUS_SI91X_INVALID_INPUT_DATAValue:
((sl_status_t)0x100C1)
Invalid input data, Re-check filename, lengths, etc.
SL_STATUS_SI91X_NO_SPACE_AVAILABLE_FOR_NEW_FILE#
#define SL_STATUS_SI91X_NO_SPACE_AVAILABLE_FOR_NEW_FILEValue:
((sl_status_t)0x100C2)
Space unavailable for new file.
SL_STATUS_SI91X_EXISTING_FILE_OVERWRITE#
#define SL_STATUS_SI91X_EXISTING_FILE_OVERWRITEValue:
((sl_status_t)0x100C3)
Existing file overwrite: Exceeds size of previous file. Use erase and try again.
SL_STATUS_SI91X_NO_SUCH_FILE_FOUND#
#define SL_STATUS_SI91X_NO_SUCH_FILE_FOUNDValue:
((sl_status_t)0x100C4)
No such file found. Re-check filename.
SL_STATUS_SI91X_MEMORY_ERROR#
#define SL_STATUS_SI91X_MEMORY_ERRORValue:
((sl_status_t)0x100C5)
Memory Error: No memory available.
SL_STATUS_SI91X_RECEIVED_MORE_WEB_PAGE_DATA#
#define SL_STATUS_SI91X_RECEIVED_MORE_WEB_PAGE_DATAValue:
((sl_status_t)0x100C6)
Received more web page data than the total length initially specified.
SL_STATUS_SI91X_SET_REGION_ERROR#
#define SL_STATUS_SI91X_SET_REGION_ERRORValue:
((sl_status_t)0x100C7)
Error in set region command.
SL_STATUS_SI91X_INVALID_WEBPAGE_CURRENT_CHUNK_LEN#
#define SL_STATUS_SI91X_INVALID_WEBPAGE_CURRENT_CHUNK_LENValue:
((sl_status_t)0x100C8)
Web page current chunk length is incorrect.
SL_STATUS_SI91X_AP_SET_REGION_COMMAND_ERROR#
#define SL_STATUS_SI91X_AP_SET_REGION_COMMAND_ERRORValue:
((sl_status_t)0x100CA)
Error in AP set region command.
SL_STATUS_SI91X_AP_SET_REGION_COMMAND_PARAMETERS_ERROR#
#define SL_STATUS_SI91X_AP_SET_REGION_COMMAND_PARAMETERS_ERRORValue:
((sl_status_t)0x100CB)
Error in AP set region command parameters.
SL_STATUS_SI91X_REGION_CODE_NOT_SUPPORTED#
#define SL_STATUS_SI91X_REGION_CODE_NOT_SUPPORTEDValue:
((sl_status_t)0x100CC)
Region code not supported.
SL_STATUS_SI91X_EXTRACTING_COUNTRY_REGION_FROM_BEACON_FAILED#
#define SL_STATUS_SI91X_EXTRACTING_COUNTRY_REGION_FROM_BEACON_FAILEDValue:
((sl_status_t)0x100CD)
Error in extracting country region from beacon.
SL_STATUS_SI91X_SELECTED_REGION_NOT_SUPPORTED#
#define SL_STATUS_SI91X_SELECTED_REGION_NOT_SUPPORTEDValue:
((sl_status_t)0x100CE)
Device does not have selected region support.
SL_STATUS_SI91X_SSL_TLS_CONTEXT_CREATION_FAILED#
#define SL_STATUS_SI91X_SSL_TLS_CONTEXT_CREATION_FAILEDValue:
((sl_status_t)0x100D1)
SSL/TLS context create failed.
SL_STATUS_SI91X_SSL_TLS_HANDSHAKE_FAIL#
#define SL_STATUS_SI91X_SSL_TLS_HANDSHAKE_FAILValue:
((sl_status_t)0x100D2)
SSL/TLS handshake failed. Socket will be closed.
SL_STATUS_SI91X_SSL_TLS_MAX_SOCKETS_REACHED#
#define SL_STATUS_SI91X_SSL_TLS_MAX_SOCKETS_REACHEDValue:
((sl_status_t)0x100D3)
SSL/TLS max sockets reached.
SL_STATUS_SI91X_FTP_CLIENT_NOT_CONNECTED#
#define SL_STATUS_SI91X_FTP_CLIENT_NOT_CONNECTEDValue:
((sl_status_t)0x100D3)
FTP client is not connected.
SL_STATUS_SI91X_CIPHER_SET_FAILED#
#define SL_STATUS_SI91X_CIPHER_SET_FAILEDValue:
((sl_status_t)0x100D4)
Cipher set failure.
SL_STATUS_SI91X_HTTP_CREDENTIALS_MAX_LEN_EXCEEDED#
#define SL_STATUS_SI91X_HTTP_CREDENTIALS_MAX_LEN_EXCEEDEDValue:
((sl_status_t)0x100F1)
HTTP credentials maximum length exceeded.
SL_STATUS_SI91X_FEATURE_NOT_SUPPORTED#
#define SL_STATUS_SI91X_FEATURE_NOT_SUPPORTEDValue:
((sl_status_t)0x100F7)
Feature not supported.
SL_STATUS_SI91X_FLASH_WRITE_OR_FLASH_DATA_VERIFICATION_FAILED#
#define SL_STATUS_SI91X_FLASH_WRITE_OR_FLASH_DATA_VERIFICATION_FAILEDValue:
((sl_status_t)0x100F8)
Unable to write to flash OR flash data verification failed.
SL_STATUS_SI91X_CALIBRATION_DATA_VERIFICATION_FAILED#
#define SL_STATUS_SI91X_CALIBRATION_DATA_VERIFICATION_FAILEDValue:
((sl_status_t)0x100F9)
Calibration data verification failed.
SL_STATUS_SI91X_SNMP_INTERNAL_ERROR#
#define SL_STATUS_SI91X_SNMP_INTERNAL_ERRORValue:
((sl_status_t)0x10100)
SNMP internal error.
SL_STATUS_SI91X_SNMP_INVALID_IP_PROTOCOL#
#define SL_STATUS_SI91X_SNMP_INVALID_IP_PROTOCOLValue:
((sl_status_t)0x10104)
SNMP invalid IP protocol error.
SL_STATUS_SI91X_NO_DATA_RECEIVED_OR_RECEIVE_TIMEOUT#
#define SL_STATUS_SI91X_NO_DATA_RECEIVED_OR_RECEIVE_TIMEOUTValue:
((sl_status_t)0x1BB01)
No data received or receive timeout.
SL_STATUS_SI91X_INSUFFICIENT_DATA_FOR_TIME_CONVERSION#
#define SL_STATUS_SI91X_INSUFFICIENT_DATA_FOR_TIME_CONVERSIONValue:
((sl_status_t)0x1BB08)
Insufficient data for converting NTP time to mm-dd-yy time format.
SL_STATUS_SI91X_INVALID_SNTP_SERVER_ADDRESS#
#define SL_STATUS_SI91X_INVALID_SNTP_SERVER_ADDRESSValue:
((sl_status_t)0x1BB0A)
Invalid SNTP server address.
SL_STATUS_SI91X_SNTP_CLIENT_NOT_STARTED#
#define SL_STATUS_SI91X_SNTP_CLIENT_NOT_STARTEDValue:
((sl_status_t)0x1BB0B)
SNTP client not started.
SL_STATUS_SI91X_SNTP_SERVER_UNAVAILABLE
#define SL_STATUS_SI91X_SNTP_SERVER_UNAVAILABLEValue:
((sl_status_t)0x1BB10)
SNTP server not available. Client will not get any time update service from current server.
SL_STATUS_SI91X_SNTP_SERVER_AUTHENTICATION_FAILED#
#define SL_STATUS_SI91X_SNTP_SERVER_AUTHENTICATION_FAILEDValue:
((sl_status_t)0x1BB15)
SNTP server authentication failed.
SL_STATUS_SI91X_INTERNAL_ERROR#
#define SL_STATUS_SI91X_INTERNAL_ERRORValue:
((sl_status_t)0x1BB0E)
Internal error.
SL_STATUS_SI91X_MULTICAST_IP_ADDRESS_ENTRY_NOT_FOUND#
#define SL_STATUS_SI91X_MULTICAST_IP_ADDRESS_ENTRY_NOT_FOUNDValue:
((sl_status_t)0x1BB16)
Entry not found for multicast IP address.
SL_STATUS_SI91X_MULTICAST_NO_ENTRIES_FOUND#
#define SL_STATUS_SI91X_MULTICAST_NO_ENTRIES_FOUNDValue:
((sl_status_t)0x1BB17)
No more entries found for multicast.
SL_STATUS_SI91X_IP_ADDRESS_ERROR#
#define SL_STATUS_SI91X_IP_ADDRESS_ERRORValue:
((sl_status_t)0x1BB21)
IP address error.
SL_STATUS_SI91X_SOCKET_ALREADY_BOUND#
#define SL_STATUS_SI91X_SOCKET_ALREADY_BOUNDValue:
((sl_status_t)0x1BB22)
Socket already bound.
SL_STATUS_SI91X_PORT_UNAVAILABLE
#define SL_STATUS_SI91X_PORT_UNAVAILABLEValue:
((sl_status_t)0x1BB23)
Port not available.
SL_STATUS_SI91X_SOCKET_NOT_CREATED#
#define SL_STATUS_SI91X_SOCKET_NOT_CREATEDValue:
((sl_status_t)0x1BB27)
Socket is not created.
SL_STATUS_SI91X_ICMP_REQUEST_FAILED#
#define SL_STATUS_SI91X_ICMP_REQUEST_FAILEDValue:
((sl_status_t)0x1BB29)
ICMP request failed.
SL_STATUS_SI91X_MAX_LISTEN_SOCKETS_REACHED#
#define SL_STATUS_SI91X_MAX_LISTEN_SOCKETS_REACHEDValue:
((sl_status_t)0x1BB33)
Maximum listen sockets reached.
SL_STATUS_SI91X_DHCP_DUPLICATE_LISTEN#
#define SL_STATUS_SI91X_DHCP_DUPLICATE_LISTENValue:
((sl_status_t)0x1BB34)
DHCP duplicate listen.
SL_STATUS_SI91X_PORT_NOT_IN_CLOSE_STATE#
#define SL_STATUS_SI91X_PORT_NOT_IN_CLOSE_STATEValue:
((sl_status_t)0x1BB35)
Port not in closed state.
SL_STATUS_SI91X_SOCKET_CLOSED#
#define SL_STATUS_SI91X_SOCKET_CLOSEDValue:
((sl_status_t)0x1BB36)
Socket is closed or in process of closing.
SL_STATUS_SI91X_PROCESS_IN_PROGRESS#
#define SL_STATUS_SI91X_PROCESS_IN_PROGRESSValue:
((sl_status_t)0x1BB37)
Process in progress.
SL_STATUS_SI91X_CONNECT_TO_NON_EXISTING_TCP_SERVER_SOCKET#
#define SL_STATUS_SI91X_CONNECT_TO_NON_EXISTING_TCP_SERVER_SOCKETValue:
((sl_status_t)0x1BB38)
Trying to connect non-existing TCP server socket.
SL_STATUS_SI91X_ERROR_IN_LEN_OF_THE_COMMAND#
#define SL_STATUS_SI91X_ERROR_IN_LEN_OF_THE_COMMANDValue:
((sl_status_t)0x1BB3E)
Error in length of the command ('Exceeds number of characters' is mentioned in the PRM).
SL_STATUS_SI91X_WRONG_PACKET_INFO#
#define SL_STATUS_SI91X_WRONG_PACKET_INFOValue:
((sl_status_t)0x1BB40)
Wrong packet info.
SL_STATUS_SI91X_SOCKET_STILL_BOUND#
#define SL_STATUS_SI91X_SOCKET_STILL_BOUNDValue:
((sl_status_t)0x1BB42)
Socket is still bound.
SL_STATUS_SI91X_NO_FREE_PORT#
#define SL_STATUS_SI91X_NO_FREE_PORTValue:
((sl_status_t)0x1BB45)
No free port.
SL_STATUS_SI91X_INVALID_PORT#
#define SL_STATUS_SI91X_INVALID_PORTValue:
((sl_status_t)0x1BB46)
Invalid port.
SL_STATUS_SI91X_FEATURE_UNSUPPORTED#
#define SL_STATUS_SI91X_FEATURE_UNSUPPORTEDValue:
((sl_status_t)0x1BB4B)
Feature not supported.
SL_STATUS_SI91X_SOCKET_IN_UNCONNECTED_STATE#
#define SL_STATUS_SI91X_SOCKET_IN_UNCONNECTED_STATEValue:
((sl_status_t)0x1BB50)
Socket is not in connected state. Disconnected from server. In case of FTP, user need to give destroy command after receiving this error.
SL_STATUS_SI91X_POP3_SESSION_CREATION_FAILED#
#define SL_STATUS_SI91X_POP3_SESSION_CREATION_FAILEDValue:
((sl_status_t)0x1BB87)
POP3 session creation failed / POP3 session got terminated.
SL_STATUS_SI91X_DHCPV6_HANDSHAKE_FAIL#
#define SL_STATUS_SI91X_DHCPV6_HANDSHAKE_FAILValue:
((sl_status_t)0x1BB9C)
DHCPv6 handshake failure.
SL_STATUS_SI91X_DHCP_INVALID_IP_RESPONSE#
#define SL_STATUS_SI91X_DHCP_INVALID_IP_RESPONSEValue:
((sl_status_t)0x1BB9D)
DHCP invalid IP response.
SL_STATUS_SI91X_SMTP_AUTHENTICATION_ERROR#
#define SL_STATUS_SI91X_SMTP_AUTHENTICATION_ERRORValue:
((sl_status_t)0x1BBA0)
SMTP authentication error.
SL_STATUS_SI91X_SMTP_OVER_SIZE_MAIL_DATA#
#define SL_STATUS_SI91X_SMTP_OVER_SIZE_MAIL_DATAValue:
((sl_status_t)0x1BBA1)
No DNS server was specified, SMTP over size mail data.
SL_STATUS_SI91X_SMTP_INVALID_SERVER_REPLY#
#define SL_STATUS_SI91X_SMTP_INVALID_SERVER_REPLYValue:
((sl_status_t)0x1BBA2)
SMTP invalid server reply.
SL_STATUS_SI91X_SMTP_DNS_QUERY_FAILED#
#define SL_STATUS_SI91X_SMTP_DNS_QUERY_FAILEDValue:
((sl_status_t)0x1BBA3)
DNS query failed, SMTP internal error.
SL_STATUS_SI91X_SMTP_BAD_DNS_ADDRESS#
#define SL_STATUS_SI91X_SMTP_BAD_DNS_ADDRESSValue:
((sl_status_t)0x1BBA4)
Bad DNS address, SMTP server error code received.
SL_STATUS_SI91X_SMTP_INVALID_PARAMETERS#
#define SL_STATUS_SI91X_SMTP_INVALID_PARAMETERSValue:
((sl_status_t)0x1BBA5)
SMTP invalid parameters.
SL_STATUS_SI91X_SMTP_PACKET_ALLOCATION_FAILED#
#define SL_STATUS_SI91X_SMTP_PACKET_ALLOCATION_FAILEDValue:
((sl_status_t)0x1BBA6)
SMTP packet allocation failed.
SL_STATUS_SI91X_SMTP_GREET_REPLY_FAILED#
#define SL_STATUS_SI91X_SMTP_GREET_REPLY_FAILEDValue:
((sl_status_t)0x1BBA7)
SMTP Greet reply failed.
SL_STATUS_SI91X_SMTP_PARAMETER_ERROR#
#define SL_STATUS_SI91X_SMTP_PARAMETER_ERRORValue:
((sl_status_t)0x1BBA8)
Parameter error, SMTP hello reply error.
SL_STATUS_SI91X_SMTP_MAIL_REPLY_ERROR#
#define SL_STATUS_SI91X_SMTP_MAIL_REPLY_ERRORValue:
((sl_status_t)0x1BBA9)
SMTP mail reply error.
SL_STATUS_SI91X_SMTP_RCPT_REPLY_ERROR#
#define SL_STATUS_SI91X_SMTP_RCPT_REPLY_ERRORValue:
((sl_status_t)0x1BBAA)
SMTP RCPT reply error.
SL_STATUS_SI91X_SMTP_MESSAGE_REPLY_ERROR#
#define SL_STATUS_SI91X_SMTP_MESSAGE_REPLY_ERRORValue:
((sl_status_t)0x1BBAB)
SMTP message reply error.
SL_STATUS_SI91X_SMTP_DATA_REPLY_ERROR#
#define SL_STATUS_SI91X_SMTP_DATA_REPLY_ERRORValue:
((sl_status_t)0x1BBAC)
SMTP data reply error.
SL_STATUS_SI91X_SMTP_AUTH_REPLY_ERROR#
#define SL_STATUS_SI91X_SMTP_AUTH_REPLY_ERRORValue:
((sl_status_t)0x1BBAD)
SMTP authentication reply error.
SL_STATUS_SI91X_SMTP_SERVER_REPLY_ERROR#
#define SL_STATUS_SI91X_SMTP_SERVER_REPLY_ERRORValue:
((sl_status_t)0x1BBAE)
SMTP server error reply.
SL_STATUS_SI91X_DNS_DUPLICATE_ENTRY#
#define SL_STATUS_SI91X_DNS_DUPLICATE_ENTRYValue:
((sl_status_t)0x1BBAF)
DNS duplicate entry.
SL_STATUS_SI91X_SMTP_OVERSIZE_SERVER_REPLY#
#define SL_STATUS_SI91X_SMTP_OVERSIZE_SERVER_REPLYValue:
((sl_status_t)0x1BBB1)
SMTP oversize server reply.
SL_STATUS_SI91X_SMTP_CLIENT_NOT_INITIALIZED#
#define SL_STATUS_SI91X_SMTP_CLIENT_NOT_INITIALIZEDValue:
((sl_status_t)0x1BBB2)
SMTP client not initialized.
SL_STATUS_SI91X_DNS_IPV6_NOT_SUPPORTED#
#define SL_STATUS_SI91X_DNS_IPV6_NOT_SUPPORTEDValue:
((sl_status_t)0x1BBB3)
DNS IPv6 not supported.
SL_STATUS_SI91X_INVALID_MAIL_INDEX_FOR_POP3_MAIL_RETRIEVE_COMMAND#
#define SL_STATUS_SI91X_INVALID_MAIL_INDEX_FOR_POP3_MAIL_RETRIEVE_COMMANDValue:
((sl_status_t)0x1BBC5)
Invalid mail index for POP3 mail retrieve command.
SL_STATUS_SI91X_SSL_TLS_HANDSHAKE_FAILED#
#define SL_STATUS_SI91X_SSL_TLS_HANDSHAKE_FAILEDValue:
((sl_status_t)0x1BBD2)
SSL/TLS handshake failed.
SL_STATUS_SI91X_FTP_CLIENT_DISCONNECTED#
#define SL_STATUS_SI91X_FTP_CLIENT_DISCONNECTEDValue:
((sl_status_t)0x1BBD3)
FTP client is not connected or disconnected with the FTP server.
SL_STATUS_SI91X_FTP_CLIENT_NOT_DISCONNECTED#
#define SL_STATUS_SI91X_FTP_CLIENT_NOT_DISCONNECTEDValue:
((sl_status_t)0x1BBD4)
FTP client is not disconnected.
SL_STATUS_SI91X_FTP_FILE_NOT_OPENED#
#define SL_STATUS_SI91X_FTP_FILE_NOT_OPENEDValue:
((sl_status_t)0x1BBD5)
FTP file is not opened.
SL_STATUS_SI91X_SSL_TLS_HANDSHAKE_TIMEOUT_OR_FTP_FILE_NOT_CLOSED#
#define SL_STATUS_SI91X_SSL_TLS_HANDSHAKE_TIMEOUT_OR_FTP_FILE_NOT_CLOSEDValue:
((sl_status_t)0x1BBD6)
SSL/TLS handshake timeout or FTP file is not closed.
SL_STATUS_SI91X_FTP_EXPECTED_1XX_RESPONSE_NOT_RECEIVED#
#define SL_STATUS_SI91X_FTP_EXPECTED_1XX_RESPONSE_NOT_RECEIVEDValue:
((sl_status_t)0x1BBD9)
Expected [1XX response from FTP server but not received].
SL_STATUS_SI91X_FTP_EXPECTED_2XX_RESPONSE_NOT_RECEIVED#
#define SL_STATUS_SI91X_FTP_EXPECTED_2XX_RESPONSE_NOT_RECEIVEDValue:
((sl_status_t)0x1BBDA)
Expected [2XX response from FTP server but not received].
SL_STATUS_SI91X_FTP_EXPECTED_22X_RESPONSE_NOT_RECEIVED#
#define SL_STATUS_SI91X_FTP_EXPECTED_22X_RESPONSE_NOT_RECEIVEDValue:
((sl_status_t)0x1BBDB)
Expected [22X response from FTP server but not received].
SL_STATUS_SI91X_FTP_EXPECTED_23X_RESPONSE_NOT_RECEIVED#
#define SL_STATUS_SI91X_FTP_EXPECTED_23X_RESPONSE_NOT_RECEIVEDValue:
((sl_status_t)0x1BBDC)
Expected [23X response from FTP server but not received].
SL_STATUS_SI91X_FTP_EXPECTED_3XX_RESPONSE_NOT_RECEIVED#
#define SL_STATUS_SI91X_FTP_EXPECTED_3XX_RESPONSE_NOT_RECEIVEDValue:
((sl_status_t)0x1BBDD)
Expected [3XX response from FTP server but not received].
SL_STATUS_SI91X_FTP_EXPECTED_33X_RESPONSE_NOT_RECEIVED#
#define SL_STATUS_SI91X_FTP_EXPECTED_33X_RESPONSE_NOT_RECEIVEDValue:
((sl_status_t)0x1BBDE)
Expected [33X response from FTP server but not received].
SL_STATUS_SI91X_HTTP_TIMEOUT#
#define SL_STATUS_SI91X_HTTP_TIMEOUTValue:
((sl_status_t)0x1BBE1)
HTTP timeout.
SL_STATUS_SI91X_HTTP_FAILED#
#define SL_STATUS_SI91X_HTTP_FAILEDValue:
((sl_status_t)0x1BBE2)
HTTP failed.
SL_STATUS_SI91X_HTTP_PUT_CLIENT_TIMEOUT#
#define SL_STATUS_SI91X_HTTP_PUT_CLIENT_TIMEOUTValue:
((sl_status_t)0x1BBE7)
HTTP timeout for HTTP PUT client.
SL_STATUS_SI91X_AUTHENTICATION_ERROR#
#define SL_STATUS_SI91X_AUTHENTICATION_ERRORValue:
((sl_status_t)0x1BBEB)
Authentication error.
SL_STATUS_SI91X_INVALID_PACKET_LENGTH#
#define SL_STATUS_SI91X_INVALID_PACKET_LENGTHValue:
((sl_status_t)0x1BBED)
Invalid packet length. Content length and received data length is mismatching.
SL_STATUS_SI91X_SERVER_RESPONDS_BEFORE_REQUEST_COMPLETE#
#define SL_STATUS_SI91X_SERVER_RESPONDS_BEFORE_REQUEST_COMPLETEValue:
((sl_status_t)0x1BBEF)
Server responds before HTTP client request is complete.
SL_STATUS_SI91X_HTTP_PASSWORD_TOO_LONG#
#define SL_STATUS_SI91X_HTTP_PASSWORD_TOO_LONGValue:
((sl_status_t)0x1BBF0)
HTTP/HTTPS password is too long.
SL_STATUS_SI91X_MQTT_PING_TIMEOUT#
#define SL_STATUS_SI91X_MQTT_PING_TIMEOUTValue:
((sl_status_t)0x1BBF1)
MQTT ping time out error.
SL_STATUS_SI91X_MQTT_COMMAND_SENT_IN_INCORRECT_STATE#
#define SL_STATUS_SI91X_MQTT_COMMAND_SENT_IN_INCORRECT_STATEValue:
((sl_status_t)0x1BBF2)
MQTT command sent in incorrect state.
SL_STATUS_SI91X_MQTT_ACK_TIMEOUT#
#define SL_STATUS_SI91X_MQTT_ACK_TIMEOUTValue:
((sl_status_t)0x1BBF3)
MQTT ACK time out error.
SL_STATUS_SI91X_POP3_INVALID_MAIL_INDEX#
#define SL_STATUS_SI91X_POP3_INVALID_MAIL_INDEXValue:
((sl_status_t)0x1BBFF)
POP3 error for invalid mail index.
SL_STATUS_SI91X_SOCKET_NOT_CONNECTED#
#define SL_STATUS_SI91X_SOCKET_NOT_CONNECTEDValue:
((sl_status_t)0x1FFFF)
Listening TCP socket in device is not connected to the remote peer, or the LTCP socket is not yet opened in the device.
SL_STATUS_SI91X_SOCKET_LIMIT_EXCEEDED#
#define SL_STATUS_SI91X_SOCKET_LIMIT_EXCEEDEDValue:
((sl_status_t)0x1FFFE)
Sockets not available. The error comes if the host tries to open more than 10 sockets.
SL_STATUS_SI91X_HTTP_OTAF_INVALID_PACKET#
#define SL_STATUS_SI91X_HTTP_OTAF_INVALID_PACKETValue:
((sl_status_t)0x1FFFD)
HTTP OTAF invalid packet.
SL_STATUS_SI91X_TCP_IP_INIT_FAILED#
#define SL_STATUS_SI91X_TCP_IP_INIT_FAILEDValue:
((sl_status_t)0x1FFFC)
TCP_IP initialization failed.
SL_STATUS_SI91X_CONCURRENT_IP_CREATION_ERROR#
#define SL_STATUS_SI91X_CONCURRENT_IP_CREATION_ERRORValue:
((sl_status_t)0x1FFFB)
Cannot create IP in same interface in concurrent mode.
SL_STATUS_SI91X_HTTP_OTAF_INCOMPLETE_PACKET#
#define SL_STATUS_SI91X_HTTP_OTAF_INCOMPLETE_PACKETValue:
((sl_status_t)0x1FFF4)
HTTP OTAF incomplete packet.
SL_STATUS_SI91X_INVALID_STORE_CONFIGURATION_PROFILE#
#define SL_STATUS_SI91X_INVALID_STORE_CONFIGURATION_PROFILEValue:
((sl_status_t)0x1FFF5)
Store configuration profile type mismatch or invalid profile type.
SL_STATUS_SI91X_MQTT_REMOTE_TERMINATE_ERROR#
#define SL_STATUS_SI91X_MQTT_REMOTE_TERMINATE_ERRORValue:
((sl_status_t)0x1FFF6)
MQTT remote terminate error.
SL_STATUS_SI91X_BYTE_STUFFING_ERROR_IN_AT_MODE#
#define SL_STATUS_SI91X_BYTE_STUFFING_ERROR_IN_AT_MODEValue:
((sl_status_t)0x1FFF7)
Byte stuffing error in AT mode.
SL_STATUS_SI91X_INVALID_COMMAND_OR_OPERATION#
#define SL_STATUS_SI91X_INVALID_COMMAND_OR_OPERATIONValue:
((sl_status_t)0x1FFF8)
Invalid command (e.g. parameters insufficient or invalid in the command). Invalid operation (e.g. power save command with the same mode given twice, accessing wrong socket, creating more than allowed sockets ).
SL_STATUS_SI91X_HTTP_OTAF_NO_PACKET#
#define SL_STATUS_SI91X_HTTP_OTAF_NO_PACKETValue:
((sl_status_t)0x1FFF9)
HTTP OTAF no packet.
SL_STATUS_SI91X_TCP_SOCKET_NOT_CONNECTED#
#define SL_STATUS_SI91X_TCP_SOCKET_NOT_CONNECTEDValue:
((sl_status_t)0x1FFFA)
TCP socket is not connected.
SL_STATUS_SI91X_MAX_STATION_COUNT_EXCEEDED#
#define SL_STATUS_SI91X_MAX_STATION_COUNT_EXCEEDEDValue:
((sl_status_t)0x1FFC5)
Station count exceeded max station supported.
SL_STATUS_SI91X_UNABLE_TO_SEND_TCP_DATA#
#define SL_STATUS_SI91X_UNABLE_TO_SEND_TCP_DATAValue:
((sl_status_t)0x1FFC4)
Unable to send TCP data.
SL_STATUS_SI91X_SOCKET_BUFFER_TOO_SMALL#
#define SL_STATUS_SI91X_SOCKET_BUFFER_TOO_SMALLValue:
((sl_status_t)0x1FFBC)
Socket buffer too small.
SL_STATUS_SI91X_INVALID_CONTENT_IN_DNS_RESPONSE#
#define SL_STATUS_SI91X_INVALID_CONTENT_IN_DNS_RESPONSEValue:
((sl_status_t)0x1FFBB)
Invalid content in the DNS response to the DNS resolution query.
SL_STATUS_SI91X_DNS_CLASS_ERROR_IN_DNS_RESPONSE#
#define SL_STATUS_SI91X_DNS_CLASS_ERROR_IN_DNS_RESPONSEValue:
((sl_status_t)0x1FFBA)
DNS class error in response to the DNS resolution query.
SL_STATUS_SI91X_DNS_COUNT_ERROR_IN_DNS_RESPONSE#
#define SL_STATUS_SI91X_DNS_COUNT_ERROR_IN_DNS_RESPONSEValue:
((sl_status_t)0x1FFB8)
DNS count error in response to the DNS resolution query.
SL_STATUS_SI91X_DNS_RETURN_CODE_ERROR_IN_DNS_RESPONSE#
#define SL_STATUS_SI91X_DNS_RETURN_CODE_ERROR_IN_DNS_RESPONSEValue:
((sl_status_t)0x1FFB7)
DNS return code error in the response to the DNS resolution query.
SL_STATUS_SI91X_DNS_OPCODE_ERROR_IN_DNS_RESPONSE#
#define SL_STATUS_SI91X_DNS_OPCODE_ERROR_IN_DNS_RESPONSEValue:
((sl_status_t)0x1FFB6)
DNS Opcode error in the response to the DNS resolution query.
SL_STATUS_SI91X_DNS_ID_MISMATCH#
#define SL_STATUS_SI91X_DNS_ID_MISMATCHValue:
((sl_status_t)0x1FFB5)
DNS id mismatch between DNS resolution request and response.
SL_STATUS_SI91X_INVALID_INPUT_IN_DNS_QUERY#
#define SL_STATUS_SI91X_INVALID_INPUT_IN_DNS_QUERYValue:
((sl_status_t)0x1FFAB)
An invalid input to the DNS resolution query.
SL_STATUS_SI91X_DNS_RESPONSE_TIMEOUT#
#define SL_STATUS_SI91X_DNS_RESPONSE_TIMEOUTValue:
((sl_status_t)0x1FF42)
DNS response was timed out.
SL_STATUS_SI91X_ARP_REQUEST_FAILURE#
#define SL_STATUS_SI91X_ARP_REQUEST_FAILUREValue:
((sl_status_t)0x1FFA1)
ARP request failure.
SL_STATUS_SI91X_UNABLE_TO_UPDATE_TCP_WINDOW#
#define SL_STATUS_SI91X_UNABLE_TO_UPDATE_TCP_WINDOWValue:
((sl_status_t)0x1FF91)
Unable to update TCP window.
SL_STATUS_SI91X_DHCP_LEASE_EXPIRED#
#define SL_STATUS_SI91X_DHCP_LEASE_EXPIREDValue:
((sl_status_t)0x1FF9D)
DHCP lease time expired.
SL_STATUS_SI91X_DHCP_HANDSHAKE_FAILURE#
#define SL_STATUS_SI91X_DHCP_HANDSHAKE_FAILUREValue:
((sl_status_t)0x1FF9C)
DHCP handshake failure.
SL_STATUS_SI91X_WEBSOCKET_CREATION_FAILED#
#define SL_STATUS_SI91X_WEBSOCKET_CREATION_FAILEDValue:
((sl_status_t)0x1FF88)
This error is issued when WebSocket creation failed.
SL_STATUS_SI91X_TRYING_TO_CONNECT_NON_EXISTENT_TCP_SERVER_SOCKET#
#define SL_STATUS_SI91X_TRYING_TO_CONNECT_NON_EXISTENT_TCP_SERVER_SOCKETValue:
((sl_status_t)0x1FF87)
This error is issued when device tried to connect to a non-existent TCP server socket on the remote side.
SL_STATUS_SI91X_TRYING_TO_CLOSE_NON_EXISTENT_SOCKET#
#define SL_STATUS_SI91X_TRYING_TO_CLOSE_NON_EXISTENT_SOCKETValue:
((sl_status_t)0x1FF86)
This error is issued when tried to close non-existent socket. or invalid socket descriptor.
SL_STATUS_SI91X_INVALID_SOCKET_PARAMETERS#
#define SL_STATUS_SI91X_INVALID_SOCKET_PARAMETERSValue:
((sl_status_t)0x1FF85)
Invalid socket parameters.
SL_STATUS_SI91X_FEATURE_NOT_AVAILABLE#
#define SL_STATUS_SI91X_FEATURE_NOT_AVAILABLEValue:
((sl_status_t)0x1FF82)
Feature not supported.
SL_STATUS_SI91X_SOCKET_ALREADY_OPEN#
#define SL_STATUS_SI91X_SOCKET_ALREADY_OPENValue:
((sl_status_t)0x1FF81)
Socket already open.
SL_STATUS_SI91X_MAX_SOCKETS_EXCEEDED#
#define SL_STATUS_SI91X_MAX_SOCKETS_EXCEEDEDValue:
((sl_status_t)0x1FF80)
Attempt to open more than the maximum allowed number of sockets.
SL_STATUS_SI91X_DATA_LENGTH_EXCEEDS_MSS#
#define SL_STATUS_SI91X_DATA_LENGTH_EXCEEDS_MSSValue:
((sl_status_t)0x1FF7E)
Data length exceeds mss.
SL_STATUS_SI91X_IP_CONFLICT_ERROR#
#define SL_STATUS_SI91X_IP_CONFLICT_ERRORValue:
((sl_status_t)0x1FF75)
DUT unable to configure IP address due to IP conflict.
SL_STATUS_SI91X_FEATURE_NOT_ENABLED#
#define SL_STATUS_SI91X_FEATURE_NOT_ENABLEDValue:
((sl_status_t)0x1FF74)
Feature not enabled.
SL_STATUS_SI91X_DHCP_SERVER_NOT_SET#
#define SL_STATUS_SI91X_DHCP_SERVER_NOT_SETValue:
((sl_status_t)0x1FF73)
DHCP server not set in AP mode.
SL_STATUS_SI91X_AP_SET_REGION_PARAM_ERROR#
#define SL_STATUS_SI91X_AP_SET_REGION_PARAM_ERRORValue:
((sl_status_t)0x1FF71)
Error in AP set region command parameters.
SL_STATUS_SI91X_SSL_TLS_NOT_SUPPORTED#
#define SL_STATUS_SI91X_SSL_TLS_NOT_SUPPORTEDValue:
((sl_status_t)0x1FF70)
SSL/TLS not supported.
SL_STATUS_SI91X_JSON_NOT_SUPPORTED#
#define SL_STATUS_SI91X_JSON_NOT_SUPPORTEDValue:
((sl_status_t)0x1FF6F)
JSON not supported.
SL_STATUS_SI91X_INVALID_OPERATING_MODE#
#define SL_STATUS_SI91X_INVALID_OPERATING_MODEValue:
((sl_status_t)0x1FF6E)
Invalid operating mode.
SL_STATUS_SI91X_INVALID_SOCKET_CONFIG_PARAMS#
#define SL_STATUS_SI91X_INVALID_SOCKET_CONFIG_PARAMSValue:
((sl_status_t)0x1FF6D)
Invalid socket configuration parameters.
SL_STATUS_SI91X_WEBSOCKET_CREATION_TIMEOUT#
#define SL_STATUS_SI91X_WEBSOCKET_CREATION_TIMEOUTValue:
((sl_status_t)0x1FF6C)
Web socket creation timeout.
SL_STATUS_SI91X_PARAM_MAX_VALUE_EXCEEDED#
#define SL_STATUS_SI91X_PARAM_MAX_VALUE_EXCEEDEDValue:
((sl_status_t)0x1FF6B)
Parameter maximum allowed value is exceeded.
SL_STATUS_SI91X_SOCKET_READ_TIMEOUT#
#define SL_STATUS_SI91X_SOCKET_READ_TIMEOUTValue:
((sl_status_t)0x1FF6A)
Socket read timeout.
SL_STATUS_SI91X_INVALID_COMMAND_SEQUENCE#
#define SL_STATUS_SI91X_INVALID_COMMAND_SEQUENCEValue:
((sl_status_t)0x1FF69)
Invalid command in sequence.
SL_STATUS_SI91X_DNS_RESPONSE_TIMEOUT_ERROR#
#define SL_STATUS_SI91X_DNS_RESPONSE_TIMEOUT_ERRORValue:
((sl_status_t)0x1FF42)
DNS response timed out.
SL_STATUS_SI91X_HTTP_SOCKET_CREATION_FAILED#
#define SL_STATUS_SI91X_HTTP_SOCKET_CREATION_FAILEDValue:
((sl_status_t)0x1FF41)
HTTP socket creation failed.
SL_STATUS_SI91X_HTTP_GET_CMD_IN_PROGRESS#
#define SL_STATUS_SI91X_HTTP_GET_CMD_IN_PROGRESSValue:
((sl_status_t)0x10005)
HTTP GET command is in progress.
SL_STATUS_SI91X_TCP_CLOSE_BEFORE_RESPONSE_ERROR#
#define SL_STATUS_SI91X_TCP_CLOSE_BEFORE_RESPONSE_ERRORValue:
((sl_status_t)0x1FF40)
TCP socket close command is issued before getting the response of the previous close command.
SL_STATUS_SI91X_WAIT_ON_HOST_FEATURE_NOT_ENABLED#
#define SL_STATUS_SI91X_WAIT_ON_HOST_FEATURE_NOT_ENABLEDValue:
((sl_status_t)0x1FF36)
'Wait On Host' feature not enabled.
SL_STATUS_SI91X_STORE_CONFIG_CHECKSUM_INVALID#
#define SL_STATUS_SI91X_STORE_CONFIG_CHECKSUM_INVALIDValue:
((sl_status_t)0x1FF35)
Store configuration checksum validation failed.
SL_STATUS_SI91X_TCP_KEEP_ALIVE_TIMEOUT#
#define SL_STATUS_SI91X_TCP_KEEP_ALIVE_TIMEOUTValue:
((sl_status_t)0x1FF33)
TCP keep alive timed out.
SL_STATUS_SI91X_TCP_ACK_FAILED_FOR_SYN_ACK#
#define SL_STATUS_SI91X_TCP_ACK_FAILED_FOR_SYN_ACKValue:
((sl_status_t)0x1FF2D)
TCP ACK failed for TCP SYN-ACK.
SL_STATUS_SI91X_MEMORY_LIMIT_EXCEEDED#
#define SL_STATUS_SI91X_MEMORY_LIMIT_EXCEEDEDValue:
((sl_status_t)0x1FF2C)
Memory limit exceeded in a given operating mode.
SL_STATUS_SI91X_MEMORY_LIMIT_EXCEEDED_DURING_AUTO_JOIN#
#define SL_STATUS_SI91X_MEMORY_LIMIT_EXCEEDED_DURING_AUTO_JOINValue:
((sl_status_t)0x1FF2A)
Memory limit exceeded in an operating mode during auto join/create.
SL_STATUS_SI91X_PUF_OPERATION_BLOCKED#
#define SL_STATUS_SI91X_PUF_OPERATION_BLOCKEDValue:
((sl_status_t)0x1CC2F)
PUF operation is blocked.
SL_STATUS_SI91X_PUF_ACTIVATION_CODE_INVALID#
#define SL_STATUS_SI91X_PUF_ACTIVATION_CODE_INVALIDValue:
((sl_status_t)0x1CC31)
PUF activation code invalid.
SL_STATUS_SI91X_PUF_INPUT_PARAMETERS_INVALID#
#define SL_STATUS_SI91X_PUF_INPUT_PARAMETERS_INVALIDValue:
((sl_status_t)0x1CC32)
PUF input parameters invalid.
SL_STATUS_SI91X_PUF_IN_ERROR_STATE#
#define SL_STATUS_SI91X_PUF_IN_ERROR_STATEValue:
((sl_status_t)0x1CC33)
PUF in error state.
SL_STATUS_SI91X_PUF_OPERATION_NOT_ALLOWED#
#define SL_STATUS_SI91X_PUF_OPERATION_NOT_ALLOWEDValue:
((sl_status_t)0x1CC34)
PUF operation not allowed.
SL_STATUS_SI91X_PUF_OPERATION_FAILED#
#define SL_STATUS_SI91X_PUF_OPERATION_FAILEDValue:
((sl_status_t)0x1CC35)
PUF operation failed.
SL_STATUS_SI91X_AUTO_JOIN_IN_PROGRESS#
#define SL_STATUS_SI91X_AUTO_JOIN_IN_PROGRESSValue:
((sl_status_t)0x15A5A)
Auto join or user store configuration going on.
SL_STATUS_SI91X_RSNIE_FROM_AP_INVALID#
#define SL_STATUS_SI91X_RSNIE_FROM_AP_INVALIDValue:
((sl_status_t)0x1FFE1)
Improper RSNIE from AP to station.
SL_STATUS_SI91X_SNTP_MAX_ATTEMPTS_REACHED#
#define SL_STATUS_SI91X_SNTP_MAX_ATTEMPTS_REACHEDValue:
((sl_status_t)0x1FF5F)
Reached maximum SNTP invalid attempts.
SL_STATUS_SI91X_FREQUENCY_OFFSET_ZER0#
#define SL_STATUS_SI91X_FREQUENCY_OFFSET_ZER0Value:
((sl_status_t)0x100FC)
Frequency offset sent is zero.
SL_STATUS_SI91X_FREQUENCY_OFFSET_OUT_OF_LIMITS#
#define SL_STATUS_SI91X_FREQUENCY_OFFSET_OUT_OF_LIMITSValue:
((sl_status_t)0x100FB)
Frequency offset specified goes beyond upper or lower limits and indicates that frequency offset cannot be changed further.