MQTT Client credentials structure.
Public Attributes#
uint16_t
Length of the username. Length should not exceed 122 bytes including NULL termination character.
uint16_t
Length of the password. Length should not exceed 62 bytes including NULL termination character.
uint8_t
A flexible array to store both username and password.
Public Attribute Documentation#
username_length#
uint16_t sl_mqtt_client_credentials_t::username_length
Length of the username. Length should not exceed 122 bytes including NULL termination character.
Definition at line
134
of file components/service/mqtt/inc/sl_mqtt_client_types.h
password_length#
uint16_t sl_mqtt_client_credentials_t::password_length
Length of the password. Length should not exceed 62 bytes including NULL termination character.
Definition at line
136
of file components/service/mqtt/inc/sl_mqtt_client_types.h
data#
uint8_t sl_mqtt_client_credentials_t::data[]
A flexible array to store both username and password.
Definition at line
137
of file components/service/mqtt/inc/sl_mqtt_client_types.h