HTTP client request configurations.

Public Attributes#

uint8_t *

HTTP server IP address.

uint8_t *

URL string for requested resource.

uint16_t

HTTP server port number.

si91x_socket_type_length_value_t *

SNI extension address. si91x_socket_type_length_value_t.

uint8_t *

HTTP body to be sent to the server. Setting this to null will process the request in chunked encoding.

uint32_t

Body length of data to be posted. In case of chunked request, body length should be equal to total content length.

User-defined extended header. If null, default extended header will be added internally. sl_http_client_header_t.

uint16_t

HTTP request timeout period. (Si91x chipsets does not support this feature).

uint16_t

HTTP request maximum retry count after timeout. (Si91x chipsets does not support this feature).

uint16_t

Retry period after max retry count reach. (Si91x chipsets does not support this feature).

bool

Flag to use same TCP socket for connection. (Si91x chipsets does not support this feature).

void *

User defined context.

Public Attribute Documentation#

http_method_type#

sl_http_client_method_type_t sl_http_client_request_t::http_method_type

HTTP request method. sl_http_client_method_type_t.


ip_address#

uint8_t* sl_http_client_request_t::ip_address

HTTP server IP address.


resource#

uint8_t* sl_http_client_request_t::resource

URL string for requested resource.

The maximum supported HTTP URL is 2048 bytes, when the SL_SI91X_FEAT_LONG_HTTP_URL Bit is enabled in the feature_bit_map. If the SL_SI91X_FEAT_LONG_HTTP_URL Bit is disabled then the maximum supported length for HTTP URL is (872-(length of User_name + length of Password) - length of hostname - length of IP address) bytes excluding delimiters.


port#

uint16_t sl_http_client_request_t::port

HTTP server port number.


sni_extension#

si91x_socket_type_length_value_t* sl_http_client_request_t::sni_extension

SNI extension address. si91x_socket_type_length_value_t.


body#

uint8_t* sl_http_client_request_t::body

HTTP body to be sent to the server. Setting this to null will process the request in chunked encoding.


body_length#

uint32_t sl_http_client_request_t::body_length

Body length of data to be posted. In case of chunked request, body length should be equal to total content length.


extended_header#

sl_http_client_header_t* sl_http_client_request_t::extended_header

User-defined extended header. If null, default extended header will be added internally. sl_http_client_header_t.


timeout_ms#

uint16_t sl_http_client_request_t::timeout_ms

HTTP request timeout period. (Si91x chipsets does not support this feature).


retry_count#

uint16_t sl_http_client_request_t::retry_count

HTTP request maximum retry count after timeout. (Si91x chipsets does not support this feature).


retry_period_ms#

uint16_t sl_http_client_request_t::retry_period_ms

Retry period after max retry count reach. (Si91x chipsets does not support this feature).


tcp_connection_reuse#

bool sl_http_client_request_t::tcp_connection_reuse

Flag to use same TCP socket for connection. (Si91x chipsets does not support this feature).


context#

void* sl_http_client_request_t::context

User defined context.


event_handler#

sl_http_client_event_handler_t sl_http_client_request_t::event_handler

Callback method. sl_http_client_event_handler_t.