HTTP server configuration.

Public Attributes#

uint16_t

Port number of the HTTP server.

Array of request Handlers.

uint16_t

Length of request handlers Array.

Public Attribute Documentation#

port#

uint16_t sl_http_server_config_t::port

Port number of the HTTP server.


Definition at line 190 of file components/service/sl_http_server/inc/sl_http_server_types.h

handlers_list#

sl_http_server_handler_t* sl_http_server_config_t::handlers_list

Array of request Handlers.


Definition at line 191 of file components/service/sl_http_server/inc/sl_http_server_types.h

handlers_count#

uint16_t sl_http_server_config_t::handlers_count

Length of request handlers Array.


Definition at line 192 of file components/service/sl_http_server/inc/sl_http_server_types.h

default_handler#

sl_http_request_handler_t sl_http_server_config_t::default_handler

Default handler.


Definition at line 193 of file components/service/sl_http_server/inc/sl_http_server_types.h