Types#

This section provides a reference to the SNTP API data types.

Modules#

SL_ATTRIBUTE_PACKED

sl_sntp_client_response_t

sl_sntp_client_config_t

Typedefs#

typedef void(*
sl_sntp_client_event_handler_t)(sl_sntp_client_response_t *response, uint8_t *user_data, uint16_t user_data_length)

SNTP response handler.

typedef void(*
sl_sntp_set_time_sync_notification_handler_t)(const uint8_t cmd_type, sl_status_t status, const uint8_t *buffer)

SNTP time sync notification handler.

Typedef Documentation#

sl_sntp_client_event_handler_t#

sl_sntp_client_event_handler_t )(sl_sntp_client_response_t *response, uint8_t *user_data, uint16_t user_data_length)

SNTP response handler.

Parameters
TypeDirectionArgument NameDescription
[in]response

SNTP response of type sl_sntp_client_response_t

[in]user_data

User data passed in sl_sntp_client_get_time(), sl_sntp_client_get_time_date(), sl_sntp_client_get_server_info() APIs.

[in]user_data_length

User data length in sl_sntp_client_get_time(), sl_sntp_client_get_time_date(), sl_sntp_client_get_server_info() APIs


sl_sntp_set_time_sync_notification_handler_t#

sl_sntp_set_time_sync_notification_handler_t )(const uint8_t cmd_type, sl_status_t status, const uint8_t *buffer)

SNTP time sync notification handler.

Parameters
TypeDirectionArgument NameDescription
[in]cmd_type

command type

[in]status

sl_status_t.See https://docs.silabs.com/gecko-platform/4.1/common/api/group-status for details.

[in]buffer

Data buffer

Note

  • This features is not supported currently in Si917 chipsets