Public Attributes#

uint8_t

Scanning Status -.

uint8_t

Scanning type -.

uint8_t

To filter incoming advertising reports -.

uint8_t

Address type of the local device -.

uint16_t

Scan interval -.

uint16_t

Scan window -.

Public Attribute Documentation#

status#

uint8_t rsi_ble_req_scan_s::status

Scanning Status -.

  0 - disable 
  • 1 - enable


scan_type#

uint8_t rsi_ble_req_scan_s::scan_type

Scanning type -.

#define SCAN_TYPE_ACTIVE 0x01

  • #define SCAN_TYPE_PASSIVE 0x00


filter_type#

uint8_t rsi_ble_req_scan_s::filter_type

To filter incoming advertising reports -.

FILTERING_DISABLED = 0 (default)

  • ACCEPTLIST_FILTERING = 1 Note


own_addr_type#

uint8_t rsi_ble_req_scan_s::own_addr_type

Address type of the local device -.

  #define LE_PUBLIC_ADDRESS                  0x00 
  •   #define LE_RANDOM_ADDRESS                  0x01 
    
  •   #define LE_RESOLVABLE_PUBLIC_ADDRESS       0x02 
    
  •   #define LE_RESOLVABLE_RANDOM_ADDRESS       0x03  
    

scan_int#

uint16_t rsi_ble_req_scan_s::scan_int

Scan interval -.

 This is defined as the time interval from when the Controller started
 its last LE scan until it begins the subsequent LE scan. 
  •  Range: 0x0004 to 0x4000 
    

scan_win#

uint16_t rsi_ble_req_scan_s::scan_win

Scan window -.

  The duration of the LE scan. LE_Scan_Window shall be less than or equal to LE_Scan_Interval 
  •   Range: 0x0004 to 0x4000