Public Attributes#

uint16_t

Packet count of CRC fails (Cyclic Redundancy Check (CRC))

uint16_t

Packet count of CRC fails (Cyclic Redundancy Check (CRC))

uint16_t

Packet count of aborted Tx.

uint16_t

Packet count of dropped Rx.

uint16_t

Packet count of CCA Idle (Clear Channel Assessment (CCA))

uint16_t

Packet count of Rx start.

uint16_t

Packet count of aborted Rx.

uint16_t

Packet count of successful transmissions.

int8_t

Received Signal Strength Indicator of the packet.

uint16_t

Packet count of ID packets received.

uint16_t

Dummy array of length 5.

Public Attribute Documentation#

crc_fail_cnt#

uint16_t rsi_bt_per_stats_s::crc_fail_cnt

Packet count of CRC fails (Cyclic Redundancy Check (CRC))


crc_pass_cnt#

uint16_t rsi_bt_per_stats_s::crc_pass_cnt

Packet count of CRC fails (Cyclic Redundancy Check (CRC))


tx_abort_cnt#

uint16_t rsi_bt_per_stats_s::tx_abort_cnt

Packet count of aborted Tx.


rx_drop_cnt#

uint16_t rsi_bt_per_stats_s::rx_drop_cnt

Packet count of dropped Rx.


rx_cca_idle_cnt#

uint16_t rsi_bt_per_stats_s::rx_cca_idle_cnt

Packet count of CCA Idle (Clear Channel Assessment (CCA))


rx_start_idle_cnt#

uint16_t rsi_bt_per_stats_s::rx_start_idle_cnt

Packet count of Rx start.


rx_abrt_cnt#

uint16_t rsi_bt_per_stats_s::rx_abrt_cnt

Packet count of aborted Rx.


tx_dones#

uint16_t rsi_bt_per_stats_s::tx_dones

Packet count of successful transmissions.


rssi#

int8_t rsi_bt_per_stats_s::rssi

Received Signal Strength Indicator of the packet.


id_pkts_rcvd#

uint16_t rsi_bt_per_stats_s::id_pkts_rcvd

Packet count of ID packets received.


dummy#

uint16_t rsi_bt_per_stats_s::dummy[5]

Dummy array of length 5.