IP Addresses#
This section provides a reference to the IP Address module including functions, data types, and constants.
Modules#
Enumerations#
enum
enum
SL_IPV4 = (1 << 2)
SL_IPV6 = (1 << 3)
SL_IPV6_LINK_LOCAL = SL_IPV6 + 1
SL_IPV6_SITE_LOCAL = SL_IPV6 + 2
SL_IPV6_GLOBAL = SL_IPV6 + 3
SL_INVALID_IP = 0
}
Enumeration of IP address type.
enum
SL_IP_MANAGEMENT_STATIC_IP = 1
SL_IP_MANAGEMENT_DHCP
SL_IP_MANAGEMENT_LINK_LOCAL
}
Enumeration of IP Management type.
Enumeration Documentation#
sl_ip_address_type_t#
sl_ip_address_type_t
Enumeration of IP address type.
| Enumerator | |
|---|---|
| SL_IPV4 | IPv4. |
| SL_IPV6 | IPv6. Unspecified sub-type. |
| SL_IPV6_LINK_LOCAL | IPv6. Link local address. |
| SL_IPV6_SITE_LOCAL | IPv6. Site local address. |
| SL_IPV6_GLOBAL | IPv6. Global address. |
| SL_INVALID_IP | SL_INVALID_IP. |
sl_ip_management_t#
sl_ip_management_t
Enumeration of IP Management type.
| Enumerator | |
|---|---|
| SL_IP_MANAGEMENT_STATIC_IP | Assign STATIC IP address to an interface. |
| SL_IP_MANAGEMENT_DHCP | Assign IP address to an interface dynamically using DHCP. |
| SL_IP_MANAGEMENT_LINK_LOCAL | Assign IP address using link-local addressing. |