Constants#

This section provides a reference to the AES Crypto API constants.

Enumerations#

enum
SL_SI91X_AES_CBC = 1
SL_SI91X_AES_ECB
SL_SI91X_AES_CTR
}

Enumeration defining AES modes supported by the SI91X device.

enum
SL_SI91X_AES_ENCRYPT = 1
SL_SI91X_AES_DECRYPT
}

Enumeration defining AES encryption and decryption types.

enum
SL_SI91X_AES_KEY_SIZE_128 = 16
SL_SI91X_AES_KEY_SIZE_192 = 24
SL_SI91X_AES_KEY_SIZE_256 = 32
}

Enumeration defining AES key sizes supported by the SI91X device.

Macros#

#define

AES BLOCK SIZE of 16 bytes or 128 bits.

Enumeration Documentation#

sl_si91x_aes_mode_t#

sl_si91x_aes_mode_t

Enumeration defining AES modes supported by the SI91X device.

This enumeration defines different AES modes supported by the SI91X device, such as AES CBC, AES ECB, and AES CTR modes.

Enumerator
SL_SI91X_AES_CBC

AES CBC mode.

SL_SI91X_AES_ECB

AES ECB mode.

SL_SI91X_AES_CTR

AES CTR mode.


sl_si91x_aes_type_t#

sl_si91x_aes_type_t

Enumeration defining AES encryption and decryption types.

This enumeration defines the types of AES operations supported, including encryption and decryption.

Enumerator
SL_SI91X_AES_ENCRYPT

AES Encryption.

SL_SI91X_AES_DECRYPT

AES Decryption.


sl_si91x_aes_key_size_t#

sl_si91x_aes_key_size_t

Enumeration defining AES key sizes supported by the SI91X device.

This enumeration defines the key sizes supported by the AES encryption algorithm on the SI91X device, including 128-bit, 192-bit, and 256-bit key sizes.

Enumerator
SL_SI91X_AES_KEY_SIZE_128

key size of 128 bits

SL_SI91X_AES_KEY_SIZE_192

key size of 192 bits

SL_SI91X_AES_KEY_SIZE_256

key size of 256 bits


Macro Definition Documentation#

SL_SI91X_AES_BLOCK_SIZE#

#define SL_SI91X_AES_BLOCK_SIZE
Value:
16

AES BLOCK SIZE of 16 bytes or 128 bits.