HTTP client request configurations.
Public Attributes#
HTTP request method. sl_http_client_method_type_t.
HTTP server IP address.
URL string for requested resource.
HTTP server port number.
SNI extension address. si91x_socket_type_length_value_t.
HTTP body to be sent to the server. Setting this to null will process the request in chunked encoding.
Body length of data to be posted. In case of chunked request, body length should be equal to total content length.
User-defined extended header. If null, default extended header will be added internally. sl_http_client_header_t.
HTTP request timeout period. (Si91x chipsets does not support this feature).
HTTP request maximum retry count after timeout. (Si91x chipsets does not support this feature).
Retry period after max retry count reach. (Si91x chipsets does not support this feature).
Flag to use same TCP socket for connection. (Si91x chipsets does not support this feature).
User defined context.
The hostname of the HTTP server, as specified in the request header. If the hostname is NULL, then the ip_address is used instead of the hostname.
Public Attribute Documentation#
http_method_type#
sl_http_client_method_type_t sl_http_client_request_t::http_method_type
HTTP request method. sl_http_client_method_type_t.
resource#
uint8_t* sl_http_client_request_t::resource
URL string for requested resource.
The maximum supported HTTP URL is 2048 bytes, when the SL_SI91X_FEAT_LONG_HTTP_URL Bit is enabled in the feature_bit_map. If the SL_SI91X_FEAT_LONG_HTTP_URL Bit is disabled then the maximum supported length for HTTP URL is (872-(length of User_name + length of Password) - length of hostname - length of IP address) bytes excluding delimiters.
sni_extension#
si91x_socket_type_length_value_t* sl_http_client_request_t::sni_extension
SNI extension address. si91x_socket_type_length_value_t.
body#
uint8_t* sl_http_client_request_t::body
HTTP body to be sent to the server. Setting this to null will process the request in chunked encoding.
body_length#
uint32_t sl_http_client_request_t::body_length
Body length of data to be posted. In case of chunked request, body length should be equal to total content length.
extended_header#
sl_http_client_header_t* sl_http_client_request_t::extended_header
User-defined extended header. If null, default extended header will be added internally. sl_http_client_header_t.
timeout_ms#
uint16_t sl_http_client_request_t::timeout_ms
HTTP request timeout period. (Si91x chipsets does not support this feature).
retry_count#
uint16_t sl_http_client_request_t::retry_count
HTTP request maximum retry count after timeout. (Si91x chipsets does not support this feature).
retry_period_ms#
uint16_t sl_http_client_request_t::retry_period_ms
Retry period after max retry count reach. (Si91x chipsets does not support this feature).
tcp_connection_reuse#
bool sl_http_client_request_t::tcp_connection_reuse
Flag to use same TCP socket for connection. (Si91x chipsets does not support this feature).
event_handler#
sl_http_client_event_handler_t sl_http_client_request_t::event_handler
Callback method. sl_http_client_event_handler_t.
host_name#
uint8_t* sl_http_client_request_t::host_name
The hostname of the HTTP server, as specified in the request header. If the hostname is NULL, then the ip_address is used instead of the hostname.