Functions#

This section provides a reference to the Ping API functions.

Functions#

sl_status_t
sl_si91x_send_ping(sl_ip_address_t ip_address, uint16_t ping_packet_size)

Send an ICMP ping request.

Function Documentation#

sl_si91x_send_ping#

sl_status_t sl_si91x_send_ping (sl_ip_address_t ip_address, uint16_t ping_packet_size)

Send an ICMP ping request.

Parameters
TypeDirectionArgument NameDescription
sl_ip_address_t[in]ip_address

Destination IP address (IPv4 or IPv6) and SL IP type identified by sl_ip_address_t

uint16_t[in]ping_packet_size

Size of a ping packet

  • Pre-condition:

Returns

Note