You are viewing documentation for version:
SNTP Server Info response.
Public Attributes#
uint8_t
Ip version of the SNTP server. 4 for IPV4 and 6 for IPV6.
uint8_t
Ipv4 address of the SNTP server.
unsigned long
Ipv6 address of the SNTP server.
union SL_ATTRIBUTE_PACKED::@0
Public Attribute Documentation#
command_type#
uint8_t SL_ATTRIBUTE_PACKED::command_type
command type
ip_version#
uint8_t SL_ATTRIBUTE_PACKED::ip_version
Ip version of the SNTP server. 4 for IPV4 and 6 for IPV6.
ipv4_address#
uint8_t SL_ATTRIBUTE_PACKED::ipv4_address[4]
Ipv4 address of the SNTP server.
ipv6_address#
unsigned long SL_ATTRIBUTE_PACKED::ipv6_address[4]
Ipv6 address of the SNTP server.
server_ip_address#
union SL_ATTRIBUTE_PACKED::@0 SL_ATTRIBUTE_PACKED::server_ip_address
sntp_method#
uint8_t SL_ATTRIBUTE_PACKED::sntp_method
SNTP server method.