Folder Structure#
This section compares the folders in the WiSeConnect™ SDK v2.x and v3.x GitHub repositories.
2.x Folder | Description | 3.x Folder | Description |
|---|---|---|---|
| WiSeConnect 3.x source code and Simplicity Studio component definitions | ||
| Network processor firmware images |
| Same as v2.x |
| Lite firmware image | ||
| Standard firmware image | ||
| All v2.x documentation including release notes, getting started, API reference, and so on. |
| Release notes, software reference manual, and app notes for v3.x |
| Application examples |
| Same as v2.x |
| Configuration settings and Simplicity Studio component definitions for platforms (EFR™, EFM™, etc.) and modes (NCP, SoC, etc.) | ||
| See sub-folders below |
| See sub-folders below |
| Certificates |
| Same as v2.x |
| Simplicity Studio component definition for certificates | ||
| Default configuration header files | ||
| Default configurations for the Lightweight IP (LwIP) networking layers used in hosted mode | ||
| Miscellaneous declarations and configuration settings | ||
| Python test scripts for examples. |
| Same as v2.x |
| WiSeConnect 2.x source code and Simplicity Studio component definitions | ||
| Third-party software such as Amazon web services internet-of-things (AWS IoT) SDK, Azure SDK, and others |
| Same as v2.x but the third-party software included is different |
| Common utility functions for internet protocol version 6 (IPv6), logging, certificate handling, and others |
| Same as v2.x |