Functions#

This section provides a reference to the AES Crypto API Functions.

Functions#

sl_status_t
sl_si91x_aes(sl_si91x_aes_config_t *config, uint8_t *output)

This API is used to encrypt/decrypt the message according to the given configuration.

Function Documentation#

sl_si91x_aes#

sl_status_t sl_si91x_aes (sl_si91x_aes_config_t * config, uint8_t * output)

This API is used to encrypt/decrypt the message according to the given configuration.

Parameters
TypeDirectionArgument NameDescription
sl_si91x_aes_config_t *[in]config

Configuration object of type sl_si91x_aes_config_t

uint8_t *[out]output

Buffer to store the output.

This is a blocking API. Returns