IP configuration for a network interface.
Public Attributes#
sl_ip_management_t
IP Assignment Type of sl_ip_management_t.
sl_ip_address_type_t
IP Address Type of sl_ip_address_type_t.
char *
Host name visible on network.
IPv4 setting to be used in case of static IP address assignment of type sl_net_ipv4_setting_t.
IPv6 setting to be used in case of static IP address assignment of type sl_net_ipv6_setting_t.
struct sl_net_ip_configuration_t::@0
IP setting to be used for static IP address assignment.
Public Attribute Documentation#
v4#
sl_net_ipv4_setting_t sl_net_ip_configuration_t::v4
IPv4 setting to be used in case of static IP address assignment of type sl_net_ipv4_setting_t.
v6#
sl_net_ipv6_setting_t sl_net_ip_configuration_t::v6
IPv6 setting to be used in case of static IP address assignment of type sl_net_ipv6_setting_t.
ip#
struct sl_net_ip_configuration_t::@0 sl_net_ip_configuration_t::ip
IP setting to be used for static IP address assignment.