Sensor Hub#


Introduction#

  • Sensor Hub products are primarily intended to address consumer, industrial, and medical applications that require wireless connectivity, extremely low power, and high performance for sensor fusion algorithms. The MCU core, wireless connectivity, and peripherals are identical to the SI917 CCP Radio board.

  • Sensor Hub functions as a sensor management system, facilitating hardware abstraction layer, peripheral drivers, and sensor driver layer integration to collect and distribute desired sensor data.

  • It enables users to collect sensor data based on time interval or number of samples or when a specific data requirement are met.

  • Sensor Hub serves as a framework that can be seamlessly integrated into any application requiring sensor management.

  • The Sensor HUB works with sensors as per configurations provided by the application and notifies the necessary events throughout the application.

  • The configuration for the sensors must be provided through the sensor hub config file on which the sensor hub should act.

  • Sensor Hub relies on FreeRTOS using CMSIS RTOS version 2 wrapper.


Configuration#

  • Sensor Hub has 2 Sensor Mode:

  • SL_SH_POLLING_MODE: This mode is Timer based.

  • SL_SH_INTERRUPT_MODE: This mode is NPSS Button 0 GPIO Interrupt based.

  • There are 3 types of data_deliver.mode in Polling Sensor Mode and they are SL_SH_THRESHOLD, SL_SH_TIMEOUT and SL_SH_NUM_OF_SAMPLES.

  • SL_SH_NO_DATA data_deliver.mode is used when Interrupt Sensor Mode is selected.

  • If the user wants a value that sets a limit or boundary, above which the sensor data should be shown then SL_SH_THRESHOLD mode should be chosen

  • SL_SH_TIMEOUT mode is used when user wants to get the data at some intervals of time for some sampling time

  • SL_SH_NUM_OF_SAMPLES mode is used when user wants to get the particular number of sensor data 

  • SL_SH_NO_DATA mode is used when .

  • Here data_deliver.timeout is the time for which the sensor should keep collecting the data for.

  • sampling_interval is the the amount of time between two sensor data read is sampled or collected.

  • sampling_intr_req_pin is the GPIO pin for sampling the sensor data

  • Configure the number of sensors info in the **\sensors\inc\sensors_config.h** file

    #define SL_MAX_NUM_SENSORS              5   // Maximum sensors present in the system
    
  • Modes: Using the configuration structure, one can configure the following parameters in the sensorhub_config.c file:

    • For POLLING Sensor Mode configure the below parameters:

      .sensor_mode                = SL_SH_POLLING_MODE,
      .sampling_interval          = 100,
      
      • If sensor_mode is selected as SL_SH_POLLING_MODE, then data_deliver.mode should be configured as one of the following for a sensor configuration structure:

        • For TIMEOUT Data Mode configure the below parameters:

          .data_deliver.mode          = SL_SH_TIMEOUT,
          .data_deliver.timeout       = 1000,
          
        • For THRESHOLD Data Mode configure the below parameters:

          .data_deliver.mode          = SL_SH_THRESHOLD,
          .data_deliver.threshold     = 1000,
          
        • For SAMPLING Data Mode configure the below parameters:

          .data_deliver.mode          = SL_SH_NUM_OF_SAMPLES,
          .data_deliver.numOfSamples  = 5,
          
    • For INTERRUPT Sensor Mode configure the below parameters:

      .sensor_mode                = SL_SH_INTERRUPT_MODE,
      .sampling_intr_req_pin      = BUTTON_0_GPIO_PIN,
      .sensor_intr_type           = SL_SH_FALL_EDGE,
      .data_deliver.data_mode     = SL_SH_NO_DATA_MODE,
      
  • To configure the PS2, please update the below macro in the preprocessor settings:

    SL_SENSORHUB_POWERSAVE=1
    Enabling this macro will move the application from PS4 state to PS2 state. In PS2 state the sensor data will be sampled and collected.
    
  • To configure the power states to PS4 sleep or PS2 Sleep, please update the defines in ***\gecko_sdk_4.3.2\util\third_party\freertos\kernel.h** file as below:

    #ifndef configUSE_TICKLESS_IDLE
    #define configUSE_TICKLESS_IDLE 1           // 1 is to Enable the tickless Idle mode
    #endif
    
    #ifndef configPRE_SLEEP_PROCESSING
    #define configPRE_SLEEP_PROCESSING(x) sli_si91x_sleep_wakeup(x)               // Here x is idle time,
    #endif
    
    // Configure the sleep time by using the below macro.
    // If the number of Ideal task ticks exceeds this value, the system is allowed to sleep.
    #ifndef configEXPECTED_IDLE_TIME_BEFORE_SLEEP
       #define configEXPECTED_IDLE_TIME_BEFORE_SLEEP    70
    #endif
    

    Note:

  • By using above sleep configuration, sensor hub is going to sleep by using the idle task and idle time.

  • If the Ideal time exceeds the expected sleep time value, the system is allowed to sleep.

  • The above idle time is fed to the Alarm timer, which we are using as a wake-up source.

ADC Configurations: Configure only below parameters for ADC to change its mode from FIFO to STATIC and vice versa

  • For ADC FIFO mode, configure as shown below:

    .adc_config.adc_cfg.operation_mode        = SL_ADC_FIFO_MODE,
    .adc_config.adc_ch_cfg.sampling_rate[0]   = SL_SH_ADC_SAMPLING_RATE, // Use 100 for FIFO Mode
    
  • For ADC Static mode, configure as shown below:

    .adc_config.adc_cfg.operation_mode        = SL_ADC_STATIC_MODE,
    .adc_config.adc_ch_cfg.sampling_rate[0]   = SL_SH_ADC_SAMPLING_RATE, // Use 1000 for Static Mode
    
  • To configure the PS1 power state from PS2 State, please update the below macro in the preprocessor settings:

    SL_SH_ADC_PS1=1
     Enabling this macro will move the core from PS2 Active state to PS1 state
    
    • Please update the defines in ***\gecko_sdk_4.3.2\util\third_party\freertos\kernel.h** file as below:

      #ifndef configUSE_TICKLESS_IDLE
      #define configUSE_TICKLESS_IDLE 1           // 1 is to Enable the tickless Idle mode
      #endif
      
      #ifndef configPRE_SLEEP_PROCESSING
      #define configPRE_SLEEP_PROCESSING(x) sli_si91x_sleep_wakeup(x)               // Here x is idle time,
      #endif
      

      Note:

    • The PS1 state transition only applies to ADC FIFO Mode. Before entering this mode, kindly turn off any other sensors.


Usage#

Sensorhub provides two apis which user can use for intergrating into any application

  • sl_si91x_sensorhub_app_task(void);

  • sl_si91x_sensor_event_handler(uint8_t sensor_id, uint8_t event);

sl_si91x_sensorhub_app_task(void): initialises and starts sensor data collection. it achieves this by calling the following apis

sl_si91x_sensorhub_notify_cb_register(sl_sensor_signalEvent_t cb_event, sl_sensor_id_t *cb_ack): links the event handler provided by the user as a callback function in the event task

sl_si91x_sensorhub_init(): initializes the peripherals I2C, SPI, ADC, SDC

sl_si91x_sensorhub_detect_sensors(sl_sensor_id_t *sensor_id_info, uint8_t num_of_sensors): scans the i2c sensors provided in the sensorhub_config.c and returns the number of these sensors that are currently connected

sl_si91x_sensorhub_create_sensor(sl_sensor_id_t sensor_id): Initializes the sensor by calling the init function of the sensor provided by the user in the respective HAL, Assigs memory to it based on the data delivery mode, Creates a timer for this sensor if required

sl_si91x_sensor_hub_start(): initializes the sensor task, event task and power task

sl_si91x_sensorhub_start_sensor(sl_sensor_id_t sensor_id): starts the timers of the sensors created in create sensor api

sl_si91x_sensor_event_handler(uint8_t sensor_id, uint8_t event) is called by the event task after sensor data is collected ,in the sensorhub appilcation it prints the data based on the sensor id and uploads it to the cloud

Modules#

sl_sensorhub_errors_t

sl_data_deliver_type_t

sl_sensor_info_t

sl_sensor_handle_t

sl_sensor_list_t

sl_intr_list_t

sl_intr_list_map_t

sl_em_event_t

sl_sensor_cb_info_t

sl_i2c_config_t

sl_spi_config_t

sl_adc_config

sl_gpio_config_t

sl_sh_sdc_config_t

sl_bus_intf_config_t

Enumerations#

enum
SL_SH_POLLING_MODE
SL_SH_INTERRUPT_MODE
SL_SH_NO_MODE
}

Enumeration for Sensor HUB data reading mode.

enum
SL_SENSOR_CREATION_FAILED
SL_SENSOR_STARTED
SL_SENSOR_STOPPED
SL_SENSOR_DATA_READY
SL_SENSOR_CNFG_INVALID
SL_SENSOR_START_FAILED
SL_SENSOR_STOP_FAILED
SL_SENSOR_DELETED
SL_SENSOR_DELETE_FAILED
}

Enumeration for Sensors HUB Callback Events.

enum
SL_SH_RISE_EDGE
SL_SH_FALL_EDGE
SL_SH_LOW_LEVEL
SL_SH_HIGH_LEVEL
}

Enumeration for GPIO Interrupt Configurations.

enum
SL_SH_THRESHOLD
SL_SH_TIMEOUT
SL_SH_NUM_OF_SAMPLES
SL_SH_NO_DATA_MODE
}

Enumeration for Sensor HUB data delivery mode.

enum
SL_SENSOR_INVALID
SL_SENSOR_VALID
SL_SENSOR_START
SL_SENSOR_STOP
}

Enumeration for Sensors Status.

Typedefs#

typedef struct sl_adc_config

ADC bus interface configuration structure.

Variables#

bool

I2C bus error status.

bool

SPI bus error status.

bool

ADC bus error status.

bool
bool

All buses error status.

uint32_t

Threshold value for the sensor.

uint32_t

Threshold value for the sensor.

uint32_t

Timeout values for the sensor.

uint32_t

Timeout values for the sensor.

uint32_t

Number of samples for the sensor.

uint32_t

Number of samples for the sensor.

union sl_data_deliver_type_t::@0
char *

Name of the sensor.

int16_t

GPIO Interrupt Configurations.

uint16_t

GPIO pin for sampling the sensor data.

uint32_t

Sensor data sampling interval.

uint8_t

Address of sensor.

uint8_t

Address of sensor.

uint16_t

Channel for adc.

uint16_t

Channel for adc.

union sl_sensor_info_t::@2
sl_sensor_id_t

Sensor id.

sl_sensor_bus_t

Protocol for the sensor(spi/i2c)

Sensor Mode(Enumeration)

sl_sensor_range_t

Range of sensor.

Data delivery mode for the sensor.

sl_sensor_data_group_t *

Sensor data storage structure.

void *

Sensor handle.

void *

Sensor control handle.

uint8_t

Sensor event bits.

uint8_t

Sensor event acknowledge.

uint16_t

Maximum samples for the sensors.

Sensor configuration structure.

sl_sensor_impl_type_t *

Sensor implementation structure.

TimerHandle_t

RTOS timer handle.

uint8_t

Sensor index.

Sensor handle structure.

uint8_t

Interrupt mode sensor index.

uint16_t

Interrupt GPIO Pin.

uint16_t

Channel number for ADC interrupt.

uint16_t

Channel number for ADC interrupt.

uint8_t

Map Table Index.

Sensor list MAP Table.

void *

String the sensor data address.

sl_sensor_id_t

Sensor id information.

Sensors HUB Callback Events.

sl_sensor_signalEvent_t

Event callback.

sl_sensor_id_t *

Event callback acknowledge.

uint8_t

I2C instances(I2C0/1/2)

uint8_t

I2C power state.

uint8_t

I2C bus control configuration.

uint16_t

I2C bus speed.

uint32_t

I2C slave address.

uint8_t

SPI bus width.

uint8_t

SPI Mode(Master/Slave)

uint8_t

SPI bus power mode.

uint8_t

Chip select number.

uint8_t

SPI miscellaneous for chip select.

uint8_t

SPI slave select signal definitions.

uint32_t

SPI bus data transmission speed(clock)

uint64_t

SPI bus phase and polarity.

uint64_t

SPI control slave select mode.

uint8_t

flag to know if adc is initialized, this is necessary to deinit

uint16_t

flag to indicate data availability for all 16 channels

sl_adc_config_t

adc configuration

sl_adc_channel_config_t

adc channel configuration

uint8_t
uint32_t

I2C configuration structure.

SPI configuration structure.

ADC configuration structure.

GPIO configuration structure.

SDC configuration structure.

Functions#

sl_status_t

Initialization Peripherals of Sensor HUB.

sl_status_t
sl_si91x_sensorhub_detect_sensors(sl_sensor_id_t sensor_id_info[], uint8_t num_of_sensors)

Detect the sensors.

sl_status_t
sl_si91x_sensorhub_delete_sensor(sl_sensor_id_t sensor_id)

Delete the specific sensor from the Sensor HUB.

sl_status_t
sl_si91x_sensorhub_create_sensor(sl_sensor_id_t sensor_id)

Create a sensor instance in the sensor hub.

sl_status_t
sl_si91x_sensorhub_start_sensor(sl_sensor_id_t sensor_id)

Start the sensor operation for the given sensor.

sl_status_t
sl_si91x_sensorhub_stop_sensor(sl_sensor_id_t sensor_id)

Stop the sensor operation of the given sensor.

void
sl_si91x_em_post_event(sl_sensor_id_t sensor_id, sl_sensorhub_event_t event, void *dataPtr, TickType_t ticks_to_wait)

Post the events to event manager(EM) to be notified to the application.

void

Task to handle the sensor operations.

void

Task to handle the system power operations.

void

Task to handle the operations of the Event Manager(EM)

int32_t

Initialize the I2C Interface based on configuration.

int32_t

Initialize SPI Interface based on configuration.

int32_t
sli_si91x_i2c_sensors_scan(uint16_t address)

Scan the I2C sensors.

sl_sensor_impl_type_t *

to get sensor implementation.

int32_t

Create the sensor list index.

uint32_t
sli_si91x_get_sensor_index(sl_sensor_id_t sensor_id)

Get the sensor index for the sensor list.

uint32_t
sli_si91x_delete_sensor_list_index(sl_sensor_id_t sensor_id)

Delete the sensor index for the sensor list.

sli_si91x_get_sensor_info(sl_sensor_id_t sensor_id)

get the sensor info from the sensor configuration structure.

sl_status_t
sl_si91x_sensorhub_notify_cb_register(sl_sensor_signalEvent_t cb_event, sl_sensor_id_t *cb_ack)

Call back function to the application.

void
sl_si91x_sensors_timer_cb(TimerHandle_t xTimer)

Sensor OS timer callback function.

sl_status_t
sl_si91x_gpio_interrupt_config(uint16_t gpio_pin, sl_gpio_intr_type_t intr_type)

Configuring the different types of NPSS GPIO interrupts in the Sensor HUB.

void

Enable and set the priority of NPSS GPIO interrupt.

void
sl_si91x_gpio_interrupt_stop(uint16_t gpio_pin)

Mask and Disable the NPSS GPIO interrupt.

sl_status_t

Start the sensor hub Tasks.

void

set the alarm interrupt time.

void

initialize the Alarm block.

void
sli_si91x_config_wakeup_source(uint16_t sleep_time)

Configure the wake-up source for the system.

void
sli_si91x_sleep_wakeup(uint16_t sh_sleep_time)

Configures sleep/wakeup sources for the system.

void

Change the system status from PS4 to PS2.

void

Change the system status from PS2 to PS4.

sl_status_t

Initialize ADC Interface based on configuration.

void

Initialize and configure the systic timer for the RTOS.

void
ARM_I2C_SignalEvent(uint32_t event)

I2C event handler.

Fetch ADC bus interface information.

void
sl_si91x_adc_callback(uint8_t channel_no, uint8_t event)

ADC callback from RSI_ADC_InterruptHandler.

sl_status_t

Initialize the sdc Interface based on the configuration.

void
sli_config_sdc_params(sl_drv_sdc_config_t *sdc_config_st_p)

Macros#

#define
SL_SH_SENSOR_TASK_STACK_SIZE (512 * 2)

Sensor task stack size.

#define
SL_SH_EM_TASK_STACK_SIZE (512 * 2)

EM task stack size.

#define
SL_SH_POWER_SAVE_TASK_STACK_SIZE (512 * 2)

Power task stack size.

#define
SL_EM_TASK_RUN_TICKS osWaitForever

Max wait time of message queue in Event task.

#define
MAP_TABLE_SIZE 10

Size of the sensors interrupt MAP table.

#define
NPSS_GPIO_IRQHandler IRQ021_Handler

NPSS gpio IRQ handler.

#define
NPSS_GPIO_NVIC NPSS_TO_MCU_GPIO_INTR_IRQn

NPSS gpio IRQ Number 21.

#define
SL_ALARM_PERIODIC_TIME 10

Periodic alarm configuration in milliseconds.

#define
RC_TRIGGER_TIME 5

RC clock trigger time.

#define
RO_TRIGGER_TIME 0

RO clock trigger time.

#define
NO_OF_HOURS_IN_A_DAY 24

Number of hours in a day.

#define
NO_OF_MINUTES_IN_AN_HOUR 60

Number of minutes in an hour.

#define
NO_OF_SECONDS_IN_A_MINUTE 60

Number of Seconds in a minute.

#define
NO_OF_MILLISECONDS_IN_A_SECOND 1000

Number of milliseconds in a second.

#define
NO_OF_MONTHS_IN_A_YEAR 12

Number of months in a year.

#define
BASE_YEAR 2000

Start year for alarm configuration.

#define
NO_OF_DAYS_IN_A_MONTH_1 28

Month with 28 days.

#define
NO_OF_DAYS_IN_A_MONTH_2 29

Month with 29 days.

#define
NO_OF_DAYS_IN_A_MONTH_3 30

Month with 30 days.

#define
NO_OF_DAYS_IN_A_MONTH_4 31

Month with 31 days.

#define
RTC_ALARM_IRQHandler IRQ028_Handler

Alarm IRQ handler.

#define
NVIC_RTC_ALARM MCU_CAL_ALARM_IRQn

Alarm IRQ number 28.

#define
SL_SH_SENSORHUB_ERRORS_MASK 0
#define
SL_SH_TIMER_CREATION_FAILED (1 << SL_SH_SENSORHUB_ERRORS_MASK)

Creating OS timer for the sensor failed.

#define
SL_SH_TIMER_DELETION_FAILED (2 << SL_SH_SENSORHUB_ERRORS_MASK)

Deleting OS timer of the sensor failed.

#define
SL_SH_TIMER_START_FAIL (3 << SL_SH_SENSORHUB_ERRORS_MASK)

Starting OS timer of the sensor failed.

#define
SL_SH_TIMER_STOP_FAIL (4 << SL_SH_SENSORHUB_ERRORS_MASK)

Stopping OS timer of the sensor failed.

#define
SL_SH_MAX_SENSORS_REACHED (5 << SL_SH_SENSORHUB_ERRORS_MASK)

Max number of sensor limit reached.

#define
SL_SH_MEMORY_LIMIT_EXCEEDED (6 << SL_SH_SENSORHUB_ERRORS_MASK)

Memory allocation for sensor data storage failed.

#define
SL_SH_SENSOR_CREATE_FAIL (7 << SL_SH_SENSORHUB_ERRORS_MASK)

Sensor API is called for a sensor without creating it.

#define
SL_SH_COMMAND_SET_POWER_FAIL (8 << SL_SH_SENSORHUB_ERRORS_MASK)

Sensor set power command execution failed.

#define
SL_SH_COMMAND_SET_RANGE_FAIL (9 << SL_SH_SENSORHUB_ERRORS_MASK)

Sensor set range command execution failed.

#define
SL_SH_COMMAND_SELF_TEST_FAIL (10 << SL_SH_SENSORHUB_ERRORS_MASK)

Sensor self-test command execution failed.

#define
SL_SH_INVALID_PARAMETERS (11 << SL_SH_SENSORHUB_ERRORS_MASK)

Generic error code for any invalid parameters.

#define
SL_SH_GPIO_OUT_OF_RANGE (12 << SL_SH_SENSORHUB_ERRORS_MASK)

Invalid gpio number.

#define
SL_SH_SENSOR_IMPLEMENTATION_NOT_FOUND (13 << SL_SH_SENSORHUB_ERRORS_MASK)

No hal implementation found for given sensor type.

#define
SL_SH_INTERRUPT_TYPE_CONFIG_FAIL (14 << SL_SH_SENSORHUB_ERRORS_MASK)

Interrupt type configuration failed.

#define
SL_SH_MEMORY_ALLOCATION_FAILED (15 << SL_SH_SENSORHUB_ERRORS_MASK)

Allocating memory for sensor hal failed.

#define
SL_SH_SENSOR_INDEX_NOT_FOUND (0xFF)

Sensor not created.

#define
SL_SH_CONFIG_NOT_FOUND (16 << SL_SH_SENSORHUB_ERRORS_MASK)

Sensor configuration not found.

#define
SL_SH_INVALID_ADDRESS (17 << SL_SH_SENSORHUB_ERRORS_MASK)

No sensor found at given address.

#define
SL_SH_WRONG_INTERRUPT_TYPE (18 << SL_SH_SENSORHUB_ERRORS_MASK)

Invalid interrupt type is given for the sensor.

#define
SL_SH_INVALID_MODE (19 << SL_SH_SENSORHUB_ERRORS_MASK)

Invalid mode is given for the sensor.

#define
SL_SH_INVALID_DELIVERY_MODE (20 << SL_SH_SENSORHUB_ERRORS_MASK)

Invalid delivery mode is given for the sensor.

#define
SL_SH_HAL_SENSOR_CREATION_FAILED (21 << SL_SH_SENSORHUB_ERRORS_MASK)

Create sensor in HAL failed.

#define
SL_SH_HAL_SENSOR_DELETION_FAILED (22 << SL_SH_SENSORHUB_ERRORS_MASK)

Delete sensor in HAL failed.

#define
SL_SH_HAL_SENSOR_SAMPLE_FAIL (23 << SL_SH_SENSORHUB_ERRORS_MASK)

Sample sensor in HAL failed.

#define
SL_SH_HAL_SENSOR_CONTROL_FAIL (24 << SL_SH_SENSORHUB_ERRORS_MASK)

Control sensor in HAL failed.

#define
SL_SH_POWER_TASK_CREATION_FAILED (25 << SL_SH_SENSORHUB_ERRORS_MASK)

Power task creation failed.

#define
SL_SH_SENSOR_TASK_CREATION_FAILED (26 << SL_SH_SENSORHUB_ERRORS_MASK)

Sensor task creation failed.

#define
SL_SH_EM_TASK_CREATION_FAILED (27 << SL_SH_SENSORHUB_ERRORS_MASK)

EM task creation failed.

#define
SL_ALL_PERIPHERALS_INIT_FAILED (28 << SL_SH_SENSORHUB_ERRORS_MASK)

All(i2c,spi,adc) peripheral's initialization failed.

Enumeration Documentation#

sl_sensor_mode_t#

sl_sensor_mode_t

Enumeration for Sensor HUB data reading mode.

Enumerator
SL_SH_POLLING_MODE

POLLING_MODE.

SL_SH_INTERRUPT_MODE

INTERRUPT_MODE.

SL_SH_NO_MODE

sl_sensorhub_event_t#

sl_sensorhub_event_t

Enumeration for Sensors HUB Callback Events.

Enumerator
SL_SENSOR_CREATION_FAILED
SL_SENSOR_STARTED
SL_SENSOR_STOPPED
SL_SENSOR_DATA_READY
SL_SENSOR_CNFG_INVALID
SL_SENSOR_START_FAILED
SL_SENSOR_STOP_FAILED
SL_SENSOR_DELETED
SL_SENSOR_DELETE_FAILED

sl_gpio_intr_type_t#

sl_gpio_intr_type_t

Enumeration for GPIO Interrupt Configurations.

Enumerator
SL_SH_RISE_EDGE

Interrupt at GPIO rise edge.

SL_SH_FALL_EDGE

Interrupt at GPIO fall edge.

SL_SH_LOW_LEVEL

Interrupt at GPIO low level.

SL_SH_HIGH_LEVEL

Interrupt at GPIO high level.


sl_data_deliver_mode_t#

sl_data_deliver_mode_t

Enumeration for Sensor HUB data delivery mode.

Enumerator
SL_SH_THRESHOLD

Threshold value for sensor data delivery.

SL_SH_TIMEOUT

Timeout value for sensor data delivery.

SL_SH_NUM_OF_SAMPLES

Number of samples for sensor data delivery.

SL_SH_NO_DATA_MODE

sl_sensor_status_t#

sl_sensor_status_t

Enumeration for Sensors Status.

Enumerator
SL_SENSOR_INVALID

Sensor is Invalid.

SL_SENSOR_VALID

Sensor is Valid.

SL_SENSOR_START

Sensor is Started.

SL_SENSOR_STOP

Sensor is Stoped.


Typedef Documentation#

sl_adc_cfg_t#

typedef struct sl_adc_config sl_adc_cfg_t

ADC bus interface configuration structure.


Variable Documentation#

i2c#

bool sl_sensorhub_errors_t::i2c

I2C bus error status.


spi#

bool sl_sensorhub_errors_t::spi

SPI bus error status.


adc#

bool sl_sensorhub_errors_t::adc

ADC bus error status.


sdc#

bool sl_sensorhub_errors_t::sdc

sensor_global_status#

bool sl_sensorhub_errors_t::sensor_global_status

All buses error status.


data_mode#

sl_data_deliver_mode_t sl_data_deliver_type_t::data_mode

threshold#

uint32_t sl_data_deliver_type_t::threshold

Threshold value for the sensor.


threshold#

uint32_t sl_data_deliver_type_t::@0::threshold

Threshold value for the sensor.


timeout#

uint32_t sl_data_deliver_type_t::timeout

Timeout values for the sensor.


timeout#

uint32_t sl_data_deliver_type_t::@0::timeout

Timeout values for the sensor.


numofsamples#

uint32_t sl_data_deliver_type_t::numofsamples

Number of samples for the sensor.


numofsamples#

uint32_t sl_data_deliver_type_t::@0::numofsamples

Number of samples for the sensor.


@1#

union sl_data_deliver_type_t::@0 sl_data_deliver_type_t::@1

sensor_name#

char* sl_sensor_info_t::sensor_name

Name of the sensor.


sensor_intr_type#

int16_t sl_sensor_info_t::sensor_intr_type

GPIO Interrupt Configurations.


sampling_intr_req_pin#

uint16_t sl_sensor_info_t::sampling_intr_req_pin

GPIO pin for sampling the sensor data.


sampling_interval#

uint32_t sl_sensor_info_t::sampling_interval

Sensor data sampling interval.


address#

uint8_t sl_sensor_info_t::address

Address of sensor.


address#

uint8_t sl_sensor_info_t::@2::address

Address of sensor.


channel#

uint16_t sl_sensor_info_t::channel

Channel for adc.


channel#

uint16_t sl_sensor_info_t::@2::channel

Channel for adc.


@3#

union sl_sensor_info_t::@2 sl_sensor_info_t::@3

sensor_id#

sl_sensor_id_t sl_sensor_info_t::sensor_id

Sensor id.


sensor_bus#

sl_sensor_bus_t sl_sensor_info_t::sensor_bus

Protocol for the sensor(spi/i2c)


sensor_mode#

sl_sensor_mode_t sl_sensor_info_t::sensor_mode

Sensor Mode(Enumeration)


sensor_range#

sl_sensor_range_t sl_sensor_info_t::sensor_range

Range of sensor.


data_deliver#

sl_data_deliver_type_t sl_sensor_info_t::data_deliver

Data delivery mode for the sensor.


sensor_data_ptr#

sl_sensor_data_group_t* sl_sensor_info_t::sensor_data_ptr

Sensor data storage structure.


sensor_handle#

void* sl_sensor_handle_t::sensor_handle

Sensor handle.


ctrl_handle#

void* sl_sensor_handle_t::ctrl_handle

Sensor control handle.


sensor_event_bit#

uint8_t sl_sensor_handle_t::sensor_event_bit

Sensor event bits.


event_ack#

uint8_t sl_sensor_handle_t::event_ack

Sensor event acknowledge.


max_samples#

uint16_t sl_sensor_handle_t::max_samples

Maximum samples for the sensors.


config_st#

sl_sensor_info_t* sl_sensor_handle_t::config_st

Sensor configuration structure.


sensor_impl#

sl_sensor_impl_type_t* sl_sensor_handle_t::sensor_impl

Sensor implementation structure.


sensor_status#

sl_sensor_status_t sl_sensor_handle_t::sensor_status

Sensor status.


timer_handle#

TimerHandle_t sl_sensor_handle_t::timer_handle

RTOS timer handle.


sensor_index#

uint8_t sl_sensor_list_t::sensor_index

Sensor index.


sl_sensors_st#

sl_sensor_handle_t sl_sensor_list_t::sl_sensors_st[SL_MAX_NUM_SENSORS]

Sensor handle structure.


sensor_list_index#

uint8_t sl_intr_list_t::sensor_list_index

Interrupt mode sensor index.


intr#

uint16_t sl_intr_list_t::intr

Interrupt GPIO Pin.


adc_intr_channel#

uint16_t sl_intr_list_t::adc_intr_channel

Channel number for ADC interrupt.


sdc_intr_channel#

uint16_t sl_intr_list_t::sdc_intr_channel

Channel number for ADC interrupt.


map_index#

uint8_t sl_intr_list_map_t::map_index

Map Table Index.


map_table#

sl_intr_list_t sl_intr_list_map_t::map_table[MAP_TABLE_SIZE]

Sensor list MAP Table.


em_sensor_data#

void* sl_em_event_t::em_sensor_data

String the sensor data address.


sensor_id#

sl_sensor_id_t sl_em_event_t::sensor_id

Sensor id information.


event#

sl_sensorhub_event_t sl_em_event_t::event

Sensors HUB Callback Events.


cb_event#

sl_sensor_signalEvent_t sl_sensor_cb_info_t::cb_event

Event callback.


cb_event_ack#

sl_sensor_id_t* sl_sensor_cb_info_t::cb_event_ack

Event callback acknowledge.


i2c_id#

uint8_t sl_i2c_config_t::i2c_id

I2C instances(I2C0/1/2)


i2c_power_state#

uint8_t sl_i2c_config_t::i2c_power_state

I2C power state.


i2c_control_mode#

uint8_t sl_i2c_config_t::i2c_control_mode

I2C bus control configuration.


i2c_bus_speed#

uint16_t sl_i2c_config_t::i2c_bus_speed

I2C bus speed.


i2c_slave_addr#

uint32_t sl_i2c_config_t::i2c_slave_addr

I2C slave address.


spi_bit_width#

uint8_t sl_spi_config_t::spi_bit_width

SPI bus width.


spi_mode#

uint8_t sl_spi_config_t::spi_mode

SPI Mode(Master/Slave)


spi_power_state#

uint8_t sl_spi_config_t::spi_power_state

SPI bus power mode.


spi_cs_number#

uint8_t sl_spi_config_t::spi_cs_number

Chip select number.


spi_cs_misc_mode#

uint8_t sl_spi_config_t::spi_cs_misc_mode

SPI miscellaneous for chip select.


spi_sec_sel_sig#

uint8_t sl_spi_config_t::spi_sec_sel_sig

SPI slave select signal definitions.


spi_baud#

uint32_t sl_spi_config_t::spi_baud

SPI bus data transmission speed(clock)


spi_control_mode#

uint64_t sl_spi_config_t::spi_control_mode

SPI bus phase and polarity.


spi_cs_mode#

uint64_t sl_spi_config_t::spi_cs_mode

SPI control slave select mode.


adc_init#

uint8_t sl_adc_config::adc_init

flag to know if adc is initialized, this is necessary to deinit


adc_data_ready#

uint16_t sl_adc_config::adc_data_ready

flag to indicate data availability for all 16 channels


adc_cfg#

sl_adc_config_t sl_adc_config::adc_cfg

adc configuration


adc_ch_cfg#

sl_adc_channel_config_t sl_adc_config::adc_ch_cfg

adc channel configuration


c#

uint8_t sl_gpio_config_t::c

d#

uint32_t sl_gpio_config_t::d

sh_sdc_p_channel_sel#

uint8_t sl_sh_sdc_config_t::sh_sdc_p_channel_sel[4]

sh_sdc_n_channel_sel#

uint8_t sl_sh_sdc_config_t::sh_sdc_n_channel_sel[4]

sh_sdc_sample_ther#

uint8_t sl_sh_sdc_config_t::sh_sdc_sample_ther

sh_sdc_no_channel_sel#

uint8_t sl_sh_sdc_config_t::sh_sdc_no_channel_sel

sh_sdc_data_trigger_sel#

uint8_t sl_sh_sdc_config_t::sh_sdc_data_trigger_sel

sh_sdc_sample_trigger_sel#

uint8_t sl_sh_sdc_config_t::sh_sdc_sample_trigger_sel

sh_sdc_cnt_trig_evnt#

uint8_t sl_sh_sdc_config_t::sh_sdc_cnt_trig_evnt

sh_sdc_auxadc_diff_mode_ch#

uint8_t sl_sh_sdc_config_t::sh_sdc_auxadc_diff_mode_ch[4]

sh_sdc_auxadc_en#

uint8_t sl_sh_sdc_config_t::sh_sdc_auxadc_en

sh_sdc_adc_config_en#

uint8_t sl_sh_sdc_config_t::sh_sdc_adc_config_en

sh_sdc_clk_div#

uint8_t sl_sh_sdc_config_t::sh_sdc_clk_div

sh_sdc_samp_en#

uint8_t sl_sh_sdc_config_t::sh_sdc_samp_en

i2c_config#

sl_i2c_config_t sl_bus_intf_config_t::i2c_config

I2C configuration structure.


spi_config#

sl_spi_config_t sl_bus_intf_config_t::spi_config

SPI configuration structure.


adc_config#

sl_adc_cfg_t sl_bus_intf_config_t::adc_config

ADC configuration structure.


gpio_config#

sl_gpio_config_t sl_bus_intf_config_t::gpio_config

GPIO configuration structure.


sh_sdc_config#

sl_sh_sdc_config_t sl_bus_intf_config_t::sh_sdc_config

SDC configuration structure.


Function Documentation#

sl_si91x_sensorhub_init#

sl_status_t sl_si91x_sensorhub_init ( -, -)

Initialization Peripherals of Sensor HUB.

Parameters
TypeDirectionArgument NameDescription
[in]-

NULL

[out]-

Return the Sensor Hub bus Initialization status

This function will initialize the Peripherals, based on the user configuration. like - I2C/SPI/ADC

Returns

  • status 0 if successful, else error code as follow:

    • SL_STATUS_FAIL (0x0001)- Fail, Peripherals initialization failed

    • SL_STATUS_OK (0X000)- Success, Peripherals initialization done properly


sl_si91x_sensorhub_detect_sensors#

sl_status_t sl_si91x_sensorhub_detect_sensors (sl_sensor_id_t sensor_id_info, uint8_t num_of_sensors, -)

Detect the sensors.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id_info

- Sensor IDs

uint8_t[in]num_of_sensors

- Number of sensors given by user

[out]-

None

This function will detect the sensor, based on the user configuration. and it will store the scanned sensor ID in the structure.

Returns

  • if successful, Return number of sensors scanned else error code


sl_si91x_sensorhub_delete_sensor#

sl_status_t sl_si91x_sensorhub_delete_sensor (sl_sensor_id_t sensor_id, -)

Delete the specific sensor from the Sensor HUB.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Sensor ID

[out]-

Return the delete sensors status

This function will delete the specific sensor from the sensor list, modify the sensor status to invalid, and publish the events to the event task.

Returns

  • status 0 if successful, else error code as follow:

    • SL_STATUS_FAIL (0x0001) - Fail, Delete sensor failed

    • SL_STATUS_OK (0X000) - Success, Delete sensor Success


sl_si91x_sensorhub_create_sensor#

sl_status_t sl_si91x_sensorhub_create_sensor (sl_sensor_id_t sensor_id, -)

Create a sensor instance in the sensor hub.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Id of sensor

[out]-

Return the create sensors status

This function creates a sensor instance as per user configuration.It also allocates max sample memory for the configured sensor.

Returns

  • status 0 if successful, else error code as follow:

    • SL_STATUS_FAIL (0x0001)- Fail, Create sensor instance failed

    • SL_STATUS _OK (0X000) - Create sensor instanceSuccess ,


sl_si91x_sensorhub_start_sensor#

sl_status_t sl_si91x_sensorhub_start_sensor (sl_sensor_id_t sensor_id, -)

Start the sensor operation for the given sensor.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Id of sensor

[out]-

Return the Start sensors status

This function can be called after creating a sensor with given sensor ID It does following operations

  • Starts timer for sensor with polling mode.

  • Enable IRQ handle for sensor with interrupt mode.

Returns

  • status 0 if successful, else error code as follow:

    • SL_STATUS_FAIL (0x0001)- Fail, Sensor start failed

    • SL_STATUS _OK (0X000) - Success ,Sensor start done properly


sl_si91x_sensorhub_stop_sensor#

sl_status_t sl_si91x_sensorhub_stop_sensor (sl_sensor_id_t sensor_id, -)

Stop the sensor operation of the given sensor.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Id of sensor

[out]-

Return the Stop sensor status

This function does following operations

  • Stop the sensor operations of the given sensor.

  • Based on the sensor mode it will stop the Polling/interrupt mode operations and updates the sensor statutes.

  • Disable IRQ handles of the interrupt mode sensors.

Returns

  • status 0 if successful, else error code as follows:

    • SL_STATUS_FAIL (0x0001)- Fail, Sensor stop failed

  • SL_STATUS _OK (0X000) - Success ,Sensor stop done properly


sl_si91x_em_post_event#

void sl_si91x_em_post_event (sl_sensor_id_t sensor_id, sl_sensorhub_event_t event, void * dataPtr, TickType_t ticks_to_wait, -)

Post the events to event manager(EM) to be notified to the application.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- id of the sensor

sl_sensorhub_event_t[in]event

- sensor hub events

void *[in]dataPtr

- sensor data pointer

TickType_t[in]ticks_to_wait

- max time to wait for the post

[out]-

None

It waits for mutex till ticks_to_wait and updates event queue if mutex is acquired

Returns

  • - NULL


sl_si91x_sensor_task#

void sl_si91x_sensor_task (void , -)

Task to handle the sensor operations.

Parameters
TypeDirectionArgument NameDescription
void[in]

None

[out]-

None

Sensor Task does following operations

  • Create the OS event and mutex to perform the sensor operations.

  • Sample the Sensor data based on the event flags.

  • Check the events and post the sensor data to the em task based on the sensor data delivery mode.

Returns

  • - NULL


sl_si91x_power_state_task#

void sl_si91x_power_state_task (void , -)

Task to handle the system power operations.

Parameters
TypeDirectionArgument NameDescription
void[in]

None

[out]-

None

Power state task changes the system from one power save mode to another power save mode like(PS4 to PS2),(PS2toPS4),(Sleep_mode) using Binary semaphore

Returns

  • - NULL


sl_si91x_em_task#

void sl_si91x_em_task (void , -)

Task to handle the operations of the Event Manager(EM)

Parameters
TypeDirectionArgument NameDescription
void[in]

None

[out]-

None

Em task does following operaions

  • Create the osMessageQueue and mutex to perform the event operations.

  • Calls the callback event Returns

    • - NULL


sli_si91x_i2c_init#

int32_t sli_si91x_i2c_init (void , -)

Initialize the I2C Interface based on configuration.

Parameters
TypeDirectionArgument NameDescription
void[in]

None

[out]-

None

This function will configure/Initialize I2C Interface based on configuration.

Returns

  • I2C Initializtion status


sli_si91x_spi_init#

int32_t sli_si91x_spi_init (void , -)

Initialize SPI Interface based on configuration.

Parameters
TypeDirectionArgument NameDescription
void[in]

None

[out]-

None

This function will configure/Initialize SPI Interface based on configuration.

Returns

  • SPI Initializtion status.


sli_si91x_i2c_sensors_scan#

int32_t sli_si91x_i2c_sensors_scan (uint16_t address, -)

Scan the I2C sensors.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]address

- Address of sensor

[out]-

None

This function will scan the I2C sensors based on the sensor address.

Returns

  • status 0 if successful, else it will wait for the sensor response.


sli_si91x_get_sensor_implementation#

sl_sensor_impl_type_t * sli_si91x_get_sensor_implementation (int32_t sensor_id, -)

to get sensor implementation.

Parameters
TypeDirectionArgument NameDescription
int32_t[in]sensor_id

- Id of sensor

[out]-

None

This function will get the sensor implementation of the sensor based on sensor ID.

Returns

  • if successful, returns the Sensor implementation structure else returns an error code.


sli_si91x_create_sensor_list_index#

int32_t sli_si91x_create_sensor_list_index ( -, -)

Create the sensor list index.

Parameters
TypeDirectionArgument NameDescription
[in]-

None

[out]-

Returns the Sensor ID from the implementation struct

This function will Create the sensor list index based on the sensor status For the maximum sensors available in the sensor hub

Returns

  • returns the sensor index in sensor_list


sli_si91x_get_sensor_index#

uint32_t sli_si91x_get_sensor_index (sl_sensor_id_t sensor_id, -)

Get the sensor index for the sensor list.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Id of sensor

[out]-

None

This function will retrieve the sensor index from the sensor list based on the sensor status and sensor ID for the maximum number of sensors available in the sensor hub.

Returns


sli_si91x_delete_sensor_list_index#

uint32_t sli_si91x_delete_sensor_list_index (sl_sensor_id_t sensor_id, -)

Delete the sensor index for the sensor list.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Id of sensor

[out]-

None

This function will delete the sensor from the sensor list based on The sensor ID for the maximum number of sensors available in the sensor hub.

Returns


sli_si91x_get_sensor_info#

sl_sensor_info_t * sli_si91x_get_sensor_info (sl_sensor_id_t sensor_id, -)

get the sensor info from the sensor configuration structure.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_id_t[in]sensor_id

- Id of sensor

[out]-

None

This function will retrieve sensor data from the sensor configuration structure to update the sensor list configuration structure for the maximum number of sensors available in the sensor hub.

Returns

  • if successful, returns the sensor information. else returns NULL.


sl_si91x_sensorhub_notify_cb_register#

sl_status_t sl_si91x_sensorhub_notify_cb_register (sl_sensor_signalEvent_t cb_event, sl_sensor_id_t * cb_ack, -)

Call back function to the application.

Parameters
TypeDirectionArgument NameDescription
sl_sensor_signalEvent_t[in]cb_event

- Pointer to the callback event

sl_sensor_id_t *[in]cb_ack

- Pointer to callback acknowledge to the application

[out]-

None

This function will update the callback function event and acknowledgment.

Returns

  • - If successful returns SL_STATUS_OK else returns error code


sl_si91x_sensors_timer_cb#

void sl_si91x_sensors_timer_cb (TimerHandle_t xTimer, -)

Sensor OS timer callback function.

Parameters
TypeDirectionArgument NameDescription
TimerHandle_t[in]xTimer

- Timer handle

[out]-

None

This function will set the event flag bits based on the sensor sampling intervals. In the polling mode call the timer call-back function.

Returns

  • - NULL


sl_si91x_gpio_interrupt_config#

sl_status_t sl_si91x_gpio_interrupt_config (uint16_t gpio_pin, sl_gpio_intr_type_t intr_type, -)

Configuring the different types of NPSS GPIO interrupts in the Sensor HUB.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]gpio_pin

- NPSS gpio pin number

sl_gpio_intr_type_t[in]intr_type

NPSS gpio interrupt type

[out]-

None

This function configures the NPSS gpios and enables the interrupt mode for the gpios.

Returns

  • - If successful returns SL_STATUS_OK else returns error code


sl_si91x_gpio_interrupt_start#

void sl_si91x_gpio_interrupt_start (uint16_t gpio_pin, -)

Enable and set the priority of NPSS GPIO interrupt.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]gpio_pin

- NPSS gpio pin number

[out]-

None

This function configures and sets the priority of the NPSS GPIO interrupt. GPIO interrupt priority is (configMAX_SYSCALL_INTERRUPT_PRIORITY - 1)

Returns

  • - NULL


sl_si91x_gpio_interrupt_stop#

void sl_si91x_gpio_interrupt_stop (uint16_t gpio_pin, -)

Mask and Disable the NPSS GPIO interrupt.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]gpio_pin

- NPSS gpio pin number

[out]-

None

This function masks and disables the IRQ handler of the NPSS GPIO interrupt.

Returns

  • - NULL


sl_si91x_sensor_hub_start#

sl_status_t sl_si91x_sensor_hub_start (void , -)

Start the sensor hub Tasks.

Parameters
TypeDirectionArgument NameDescription
void[in]

None

[out]-

None

This Starts the sensor hub Tasks.

Returns

  • - If succesfull returns SL_STATUS_OK else returns error code


sli_si91x_set_alarm_intr_time#

void sli_si91x_set_alarm_intr_time (uint16_t interval, -)

set the alarm interrupt time.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]interval

- interval time

[out]-

None

This function will set the alarm interrupt based on the periodic time.

Returns

  • - NULL


sli_si91x_init_m4alarm_config#

void sli_si91x_init_m4alarm_config (void , -)

initialize the Alarm block.

Parameters
TypeDirectionArgument NameDescription
void[in]

None

[out]-

None

This function will initialize the Alarm block.

Returns

  • - NULL


sli_si91x_config_wakeup_source#

void sli_si91x_config_wakeup_source (uint16_t sleep_time, -)

Configure the wake-up source for the system.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]sleep_time

- Sleep time for the sensor hub

[out]-

None

This function will configure the wake-up source to the system.

Returns

  • - NULL


sli_si91x_sleep_wakeup#

void sli_si91x_sleep_wakeup (uint16_t sh_sleep_time, -)

Configures sleep/wakeup sources for the system.

Parameters
TypeDirectionArgument NameDescription
uint16_t[in]sh_sleep_time

- Sleep time for the sensor hub, in ADC PS-1 no parameters

[out]-

None

This function will configure sleep/wakeup sources.

Returns

  • - NULL


sli_si91x_sensorhub_ps4tops2_state#

void sli_si91x_sensorhub_ps4tops2_state (void , -)

Change the system status from PS4 to PS2.

Parameters
TypeDirectionArgument NameDescription
void[in]

None

[out]-

None

This function will change the system status from PS4 to PS2.

Returns

  • - NULL


sli_si91x_sensorhub_ps2tops4_state#

void sli_si91x_sensorhub_ps2tops4_state (void , -)

Change the system status from PS2 to PS4.

Parameters
TypeDirectionArgument NameDescription
void[in]

None

[out]-

None

This function will change the system status from PS2 to PS4.

Returns

  • - NULL


sli_si91x_adc_init#

sl_status_t sli_si91x_adc_init (void )

Initialize ADC Interface based on configuration.

Parameters
TypeDirectionArgument NameDescription
void[in]

None

This function will configure/Initialize ADC Interface based on configuration.

Returns

  • error code SL_STATUS_FAIL (0x0001)- Fail , SL_STATUS_OK (0X000)- Success


vPortSetupTimerInterrupt#

void vPortSetupTimerInterrupt (void , -)

Initialize and configure the systic timer for the RTOS.

Parameters
TypeDirectionArgument NameDescription
void[in]

None

[out]-

None

Set up the systic timer to generate the tick interrupts at the required frequency.

Returns

  • Initialize status to the application.


ARM_I2C_SignalEvent#

void ARM_I2C_SignalEvent (uint32_t event, -)

I2C event handler.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]event

- I2C transmit and receive events

[out]-

None

Returns

  • None


sl_si91x_fetch_adc_bus_intf_info#

sl_adc_cfg_t * sl_si91x_fetch_adc_bus_intf_info (void )

Fetch ADC bus interface information.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This can be used by lower level layers Returns

  • Pointer to ADC configuration structure


sl_si91x_adc_callback#

void sl_si91x_adc_callback (uint8_t channel_no, uint8_t event)

ADC callback from RSI_ADC_InterruptHandler.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel_no

- respective channel number

uint8_t[in]event

- callback event (ADC_STATIC_MODE_CALLBACK, ADC_THRSHOLD_CALLBACK, INTERNAL_DMA, FIFO_MODE_EVENT)


sli_si91x_sdc_init#

uint8_t sli_si91x_sdc_init (void )

Initialize the sdc Interface based on the configuration.

Parameters
TypeDirectionArgument NameDescription
void[in]

Returns

  • status 0 if successful, else error code SL_STATUS_FAIL (0x0001)- Fail , SL_STATUS_OK (0X000)- Success,


sli_config_sdc_params#

void sli_config_sdc_params (sl_drv_sdc_config_t * sdc_config_st_p)
Parameters
TypeDirectionArgument NameDescription
sl_drv_sdc_config_t *N/Asdc_config_st_p