Overview#

The SiWx91x™ chipset family runs the HyperText Transfer Protocol (HTTP), and HyperText Transfer Protocol Secure (HTTPS) on its internal network processor, and provides the ability for the host processor to exchange data with HTTP/HTTPS servers.

The WiSeConnect™ SDK v3.x provides an Application Programming Interface (API) to access the HTTP/HTTPS features of the device.

The WiSeConnect™ SDK v3.x also provides an API to run the HyperText Transfer Protocol (HTTP), and HyperText Transfer Protocol Secure (HTTPS) Server on its host processor. This facilitates the exchange of data between the client and server, enabling applications to handle and respond to HTTP/HTTPS requests.

The application runs on the host processor, leveraging the capabilities of the SiWx91x™ chipset family.