Common#
Modules#
rsi_bt_resp_get_bt_stack_version_s
Typedefs#
Structure representing the Bluetooth response to get the BT stack version.
Structure representing the Bluetooth Packet Error Rate (PER) statistics.
Functions#
Set the device BD address.
Set the given name to local device.
Update gain table offset/max power.
Get the local device name.
Get the RSSI of the remote device.
Get the local device address.
Get the BT stack version.
Initialize the BT device.
Deinitialize the BT device.
Select either internal / external antenna on the chip.
Select the power save profile mode for BT / BLE.
Request the local device for BT PER operation.
Typedef Documentation#
rsi_bt_resp_get_bt_stack_version_t#
typedef struct rsi_bt_resp_get_bt_stack_version_s rsi_bt_resp_get_bt_stack_version_t
Structure representing the Bluetooth response to get the BT stack version.
This structure is used to define the parameters for the response that includes the Bluetooth stack version.
rsi_bt_per_stats_t#
typedef struct rsi_bt_per_stats_s rsi_bt_per_stats_t
Structure representing the Bluetooth Packet Error Rate (PER) statistics.
This structure is used to define the parameters for collecting Bluetooth PER statistics, including counts of CRC fails, successful transmissions, and other relevant metrics.
Function Documentation#
rsi_bt_set_bd_addr#
int32_t rsi_bt_set_bd_addr (const uint8_t * dev_addr)
Set the device BD address.
Type | Direction | Argument Name | Description |
---|---|---|---|
const uint8_t * | [in] | dev_addr | - public address of the device to be set |
This is a blocking API.
Pre-conditions:
needs to be called immediately after device initialization.
Returns
The following values are returned:
0 - Success
Non-Zero Value - Failure
3 - Command is given in wrong state (i.e., not immediate after opermode)
Note
This is a blocking API. Refer to the Status Codes section for the above error codes at additional-status-codes .
rsi_bt_set_local_name#
int32_t rsi_bt_set_local_name (const uint8_t * local_name)
Set the given name to local device.
Type | Direction | Argument Name | Description |
---|---|---|---|
const uint8_t * | [in] | local_name | - Name to be set to the local device. |
This is a blocking API.
Pre-conditions:
Device should be initialized before calling this API.
Note
For BLE alone Opermode : When the name of the local device is set to a value with length more than 16 bytes then error is returned with an error code 0x4E66.
Returns
The following values are returned:
0 - Success
Non-Zero Value - Failure
Note
Refer to the Status Codes section for the above error codes at additional-status-codes.
rsi_bt_cmd_update_gain_table_offset_or_max_pwr#
int32_t rsi_bt_cmd_update_gain_table_offset_or_max_pwr (uint8_t node_id, uint8_t payload_len, uint8_t * payload, uint8_t req_type)
Update gain table offset/max power.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | [in] | node_id | - Node ID (0 - BLE, 1 - BT). |
uint8_t | [in] | payload_len | - Length of the payload. |
uint8_t * | [in] | payload | - Payload containing table data of gain table offset/max power |
uint8_t | [in] | req_type | - Update gain table request type
|
This is blocking API.
Pre-conditions:
Device should be initialized before calling this API.
Returns
The following values are returned:
0 - Success
0x4F01 - Invalid gain table payload length
0x4F02 - Invalid region.
0x4F03 - Invalid gain table offset request type
0x4F04 - Invalid node id.
Note
Refer to the Status Codes section for the above error codes at additional-status-codes.
rsi_bt_get_local_name#
int32_t rsi_bt_get_local_name (rsi_bt_resp_get_local_name_t * bt_resp_get_local_name)
Get the local device name.
Type | Direction | Argument Name | Description |
---|---|---|---|
rsi_bt_resp_get_local_name_t * | [out] | bt_resp_get_local_name | - This parameter is the response buffer to hold the response of this API. Please refer rsi_bt_resp_get_local_name_s structure for more info. |
This is a blocking API.
Pre-conditions:
Device should be initialized before calling this API.
Returns
The following values are returned:
0 - Success
Non-Zero Value - Failure
Note
Refer to the Status Codes section for the above error codes at additional-status-codes.
rsi_bt_get_rssi#
int32_t rsi_bt_get_rssi (uint8_t * dev_addr, int8_t * resp)
Get the RSSI of the remote device.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t * | [in] | dev_addr | - Remote device address. |
int8_t * | [out] | resp | - Parameter to hold the response of this API, RSSI is filled in this resp parameter. |
This is a blocking API.
Pre-conditions:
rsi_bt_connect() API need to be called before this API.
Returns
The following values are returned:
0 - Success
Non-Zero Value - Failure
Note
Refer to the Status Codes section for the above error codes at additional-status-codes.
rsi_bt_get_local_device_address#
int32_t rsi_bt_get_local_device_address (uint8_t * resp)
Get the local device address.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t * | [out] | resp | - Parameter to hold the response of this API, local bd_addr is filled in this resp parameter. |
This is a blocking API.
Pre-conditions:
Device should be initialized before calling this API.
Returns
The following values are returned:
0 - Success
Non-Zero Value - Failure
Note
Refer to the Status Codes section for the above error codes at additional-status-codes.
rsi_bt_get_bt_stack_version#
int32_t rsi_bt_get_bt_stack_version (rsi_bt_resp_get_bt_stack_version_t * bt_resp_get_bt_stack_version)
Get the BT stack version.
Type | Direction | Argument Name | Description |
---|---|---|---|
rsi_bt_resp_get_bt_stack_version_t * | [out] | bt_resp_get_bt_stack_version | - Response buffer to hold the response of this API. Please refer rsi_bt_resp_get_bt_stack_version_s structure for more info |
This is a blocking API. Returns
The following values are returned:
0 - Success
Non-Zero Value - Failure
Note
Refer to the Status Codes section for the above error codes at additional-status-codes.
rsi_bt_init#
int32_t rsi_bt_init (void )
Initialize the BT device.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
This is a blocking API.
Pre-conditions:
Device should be initialized before calling this API.
If the device is in powersave, get back the device to ACTIVE MODE by using rsi_bt_power_save_profile()
Returns
The following values are returned:
0 - Success
Non-Zero Value - Failure
Note
Refer to the Status Codes section for the above error codes at additional-status-codes.
rsi_bt_deinit#
int32_t rsi_bt_deinit (void )
Deinitialize the BT device.
Type | Direction | Argument Name | Description |
---|---|---|---|
void | N/A |
This is a blocking API.
Pre-conditions:
Device should be initialized before this API.
Returns
The following values are returned:
0 - Success
Non-Zero Value - Failure
Note
Refer to the Status Codes section for the above error codes at additional-status-codes.
rsi_bt_set_antenna#
int32_t rsi_bt_set_antenna (uint8_t antenna_value)
Select either internal / external antenna on the chip.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | [in] | antenna_value | - Parameter is used to select either internal or external antenna. Possible values:
|
This is a blocking API.
Pre-conditions:
Device should be initialized before calling this API.
Returns
The following values are returned:
0 - Success
Non-Zero Value - Failure
Note
Refer to the Status Codes section for the above error codes at additional-status-codes.
rsi_bt_power_save_profile#
int32_t rsi_bt_power_save_profile (uint8_t psp_mode, uint8_t psp_type)
Select the power save profile mode for BT / BLE.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | [in] | psp_mode | Following psp_mode is defined.
|
uint8_t | [in] | psp_type | Following psp_type is defined.
|
This is a blocking API.
Pre-conditions:
Device should be initialized before calling this API
Returns
The following values are returned:
0 - Success
Non-Zero Value - Failure
Note
If the user wants to enable power save in CoEx mode (WLAN + BT LE) mode - It is mandatory to enable WLAN power save along with BT LE power save.
The device will enter into power save if and only if both protocol (WLAN, BLE) power save modes are enabled.
Refer to the Status Codes section for the above error codes at additional-status-codes.
psp_type is only valid in psp_mode 2.
BT/BLE does not support in RSI_SLEEP_MODE_1.
BT/BLE supports only RSI_MAX_PSP mode. Remaining modes are not supported.
rsi_bt_per_stats#
int32_t rsi_bt_per_stats (uint8_t cmd_type, struct rsi_bt_per_stats_s * rsi_bt_per_stats)
Request the local device for BT PER operation.
Type | Direction | Argument Name | Description |
---|---|---|---|
uint8_t | [in] | cmd_type | - Parameter to define the command id type for PER operation.
|
struct rsi_bt_per_stats_s * | [in] | rsi_bt_per_stats | - reference to the response structure. Please refer to rsi_bt_per_stats_s structure for more info. |
Pre-conditions:
Call rsi_bt_per_tx() or rsi_bt_per_rx() before calling this API.
Returns
The following values are returned:
0 - Success
Non-Zero Value - Failure
Note
Refer Error Codes section for common error codes error-codes.