You are viewing documentation for version:
3.3.3
Structure representing the BLE event for CBFC connection complete.
This structure is used to define the parameters for a BLE event that indicates the completion of a Circular Buffer Flow Control (CBFC) connection with a remote device.
Public Attributes# uint8_t
Address of the remote device.
uint16_t
Protocol/Service Multiplexer (PSM) value.
uint16_t
Maximum Transmission Unit (MTU) size.
uint16_t
Local Channel Identifier (LCID)
Public Attribute Documentation# dev_addr# uint8_t rsi_ble_event_cbfc_conn_complete_s::dev_addr[RSI_DEV_ADDR_LEN] Address of the remote device.
psm# uint16_t rsi_ble_event_cbfc_conn_complete_s::psm Protocol/Service Multiplexer (PSM) value.
mtu# uint16_t rsi_ble_event_cbfc_conn_complete_s::mtu Maximum Transmission Unit (MTU) size.
mps# uint16_t rsi_ble_event_cbfc_conn_complete_s::mps Maximum PDU Size (MPS)
lcid# uint16_t rsi_ble_event_cbfc_conn_complete_s::lcid Local Channel Identifier (LCID)