Wi-Fi performance profile.

Public Attributes#

uint8_t

Set DTIM alignment required. One of the values from DTIM Alignment Types.

uint8_t

Number of DTIM intervals to skip. Default value is 0.

uint16_t

Listen interval in beacon intervals.

uint16_t

Monitor interval in milliseconds. Default interval 50 milliseconds is used if monitor_interval is set to 0. This is only valid when performance profile is set to ASSOCIATED_POWER_SAVE_LOW_LATENCY.

sl_wifi_twt_request_t

Target Wake Time (TWT) request settings.

sl_wifi_twt_selection_t

Target Wake Time (TWT) selection request settings.

Public Attribute Documentation#

profile#

sl_si91x_performance_profile_t sl_wifi_performance_profile_t::profile

Performance profile of type sl_si91x_performance_profile_t.


Definition at line 2103 of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h

dtim_aligned_type#

uint8_t sl_wifi_performance_profile_t::dtim_aligned_type

Set DTIM alignment required. One of the values from DTIM Alignment Types.


Definition at line 2104 of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h

num_of_dtim_skip#

uint8_t sl_wifi_performance_profile_t::num_of_dtim_skip

Number of DTIM intervals to skip. Default value is 0.


Definition at line 2105 of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h

listen_interval#

uint16_t sl_wifi_performance_profile_t::listen_interval

Listen interval in beacon intervals.


Definition at line 2106 of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h

monitor_interval#

uint16_t sl_wifi_performance_profile_t::monitor_interval

Monitor interval in milliseconds. Default interval 50 milliseconds is used if monitor_interval is set to 0. This is only valid when performance profile is set to ASSOCIATED_POWER_SAVE_LOW_LATENCY.


Definition at line 2108 of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h

twt_request#

sl_wifi_twt_request_t sl_wifi_performance_profile_t::twt_request

Target Wake Time (TWT) request settings.


Definition at line 2109 of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h

twt_selection#

sl_wifi_twt_selection_t sl_wifi_performance_profile_t::twt_selection

Target Wake Time (TWT) selection request settings.


Definition at line 2110 of file components/device/silabs/si91x/wireless/inc/sl_wifi_device.h