Calendar#
Introduction#
The Calendar application manages dates, events, alarms, and reminders within hardware constraints. This section provides a brief overview of building such an application.
Configuration#
The Calendar provides three types of triggers: Second, Millisecond, and Alarm.
Second Trigger: Provides a callback every second. To configure the Second Trigger, use sl_si91x_calendar_register_sec_trigger_callback().
Millisecond Trigger: Provides a callback every millisecond. To configure the Millisecond Trigger, use sl_si91x_calendar_register_msec_trigger_callback().
Alarm Trigger: Provides a callback at the alarm time configured by the user. To configure the alarm time, use sl_si91x_calendar_set_alarm(), and to configure the alarm trigger, use sl_si91x_calendar_register_alarm_trigger_callback().
To set up a calendar in the si91x, use the sl_calendar_clock_t structure. It is mandatory to call sl_si91x_calendar_calibration_init function before calling RO clock calibration or RC clock calibration function. After defining this structure, the following function will re-initiate and configure the calendar:
For more detailed information on configuring available parameters, see the respective peripheral example README document.
Usage#
Common Calendar functions can be used after the Calendar structures are specified, passing an instance of sl_calendar_datetime_config_t. These functions will initiate and configure the Calendar, following the implementation flow below:
sl_si91x_calendar_set_configuration - Configures the calendar settings.
sl_si91x_calendar_init - Initializes the calendar module.
sl_si91x_calendar_build_datetime_struct - Builds the datetime structure.
sl_si91x_calendar_set_date_time - Sets the date and time.
sl_si91x_calendar_deinit - Deinitializes the calendar module.
Modules#
Typedefs#
Renaming clock type enum.
Renaming datetime structure.
Renaming month structure.
Renaming days of week structure.
Typedef for the function pointer of the callback function.
Functions#
Enumeration to represent time conversion format.
Enumeration to represent the different RC clock calibration configurations.
Enumeration to represent different RO clock calibration configurations.
To configure and initialize Calendar (i.e., the RTC clock).
To configure and initialize Calendar (i.e., the RTC clock).
To fetch the current date and time of an existing Calendar i.e., RTC clock.
To calibrate the RC clock.
To calibrate the RO clock.
To register the callback for a one-millisecond trigger and enable it.
To register the callback for a one-second trigger and enable it.
To register the callback for an alarm trigger and enable it.
To deregister the callback for one millisecond trigger and disable it.
To deregister the callback for the one-second trigger and disable it.
To deregister the callback for the alarm trigger and disable it.
To set the date and time of a new alarm in RTC.
To fetch the date and time of an existing alarm set in RTC.
To build the structure for date-time configuration.
To convert a Unix timestamp to an NTP timestamp.
To convert NTP timestamp to Unix timestamp.
To return the state of the one millisecond trigger of RTC (enabled or disabled).
To check the state of the one-second trigger of RTC.
To check the state of the alarm trigger of RTC.
Convert Unix timestamp to Calendar RTC timestamp.
Convert Calendar RTC timestamp to Unix timestamp.
Starts the Calendar RTC.
To stop the Calendar RTC.
To initialize the calibration for Calendar clocks.
To clear the one millisecond trigger.
To clear the one-second trigger.
To clear the alarm trigger.
To initialize calendar operation.
To de-initialize calendar operation.
To get the calendar version.
Macros#
Alarm IRQ Handler.
RTC IRQ Handler.
Alarm NVIQ enable.
RTC NVIQ enable.
Time Conversion format enum declaration.
Time Conversion format enum declaration.
Time Conversion format enum declaration.
Typedef Documentation#
sl_calendar_datetime_config_t#
typedef RTC_TIME_CONFIG_T sl_calendar_datetime_config_t
Renaming datetime structure.
sl_calendar_days_of_week_t#
typedef RTC_DAY_OF_WEEK_T sl_calendar_days_of_week_t
Renaming days of week structure.
calendar_callback_t#
typedef void(* calendar_callback_t) (void) )(void)
Typedef for the function pointer of the callback function.
Function Documentation#
TIME_CONVERSION_ENUM#
TIME_CONVERSION_ENUM (time_conversion_enum )
Enumeration to represent time conversion format.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| time_conversion_enum | N/A |
RC_CLOCK_CALIBRATION_ENUM#
RC_CLOCK_CALIBRATION_ENUM (rc_clock_calibration_enum )
Enumeration to represent the different RC clock calibration configurations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| rc_clock_calibration_enum | N/A |
RO_CLOCK_CALIBRATION_ENUM#
RO_CLOCK_CALIBRATION_ENUM (ro_clock_calibration_enum )
Enumeration to represent different RO clock calibration configurations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| ro_clock_calibration_enum | N/A |
sl_si91x_calendar_set_configuration#
sl_status_t sl_si91x_calendar_set_configuration (sl_calendar_clock_t clock_type)
To configure and initialize Calendar (i.e., the RTC clock).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_calendar_clock_t | [in] | clock_type | (sl_calendar_clock_t) Enum for RTC Clock Type (RC or XTAL) |
This API is no longer supported due to the restriction on peripheral drivers to configure clock.
Returns
status, error code as follows:
SL_STATUS_OK (0x0000) - return ok to support backward compatibility.
For more information on the status documentation, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_set_date_time#
sl_status_t sl_si91x_calendar_set_date_time (sl_calendar_datetime_config_t * config)
To configure and initialize Calendar (i.e., the RTC clock).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_calendar_datetime_config_t * | [in] | config | Pointer to the Date Configuration Structure (sl_calendar_datetime_config_t). |
Sets the date and time of the Calendar RTC. The input parameters include a date-time structure, with the following members:
date Pointer to the Date Configuration Structure
Century (uint8_t) Century (0-3)
Year (uint8_t) Year (0-99)
Month (enum) Month from the sl_calendar_month_t enum
DayOfWeek (enum) Day of Week from the sl_calendar_days_of_week_t enum
Day (uint8_t) Day (1-31)
Hour (uint8_t) Hour (0-23)
Minute (uint8_t) Minute (0-59)
Second (uint8_t) Second (0-59)
Milliseconds (uint16_t) Milliseconds (0-999)
Pre-conditions:
Returns
Status code indicating the result:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid.
For more information on the status documentation, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_get_date_time#
sl_status_t sl_si91x_calendar_get_date_time (sl_calendar_datetime_config_t * config)
To fetch the current date and time of an existing Calendar i.e., RTC clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_calendar_datetime_config_t * | [in] | config | Pointer to the Date Configuration Structure (sl_calendar_datetime_config_t). |
The input parameter consists of a date-time structure. The structure is updated with the current date-time parameters. The members of the structure are listed below:
date Pointer to the Date Configuration Structure
Century (uint8_t) Century (0-3)
Year (uint8_t) Year (0-99)
Month (enum) Month from the sl_calendar_month_t enum
DayOfWeek (enum) Day of Week from the sl_calendar_days_of_week_t enum
Day (uint8_t) Day (1-31)
Hour (uint8_t) Hour (0-23)
Minute (uint8_t) Minute (0-59)
Second (uint8_t) Second (0-59)
Milliseconds (uint16_t) Milliseconds (0-999)
Pre-conditions:
Returns
status Status code indicating the result:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid.
For more information on the status documentation, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_rcclk_calibration#
sl_status_t sl_si91x_calendar_rcclk_calibration (clock_calibration_config_t * clock_calibration_config)
To calibrate the RC clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| clock_calibration_config_t * | [in] | clock_calibration_config | Pointer to the clock calibration structure (clock_calibration_config_t). |
This API is no longer supported due to the restriction on peripheral drivers to configure clock.
Returns
status, error code as follows:
SL_STATUS_OK (0x0000) - return ok to support backward compatibility.
For more information on the status documentation, please refer to SL STATUS DOCUMENTATION.
sl_si91x_calendar_roclk_calibration#
sl_status_t sl_si91x_calendar_roclk_calibration (clock_calibration_config_t * clock_calibration_config)
To calibrate the RO clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| clock_calibration_config_t * | [in] | clock_calibration_config | Pointer to the clock calibration structure (clock_calibration_config_t). |
This API is no longer supported due to the restriction on peripheral drivers to configure clock.
Returns
status, error code as follows:
SL_STATUS_OK (0x0000) - return ok to support backward compatibility.
For more information on the status documentation, please refer to SL STATUS DOCUMENTATION.
sl_si91x_calendar_register_msec_trigger_callback#
sl_status_t sl_si91x_calendar_register_msec_trigger_callback (calendar_callback_t callback)
To register the callback for a one-millisecond trigger and enable it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| calendar_callback_t | [in] | callback | Callback function pointer (calendar_callback_t) to be called when the millisecond interrupt is triggered. |
At the time of the trigger, the callback function passed as an argument to this function is called. It expects the callback function pointer as an input argument. Before calling this function again, it is mandatory to call sl_si91x_calendar_unregister_msec_trigger_callback, otherwise, it returns the SL_STATUS_BUSY error code.
Returns
Status code indicating the results:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_BUSY (0x0004) - The callback is already registered. Deregister the previous callback before registering a new one.
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer.
For more information on the status documentation, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_register_sec_trigger_callback#
sl_status_t sl_si91x_calendar_register_sec_trigger_callback (calendar_callback_t callback)
To register the callback for a one-second trigger and enable it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| calendar_callback_t | [in] | callback | Callback function pointer (calendar_callback_t) to be called when the second interrupt is triggered. |
At the time of the trigger, the callback function passed as an argument to this function is called. It expects the callback function pointer as an input argument. Before calling this function again, it is mandatory to call sl_si91x_calendar_unregister_sec_trigger_callback, otherwise, it returns the SL_STATUS_BUSY error code.
Returns
Status code indicating the result:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_BUSY (0x0004) - The callback is already registered. Deregister the previous callback before registering a new one.
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer.
For more information on the status documentation, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_register_alarm_trigger_callback#
sl_status_t sl_si91x_calendar_register_alarm_trigger_callback (calendar_callback_t callback)
To register the callback for an alarm trigger and enable it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| calendar_callback_t | [in] | callback | Callback function pointer (calendar_callback_t) to be called when the alarm interrupt is triggered. |
At the time of the trigger, the callback function passed as an argument to this function is called. It expects the callback function pointer as an input argument. Before calling this function again, it is mandatory to call sl_si91x_calendar_unregister_alarm_trigger_callback. Otherwise, it returns the SL_STATUS_BUSY error code.
Returns
Status code indicating the result:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_BUSY (0x0004) - The callback is already registered. Deregister the previous callback before registering a new one.
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer.
For more information on the status documentation, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_unregister_msec_trigger_callback#
sl_status_t sl_si91x_calendar_unregister_msec_trigger_callback (void )
To deregister the callback for one millisecond trigger and disable it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Note
It is mandatory to call this function before registering the callback again.
Pre-condition:
Returns
Status code indicating the result:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_FAIL (0x0001) - The function failed.
For more information on the status documentation, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_unregister_sec_trigger_callback#
sl_status_t sl_si91x_calendar_unregister_sec_trigger_callback (void )
To deregister the callback for the one-second trigger and disable it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Note
It is mandatory to call this function before registering the callback again.
Pre-condition:
Returns
Status code indicating the result:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_FAIL (0x0001) - Function failed.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_unregister_alarm_trigger_callback#
sl_status_t sl_si91x_calendar_unregister_alarm_trigger_callback (void )
To deregister the callback for the alarm trigger and disable it.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Note
It is mandatory to call this function before registering the callback again.
Pre-condition:
Returns
Status code indicating the results:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_FAIL (0x0001) - Function failed.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_set_alarm#
sl_status_t sl_si91x_calendar_set_alarm (sl_calendar_datetime_config_t * alarm)
To set the date and time of a new alarm in RTC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_calendar_datetime_config_t * | [in] | alarm | Pointer to the Date Configuration Structure (sl_calendar_datetime_config_t). |
It is a one-shot alarm; after triggering the alarm, it elapses. The input parameters consist of a date-time structure. The members of the structure are listed below:
date Pointer to the Date Configuration Structure
Century (uint8_t) Century (0-3)
Year (uint8_t) Year (0-99)
Month (enum) Month from the sl_calendar_month_t enum
DayOfWeek (enum) Day of Week from the sl_calendar_days_of_week_t enum
Day (uint8_t) Day (1-31)
Hour (uint8_t) Hour (0-23)
Minute (uint8_t) Minute (0-59)
Second (uint8_t) Second (0-59)
Milliseconds (uint16_t) Milliseconds (0-999)
Pre-conditions:
Returns
Status code indicating the result:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_get_alarm#
sl_status_t sl_si91x_calendar_get_alarm (sl_calendar_datetime_config_t * alarm)
To fetch the date and time of an existing alarm set in RTC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_calendar_datetime_config_t * | [in] | alarm | Pointer to the Date Configuration Structure (sl_calendar_datetime_config_t). |
The input parameters consist of a dummy date-time structure. The structure is updated with the current date-time parameters. The members of the structure are listed below:
date Pointer to the Date Configuration Structure
Century (uint8_t) Century (0-3)
Year (uint8_t) Year (0-99)
Month (enum) Month from the sl_calendar_month_t enum
DayOfWeek (enum) Day of Week from the sl_calendar_days_of_week_t enum
Day (uint8_t) Day (1-31)
Hour (uint8_t) Hour (0-23)
Minute (uint8_t) Minute (0-59)
Second (uint8_t) Second (0-59)
Milliseconds (uint16_t) Milliseconds (0-999)
Returns
Status code indicating the result:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_build_datetime_struct#
sl_status_t sl_si91x_calendar_build_datetime_struct (sl_calendar_datetime_config_t * date, uint8_t Century, uint8_t Year, sl_calendar_month_t Month, sl_calendar_days_of_week_t DayOfWeek, uint8_t Day, uint8_t Hour, uint8_t Minute, uint8_t Second, uint16_t Milliseconds)
To build the structure for date-time configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_calendar_datetime_config_t * | [in] | date | Pointer to the Date Configuration Structure (sl_calendar_datetime_config_t) |
| uint8_t | [in] | Century | (uint8_t) Century (0-3) |
| uint8_t | [in] | Year | (uint8_t) Year (0-99) |
| sl_calendar_month_t | [in] | Month | (enum) Month from the sl_calendar_month_t enum |
| sl_calendar_days_of_week_t | [in] | DayOfWeek | (enum) Day of Week from the sl_calendar_days_of_week_t enum |
| uint8_t | [in] | Day | (uint8_t) Day (1-31) |
| uint8_t | [in] | Hour | (uint8_t) Hour (0-23) |
| uint8_t | [in] | Minute | (uint8_t) Minute (0-59) |
| uint8_t | [in] | Second | (uint8_t) Second (0-59) |
| uint16_t | [in] | Milliseconds | (uint16_t) Milliseconds (0-999) |
By providing the following parameters as input, it validates and fills the date-time configuration structure with the respective values.
Returns
Status code indicating the result:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid.
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_convert_unix_time_to_ntp_time#
sl_status_t sl_si91x_calendar_convert_unix_time_to_ntp_time (uint32_t time, uint32_t * ntp_time)
To convert a Unix timestamp to an NTP timestamp.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | time | Unix timestamp (uint32_t) |
| uint32_t * | [out] | ntp_time | Pointer to a variable to store the NTP timestamp (uint32_t) |
This function converts a given Unix timestamp to an NTP timestamp. The Unix timestamp is provided as an input parameter, and the resulting NTP timestamp is stored in the variable pointed to by ntp_time.
Returns
Status code indicating the result:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid.
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_convert_ntp_time_to_unix_time#
sl_status_t sl_si91x_calendar_convert_ntp_time_to_unix_time (uint32_t ntp_time, uint32_t * time)
To convert NTP timestamp to Unix timestamp.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | ntp_time | NTP timestamp. |
| uint32_t * | [out] | time | Variable to store the Unix timestamp. |
This function converts a given NTP timestamp to a Unix timestamp.
Returns
sl_status_t Status code indicating the result:
SL_STATUS_OK (0x0000) - Success.
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid.
SL_STATUS_NULL_POINTER (0x0022) - The parameter is a null pointer.
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_is_msec_trigger_enabled#
boolean_t sl_si91x_calendar_is_msec_trigger_enabled (void )
To return the state of the one millisecond trigger of RTC (enabled or disabled).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
If enabled, returns true. If disabled, returns false.
Pre-condition:
Returns
(boolean) true if the trigger is enabled, false otherwise.
sl_si91x_calendar_is_sec_trigger_enabled#
boolean_t sl_si91x_calendar_is_sec_trigger_enabled (void )
To check the state of the one-second trigger of RTC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function returns the state of the one-second trigger of RTC (enabled or disabled). If enabled, it returns true. If disabled, it returns false.
Pre-condition:
Returns
(boolean) true if the trigger is enabled, false otherwise.
sl_si91x_calendar_is_alarm_trigger_enabled#
boolean_t sl_si91x_calendar_is_alarm_trigger_enabled (void )
To check the state of the alarm trigger of RTC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function returns the state of the alarm trigger of RTC (enabled or disabled). If enabled, it returns true. If disabled, it returns false.
Pre-condition:
Returns
(boolean) true if the trigger is enabled, false otherwise.
sl_si91x_calendar_convert_unix_time_to_calendar_datetime#
sl_status_t sl_si91x_calendar_convert_unix_time_to_calendar_datetime (uint32_t unix_time, sl_calendar_datetime_config_t * cal_date_time)
Convert Unix timestamp to Calendar RTC timestamp.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | unix_time | (uint32_t) Unix timestamp |
| sl_calendar_datetime_config_t * | [in] | cal_date_time | (sl_calendar_datetime_config_t *) Pointer to the Date Configuration Structure |
Timezone is not part of Calendar, assumes and converts in GMT format
Returns
status 0 if successful, else error code as follows:
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_convert_calendar_datetime_to_unix_time#
sl_status_t sl_si91x_calendar_convert_calendar_datetime_to_unix_time (sl_calendar_datetime_config_t * cal_date_time, uint32_t * unix_time)
Convert Calendar RTC timestamp to Unix timestamp.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_calendar_datetime_config_t * | [in] | cal_date_time | (sl_calendar_datetime_config_t *) Pointer to the Date Configuration Structure |
| uint32_t * | [in] | unix_time | (uint32_t *) Pointer to the Unix timestamp variable |
Timezone is not part of Calendar, converts in GMT format
Returns
status 0 if successful, else error code as follows:
SL_STATUS_OK (0x0000) - Success
SL_STATUS_INVALID_PARAMETER (0x0021) - Parameters are invalid
SL_STATUS_INVALID_RANGE (0x0028) - Parameters are invalid
For more information on status codes, see SL STATUS DOCUMENTATION.
sl_si91x_calendar_rtc_start#
__STATIC_INLINE void sl_si91x_calendar_rtc_start (void )
Starts the Calendar RTC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Pre-conditions:
sl_si91x_calendar_rtc_stop#
__STATIC_INLINE void sl_si91x_calendar_rtc_stop (void )
To stop the Calendar RTC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function stops the RTC clock.
sl_si91x_calendar_calibration_init#
__STATIC_INLINE void sl_si91x_calendar_calibration_init (void )
To initialize the calibration for Calendar clocks.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function initiates the calibration for Calendar clocks. It is mandatory to call this function before calling RO clock calibration or RC clock calibration function.
sl_si91x_calendar_clear_msec_trigger#
__STATIC_INLINE void sl_si91x_calendar_clear_msec_trigger (void )
To clear the one millisecond trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function clears the one millisecond trigger. It is generally called in the IRQ handler.
Pre-conditions:
The one millisecond trigger must be set and the IRQ handler must be configured.
sl_si91x_calendar_clear_sec_trigger#
__STATIC_INLINE void sl_si91x_calendar_clear_sec_trigger (void )
To clear the one-second trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function clears the one-second trigger. It is generally called in the IRQ handler.
Pre-conditions:
The one-second trigger must be set and the IRQ handler must be configured.
sl_si91x_calendar_clear_alarm_trigger#
__STATIC_INLINE void sl_si91x_calendar_clear_alarm_trigger (void )
To clear the alarm trigger.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function clears the alarm trigger. It is generally called in the IRQ handler.
Pre-conditions:
The alarm must be set and the IRQ handler must be configured.
sl_si91x_calendar_init#
__STATIC_INLINE void sl_si91x_calendar_init (void )
To initialize calendar operation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function powers up the RTC domain and starts the calendar clock.
sl_si91x_calendar_deinit#
__STATIC_INLINE void sl_si91x_calendar_deinit (void )
To de-initialize calendar operation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function powers down the RTC domain and stops the calendar clock.
Pre-conditions:
sl_si91x_calendar_get_version#
sl_calendar_version_t sl_si91x_calendar_get_version (void )
To get the calendar version.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
This function returns the API version of the calendar.
Returns
sl_calendar_version_t type version
Macro Definition Documentation#
TIME_CONVERSION_ENUM#
#define TIME_CONVERSION_ENUMValue:
Time Conversion format enum declaration.
RC_CLOCK_CALIBRATION_ENUM#
#define RC_CLOCK_CALIBRATION_ENUMValue:
Time Conversion format enum declaration.
RO_CLOCK_CALIBRATION_ENUM#
#define RO_CLOCK_CALIBRATION_ENUMValue:
Time Conversion format enum declaration.