Socket Configuration#

The section provides a reference to common socket configuration API function.

Modules#

sl_si91x_socket_config_t

sl_si91x_socket_type_length_value_t

Functions#

sl_status_t
sl_si91x_config_socket(sl_si91x_socket_config_t socket_config)

Configures SiWx91x specific socket settings.

Function Documentation#

sl_si91x_config_socket#

sl_status_t sl_si91x_config_socket (sl_si91x_socket_config_t socket_config)

Configures SiWx91x specific socket settings.

Parameters
[in]socket_config

Socket configuration of type sl_si91x_socket_config_t.

This function sets up the socket configuration specific to the SiWx91x. It must be called before invoking sl_si91x_socket_async. The configuration includes setting parameters such as socket type, protocol, and other options specific to the SiWx91x series.

  • Pre-conditions:

    • Ensure that the necessary initialization for the SiWx91x module has been completed.

    • This API is called before calling sl_si91x_socket_async.

Returns


Definition at line 142 of file components/device/silabs/si91x/wireless/socket/inc/sl_si91x_socket_utility.h