HTTP read data parameters.
This structure holds the parameters for reading data from an HTTP request, including the request details, buffer for storing the data, and the length of the data received.
Public Attributes#
Pointer to the request structure received in the request handler. Must not be NULL.
uint8_t *
Pointer to the user-defined memory buffer for storing received data. Must not be NULL.
uint32_t
Length of the user-defined memory buffer.
uint32_t
Amount of data received in the read operation.
Public Attribute Documentation#
request#
sl_http_server_request_t* sl_http_recv_req_data_t::request
Pointer to the request structure received in the request handler. Must not be NULL.
buffer#
uint8_t* sl_http_recv_req_data_t::buffer
Pointer to the user-defined memory buffer for storing received data. Must not be NULL.
buffer_length#
uint32_t sl_http_recv_req_data_t::buffer_length
Length of the user-defined memory buffer.
received_data_length#
uint32_t sl_http_recv_req_data_t::received_data_length
Amount of data received in the read operation.