Structure representing the BLE event for CBFC connection request.
This structure is used to define the parameters for a BLE event that involves a Circular Buffer Flow Control (CBFC) connection request from a remote device.
Public Attributes#
uint8_t
Address of the remote device.
uint16_t
Protocol/Service Multiplexer (PSM) value.
uint16_t
Local Channel Identifier (LCID)
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_event_cbfc_conn_req_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the remote device.
Definition at line
1182
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
psm#
uint16_t rsi_ble_event_cbfc_conn_req_s::psm
Protocol/Service Multiplexer (PSM) value.
Definition at line
1184
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h
lcid#
uint16_t rsi_ble_event_cbfc_conn_req_s::lcid
Local Channel Identifier (LCID)
Definition at line
1186
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h