Structure represents the BLE set antenna request.

This structure is used to define the parameters for setting the BLE antenna, that includes the antenna value which, can be internal or external.

Public Attributes#

uint8_t

Antenna value - internal/external.

Public Attribute Documentation#

value#

uint8_t rsi_ble_set_antenna_s::value

Antenna value - internal/external.