Structure representing the MQTT Client Last Will message.
This structure holds the information for the Last Will message that will be sent by the MQTT broker if the client unexpectedly disconnects. The Last Will message is a retained message that can be used to notify other clients about the disconnection.
Public Attributes#
Flag indicating whether to retain the Last Will message.
Quality of Service level for the Last Will message.
Pointer to the topic name for the Last Will message.
Length of the topic name. Should not exceed 200 bytes including NULL termination character.
Pointer to the Last Will message content.
Length of the Last Will message content. Should not exceed 60 bytes including NULL termination character.
Public Attribute Documentation#
is_retained#
bool sl_mqtt_client_last_will_message_t::is_retained
Flag indicating whether to retain the Last Will message.
will_qos_level#
sl_mqtt_qos_t sl_mqtt_client_last_will_message_t::will_qos_level
Quality of Service level for the Last Will message.
will_topic#
uint8_t* sl_mqtt_client_last_will_message_t::will_topic
Pointer to the topic name for the Last Will message.
will_topic_length#
uint16_t sl_mqtt_client_last_will_message_t::will_topic_length
Length of the topic name. Should not exceed 200 bytes including NULL termination character.
will_message#
uint8_t* sl_mqtt_client_last_will_message_t::will_message
Pointer to the Last Will message content.
will_message_length#
uint32_t sl_mqtt_client_last_will_message_t::will_message_length
Length of the Last Will message content. Should not exceed 60 bytes including NULL termination character.