The structure stores generic socket address.
The sockaddr structure represents addresses in a protocol-independent way. It includes the address family, and the address data. The actual format of the address data is determined by the address family specified in sa_family
.
Public Attributes#
uint8_t
Total length of the structure.
Address family (for example, AF_INET).
char
Socket address data. The actual format is determined by the address family.
Public Attribute Documentation#
sa_len#
uint8_t sockaddr::sa_len
Total length of the structure.
Definition at line
225
of file components/service/bsd_socket/inc/socket.h
sa_family#
sa_family_t sockaddr::sa_family
Address family (for example, AF_INET).
Definition at line
226
of file components/service/bsd_socket/inc/socket.h
sa_data#
char sockaddr::sa_data[14]
Socket address data. The actual format is determined by the address family.
Definition at line
227
of file components/service/bsd_socket/inc/socket.h