Constants#
This section provides a reference to the CHACHAPOLY Crypto API constants.
Enumerations#
Enumeration defining ChaChaPoly encryption and decryption types.
Enumeration defining ChaChaPoly modes supported by the SI91X device.
Enumeration defines the ChaChaPoly DMA enable, and disable options.
Enumeration defines ChaChaPoly key sizes supported by the SI91X device.
Enumeration Documentation#
sl_si91x_chachapoly_type_t#
sl_si91x_chachapoly_type_t
Enumeration defining ChaChaPoly encryption and decryption types.
This enumeration defines the types of ChaChaPoly operations supported, including encryption and decryption.
| Enumerator | |
|---|---|
| SL_SI91X_CHACHAPOLY_ENCRYPT | ChaChaPoly Encryption. | 
| SL_SI91X_CHACHAPOLY_DECRYPT | ChaChaPoly Decryption. | 
sl_si91x_chachapoly_mode_t#
sl_si91x_chachapoly_mode_t
Enumeration defining ChaChaPoly modes supported by the SI91X device.
This enumeration defines different ChaChaPoly modes supported by the SI91X device, such as ChaCha20, Poly1305, and ChaCha20Poly1305 modes.
| Enumerator | |
|---|---|
| SL_SI91X_CHACHA20POLY1305_MODE | CHACHA20POLY1305 mode. | 
| SL_SI91X_CHACHA20_MODE | CHACHA20 mode. | 
| SL_SI91X_CHACHAPOLY_POLY1305_KEYR_KEYS_MODE | CHACHA20POLY1305 mode with 'R', 'S' keys. | 
| SL_SI91X_POLY1305_MODE | POLY1305 mode. | 
sl_si91x_chachapoly_dma_use_t#
sl_si91x_chachapoly_dma_use_t
Enumeration defines the ChaChaPoly DMA enable, and disable options.
| Enumerator | |
|---|---|
| SL_SI91X_CHACHAPOLY_DMA_DISABLE | Disable DMA. | 
| SL_SI91X_CHACHAPOLY_DMA_ENABLE | Enable DMA. | 
sl_si91x_chachapoly_key_size_t#
sl_si91x_chachapoly_key_size_t
Enumeration defines ChaChaPoly key sizes supported by the SI91X device.
This enumeration defines the key sizes supported by the ChaChaPoly encryption algorithm on the SI91X device, that includes 256-bits key size.
| Enumerator | |
|---|---|
| SL_SI91X_CHACHAPOLY_KEY_SIZE_256 | Key size of 256-bits. |