Constants#
This section provides a reference to the ECDH Crypto API constants.
Enumerations#
Enumeration defining ECDH modes supported by the SI91X device.
Enumeration defining ECDH sub-modes.
Enumeration defining ECDH vector sizes.
Enumeration defining ECDH curve types.
Macros#
Maximum size of an ECDH vector.
Enumeration Documentation#
sl_si91x_ecdh_mode_t#
sl_si91x_ecdh_mode_t
Enumeration defining ECDH modes supported by the SI91X device.
This enumeration defines the modes of operation for the ECDH algorithm on the SI91X device.
| Enumerator | |
|---|---|
| SL_SI91X_ECDH_192 | ECDH 192 mode. | 
| SL_SI91X_ECDH_224 | ECDH 224 mode. | 
| SL_SI91X_ECDH_256 | ECDH 256 mode. | 
sl_si91x_ecdh_sub_mode_t#
sl_si91x_ecdh_sub_mode_t
Enumeration defining ECDH sub-modes.
This enumeration defines the types of ECDH operations supported, such as ECDH Multiplication, Addition, Subtraction, Double, and Affinity.
| Enumerator | |
|---|---|
| SL_SI91X_ECDH_MUL | ECDH multiplication mode. | 
| SL_SI91X_ECDH_ADD | ECDH addition mode. | 
| SL_SI91X_ECDH_SUB | ECDH subtraction mode. | 
| SL_SI91X_ECDH_DOUBLE | ECDH double mode. | 
| SL_SI91X_ECDH_AFFINITY | ECDH affinity mode. | 
sl_si91x_ecdh_vector_size_t#
sl_si91x_ecdh_vector_size_t
Enumeration defining ECDH vector sizes.
This enumeration defines the different ECDH vector sizes supported, which includes 24, 28, and 32 bytes.
| Enumerator | |
|---|---|
| SL_SI91X_ECDH_VECTOR_SIZE_192 | 192 bits or 24 bytes vector size | 
| SL_SI91X_ECDH_VECTOR_SIZE_224 | 224 bits or 28 bytes vector size | 
| SL_SI91X_ECDH_VECTOR_SIZE_256 | 256 bits or 32 bytes vector size | 
sl_si91x_ecdh_curve_type_t#
sl_si91x_ecdh_curve_type_t
Enumeration defining ECDH curve types.
This enumeration defines the different ECDH curves supported, which includes Prime field curves, binary curves, and Edwards curves.
| Enumerator | |
|---|---|
| SL_SI91X_ECDH_CURVE_P | Prime Field Curves. | 
| SL_SI91X_ECDH_CURVE_K | Binary Field Curves. | 
| SL_SI91X_ECDH_CURVE_B | Edwards Curves. |