Device configuration for Si91x device.

Public Attributes#

uint8_t

Boot option. One of the values from Load Image Types.

sl_mac_address_t *

MAC address of type sl_mac_address_t.

TA buffer allocation command parameters of type sl_si91x_dynamic_pool.

uint8_t

Type of eFuse data need to be read from flash. Refer to sl_si91x_efuse_data_type_t.

Public Attribute Documentation#

boot_option#

uint8_t sl_wifi_device_configuration_t::boot_option

Boot option. One of the values from Load Image Types.


mac_address#

sl_mac_address_t* sl_wifi_device_configuration_t::mac_address

MAC address of type sl_mac_address_t.


band#

sl_si91x_band_mode_t sl_wifi_device_configuration_t::band

Si91x Wi-Fi band of type sl_si91x_band_mode_t.


region_code#

sl_si91x_region_code_t sl_wifi_device_configuration_t::region_code

Si91x region code of type sl_si91x_region_code_t.


boot_config#

sl_si91x_boot_configuration_t sl_wifi_device_configuration_t::boot_config

Si91x boot configuration. Refer to Boot Configuration Feature Bitmaps.


ta_pool#

sl_si91x_dynamic_pool sl_wifi_device_configuration_t::ta_pool

TA buffer allocation command parameters of type sl_si91x_dynamic_pool.


efuse_data_type#

uint8_t sl_wifi_device_configuration_t::efuse_data_type

Type of eFuse data need to be read from flash. Refer to sl_si91x_efuse_data_type_t.