Clock Manager#

Introduction#

The Clock Manager module is responsible for configuring the clock tree in the Si91x system. It enhances the clock management features provided by the GSDK's emlib and device_init services, offering additional functionality for selecting clock sources and setting dividers. This module ensures optimized performance and power efficiency across various system components by managing clock configurations according to application requirements.

Configuration#

The Clock Manager supports a variety of configurations:

  • Clock Source Selection: Allows specific clock sources to be chosen for different branches.

  • Divider Configuration: Modifies clock frequencies by setting divider values.

Configuration is typically performed during device initialization using configuration files and source code.

Usage#

The following steps outline typical usage of the Clock Manager:

  1. Initialize the Clock Manager with desired configuration settings.

  2. Set up oscillator sources and configure clock dividers.

  3. Use runtime APIs to manage dynamic clock changes.

  4. Maintain stable clock configurations to ensure system reliability.

Benefits#

  • Manages complex clock trees efficiently.

  • Enhances system stability and performance.

  • Supports a wide range of Si91x devices.

  • Optimizes power consumption through efficient clock management.

Typedefs#

typedef M4_SOC_CLK_SRC_SEL_T

Typedef to select the clock source for the M4 core in the Si91x SOC.

Functions#

sl_status_t

Initializes the M4_SOC and other required clocks.

sl_status_t
sl_si91x_clock_manager_m4_set_core_clk(M4_SOC_CLK_SRC_SEL_T clk_source, uint32_t pll_freq)

To configure the M4 core clock source and configure the PLL frequency if selected as source.

sl_status_t
sl_si91x_clock_manager_set_pll_freq(PLL_TYPE_T pll_type, uint32_t pll_freq, uint32_t pll_ref_clk)

To set the selected PLL (Phase-Locked Loop) clock to the desired frequency.

To read the currently active M4 core clock source and its frequency.

uint32_t

Gets the selected PLL (Phase-Locked Loop) clock to the desired frequency.

sl_status_t
sl_si91x_clock_manager_control_pll(PLL_TYPE_T pll_type, bool enable)

Controls the selected PLL (Phase-Locked Loop) clock.

void
sl_si91x_delay_ms(uint32_t milli_seconds)

Delays execution for the specified number of milliseconds.

Macros#

#define

PLL reference clock frequency value of XTAL CLK.

Typedef Documentation#

sl_si91x_m4_soc_clk_src_sel_t#

sl_si91x_m4_soc_clk_src_sel_t

Typedef to select the clock source for the M4 core in the Si91x SOC.

This typedef maps to the M4_SOC_CLK_SRC_SEL_T type, which defines the possible clock source selections for the M4 core. The clock source selection impacts the operating frequency and performance characteristics of the M4 processor within the Si91x SOC.

Users can configure the clock source to optimize power consumption or performance based on application requirements.

Note

  • Ensure that the selected clock source is properly configured and stable before switching to avoid system instability.


Function Documentation#

sl_si91x_clock_manager_init#

sl_status_t sl_si91x_clock_manager_init (void )

Initializes the M4_SOC and other required clocks.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • sl_status_t Status code indicating the result:

    • SL_STATUS_OK - Success.

    • Corresponding error code on failure.

For more information on status codes, refer to SL STATUS DOCUMENTATION.


sl_si91x_clock_manager_m4_set_core_clk#

sl_status_t sl_si91x_clock_manager_m4_set_core_clk (M4_SOC_CLK_SRC_SEL_T clk_source, uint32_t pll_freq)

To configure the M4 core clock source and configure the PLL frequency if selected as source.

Parameters
TypeDirectionArgument NameDescription
M4_SOC_CLK_SRC_SEL_T[in]clk_source

Enum value representing different core clock sources.

uint32_t[in]pll_freq

Desired M4 core frequency in MHz.

Returns

  • sl_status_t Status code indicating the result:

    • SL_STATUS_OK - Success.

    • Corresponding error code on failure.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_clock_manager_set_pll_freq#

sl_status_t sl_si91x_clock_manager_set_pll_freq (PLL_TYPE_T pll_type, uint32_t pll_freq, uint32_t pll_ref_clk)

To set the selected PLL (Phase-Locked Loop) clock to the desired frequency.

Parameters
TypeDirectionArgument NameDescription
PLL_TYPE_T[in]pll_type

Enum specifying the type of PLL to configure.

uint32_t[in]pll_freq

Desired frequency for the PLL clock (in MHz).

uint32_t[in]pll_ref_clk

Reference clock frequency for the PLL configuration.

Returns

  • sl_status_t Status code indicating the result:

    • SL_STATUS_OK - Success.

    • Corresponding error code on failure.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_clock_manager_m4_get_core_clk_src_freq#

sl_si91x_m4_soc_clk_src_sel_t sl_si91x_clock_manager_m4_get_core_clk_src_freq (uint32_t * m4_core_clk_freq)

To read the currently active M4 core clock source and its frequency.

Parameters
TypeDirectionArgument NameDescription
uint32_t *[out]m4_core_clk_freq

Pointer to a variable where the current core clock frequency will be stored (in MHz).

Returns

  • sl_si91x_m4_soc_clk_src_sel_t The currently active core clock source:

    • 0: M4_ULPREFCLK

    • 2: M4_SOCPLLCLK

    • 3: M4_MODEMPLLCLK1

    • 4: M4_INTFPLLCLK

    • 5: M4_SLEEPCLK


sl_si91x_clock_manager_get_pll_freq#

uint32_t sl_si91x_clock_manager_get_pll_freq (PLL_TYPE_T pll_type)

Gets the selected PLL (Phase-Locked Loop) clock to the desired frequency.

Parameters
TypeDirectionArgument NameDescription
PLL_TYPE_T[in]pll_type

Enum specifying the type of PLL to configure.

Returns

  • uint32_t PLL frequency value in MHz.


sl_si91x_clock_manager_control_pll#

sl_status_t sl_si91x_clock_manager_control_pll (PLL_TYPE_T pll_type, bool enable)

Controls the selected PLL (Phase-Locked Loop) clock.

Parameters
TypeDirectionArgument NameDescription
PLL_TYPE_T[in]pll_type

Enum specifying the type of PLL to control.

bool[in]enable

Boolean value to enable (true) or disable (false) the PLL.

Returns

  • sl_status_t Status code indicating the result:

    • SL_STATUS_OK - Success.

    • Corresponding error code on failure.

For more information on status codes, see SL STATUS DOCUMENTATION.


sl_si91x_delay_ms#

void sl_si91x_delay_ms (uint32_t milli_seconds)

Delays execution for the specified number of milliseconds.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]milli_seconds

Delay time in milliseconds.

Note

  • This function provides a blocking delay.The delay is calibrated based on the SystemCoreClock frequency. If SystemCoreClock < CLOCK_THRESHOLD, the delay is calibrated with a division factor of LOW_FREQ_CLK_DIV_FAC. If SystemCoreClock >= CLOCK_THRESHOLD, the delay is calibrated with a division factor of HIGH_FREQ_CLK_DIV_FAC. This function uses __NOP() instructions for the delay loop.

For more information on status codes, see SL STATUS DOCUMENTATION.


Macro Definition Documentation#

PLL_REF_CLK_VAL_XTAL#

#define PLL_REF_CLK_VAL_XTAL
Value:
(40000000UL)

PLL reference clock frequency value of XTAL CLK.