WiSeConnect 3 - SiWx91x Platform SDK Version 3.5.0 (June 18 2025) - Release Notes#
Wi-Fi 6 + BLE (WiSeConnect 3) SDK Version 3.5.0
Simplicity SDK Version 2025.6.0
The SiWx91x Platform software development kit (SDK) provides platform features on Silicon Labs SiWx91x microcontrollers, including peripherals, drivers, and services.
Click here for earlier releases.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Driver support for BOD, GPDMA, HSPI Secondary, and OPAMP peripherals
Additional driver features for existing peripherals
Sleep stability improvements
API Changes#
APIs for newly introduced peripherals
Low-power GPIO interrupt API changes with deprecation
Bug Fixes#
Stability and functional fixes for DMA, QEI, SSI, and RHT sensors
Configuration fixes for PSRAM, ULP I2S, and PWM
Chip Enablement#
None
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
Note: See Feature Matrix for a list of any appliable APIs, examples, software variants, modes, hardware, and host interfaces applicable for each feature.
New Features#
Added support for LittleFS on common flash devices.
Added support for GCC link-time optimization (LTO).
Implemented driver support for new peripherals:
Brown-Out Detection (BOD)
General Purpose Direct Memory Access (GPDMA)
High-speed Peripheral Interface (HSPI) Secondary
Operational Amplifier (OPAMP)
Added support for an alternative way to reset the SiWx91x device after an application processor firmware update in ISP mode.
Enhancements#
Enhanced driver support for existing peripherals:
Inter-IC Sound (I2S) Pulse Code Modulation (PCM)
Universal Asynchronous Receiver/Transmitter (UART) RS485
Added Pin Tool support for SoC ULP peripherals on SoC high-power (HP) GPIO pins and vice versa.
Added an initial check in the connectivity (network processor) firmware for the anti-rollback feature before initiating the firmware download.
Enhanced peripheral drivers for configuring the ULP peripheral on SoC high-power (HP) GPIO pins and vice versa.
Adding support for overriding the default Calendar callback handler with a custom implementation.
Introduced new APIs in GPIO driver to ensure consistency in the configuration of UULP GPIO pins.
Added I/O Stream support for multiple stream types, including RTT, SWO, Debug, and VUART.
Enhanced the ULP UART peripheral with support for hardware flow control and 9-bit data mode.
Added a new
PM PS2 Componentto the Power Manager, enabling execution of required files from RAM and providing PS2 power state-specific features and dependencies.Implemented the 32 KHz RC calibration framework for both the Calendar and deep sleep timer peripherals.
Improvements made in the stability of the sleep/wake-up sequence, by fixing a lock-up issue on cold boot.
Removed Features#
Removed Feature | Was Deprecated? |
|---|---|
Capacitive Touch Sensor (CTS) | No |
32-bit mode in Config Timer | No |
Support in I2S peripheral for 12-bit and 20-bit resolutions | No |
Deprecated Features#
Mote: The Watchdog Manager service replaces the Watchdog Timer peripheral mentioned below. See Impact Statements.
Deprecated Feature | Planned Removal Date |
|---|---|
Watchdog Timer peripheral | 2026-12 |
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
New API Signature | Deprecated API replaced by this (if any) |
|---|---|
| |
| |
| |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
| None |
Modified APIs#
None
Removed APIs#
None
Deprecated APIs#
Deprecated API Name | Planned Removal Date |
|---|---|
2026-12 | |
2026-12 | |
2026-12 | |
2026-12 | |
2026-12 | |
2026-12 | |
2026-12 | |
2026-12 | |
2026-12 | |
2026-12 | |
2026-12 | |
2026-12 |
Bug Fixes#
Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect 3 SDK.
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1436051 | Issue in DMA de-init API with improper de-allocation of DMA channels. | None |
|
| 1424712 | Corrected the DMA transfer count in the ADC driver to use only the sample length value. | None |
|
| 1414543 | PSRAM device configuration files do not reflect the installed PSRAM device components. | None |
|
| 1406552 | ULP I2S component UC configuration is missing the GPIOs specified in the SiWG917 data sheet v1.0. | None |
|
| 1379979 | Addressed potential manual errors in PWM configuration by enforcing a build error if "All channels" is selected for the base timer without a `channel_0` instance. | None |
|
| 1413169 | Hard fault occurs in QEI de-init API due to a `NULL` pointer access, causing the program to enter the default handler. | None |
|
| 1430079 | QEI index and position values fail to reset in the QEI de-init API. | None |
|
| 1448261 | Eliminated the dependency on the FreeRTOS configuration file from the platform code. | None |
|
| 1445491 | Un-registering a single SSI instance in the SSI un-register callback results in all instances being un-registered, rather than just the specified SSI instance. | None |
|
| 1401741 | RHT sensor "No Hold Master" mode for temperature and humidity measurement does not work, and the API returns an error code. | None |
|
| 1416569 |
Button 1 does not work after sleep due to the GPIO driver not re-initializing. This issue was fixed by adding the sl_si91x_button_deinit API to allow proper de-initialization and re-initialization of the button after sleep.
|
None |
|
| 1435484 | Sleep/wakeup failures occur when SDIO is used with both application processor and network processor set to power save mode with RAM retention. | None |
|
| 1339252 |
Lack of thread safety in malloc leads to infinite loops during multi-threaded execution.
|
None |
|
| 1424184 | Added validation in the ADC init API to ensure that the number of channels selected in the common configuration matches the number of channels/instances added. | None |
|
Chip Enablement#
None
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect 3 SDK.
New Examples#
| Example Name | Description | Supported Software Variants (if applicable) | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
SL Si91x - BOD See README |
Demonstrates the configuration of the threshold value for BOD and monitoring the voltage levels on VMCU. When the voltage drops below the configured threshold, a BOD interrupt is triggered, and the application handles the event accordingly. | Standard and Lite |
SoC |
|
N/A |
|
SL Si91x - UART RS485 See README |
Demonstrates the configuration of UART0/1 to use in RS485 multidrop mode and to send and receive data. | Standard and Lite |
SoC |
|
N/A |
|
SL Si91x - OPAMP See README |
Demonstrates the initialization, configuration, and operation of the OPAMP peripheral by giving input on the non-inverting terminal and inverting terminal of the OPAMP and checking the output. This application example configures the OPAMP instances for various use cases, including integration with DAC for external voltage comparison. | Standard and Lite |
SoC |
|
N/A |
|
SL Si91x - GPDMA See README |
Demonstrates memory-to-memory DMA transfers of various sizes. Users can change the DMA transfer size by updating TRANSFER_LENGTH. This application example performs a generic DMA transfer using either a pre-defined configuration or a user-defined descriptor.
|
Standard and Lite |
SoC |
|
N/A |
|
SL Si91x - HSPI Secondary See README |
Demonstrates the SoC clock configuration and HSPI secondary initialization with GPDMA, ensuring smooth communication with the SPI primary and efficient callback management for HSPI operations. | Standard and Lite |
SoC |
|
N/A |
|
SL Si91x - PCM Loopback See README |
Demonstrates the PCM loopback functionality. | Standard and Lite |
SoC |
|
N/A |
|
SL Si91x - PCM Primary See README |
Demonstrates the PCM primary device data transfer using the I2S interface. | Standard and Lite |
SoC |
|
N/A |
|
SL Si91x - PCM Secondary See README |
Demonstrates the PCM secondary device transfer using the I2S interface. | Standard and Lite |
SoC |
|
N/A |
Modified Examples#
| Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
SL Si91x - RTOS Message Queue See README |
Updated with I2C driver code for data communication. | Standard and Lite |
SoC |
|
N/A |
|
SL Si91x - Config Timer See README |
Initialized a local variable to prevent un-intended output. | Standard and Lite |
SoC |
|
N/A |
Removed Examples#
Removed Example Name | Was Deprecated? |
|---|---|
Si91x - CPC SDIO Secondary FreeRTOS with Security | No |
Deprecated Examples#
None
Known Issues and Limitations#
Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect 3 SDK.
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
| 1455245 | Blackout reset fails to occur on module board SiW917Y-RB4343A Rev. A07. | None | None |
|
| 1437906 | According to the HRM for BOD, the minimum threshold voltage is 1.75 V, but the hardware triggers an interrupt at 1.9 V or below. | None | None |
|
| 1438016 | BOD does not function in ULP power state PS2. | None | None |
|
| 1417168 | While mbedTLS components and SI91X-PSA driver components are visible in the Simplicity Studio GUI, the PSA components themselves are not displayed. This causes project compilation failures when security modules are manually added to the project. | None | None |
|
| 1364360 |
For peripherals that support multiple instances, Simplicity Studio's "Add New Instance" feature suggests default instance names (e.g., inst0, inst1) which might differ from the instance names supported in the reference documentation and application examples. Users should refer to peripheral-specific documentation for the officially supported instance naming conventions.
|
None | None |
|
| N/A | The ULP Timer may experience timer drifts due to the inaccuracy of the clock source (RC oscillator). | None | None |
|
| N/A | FreeRTOS tick-less idle mode is currently not supported in the Sensor Hub example application. | None | None |
|
| N/A | Only a few wakeup sources (ULP GPIO, ULP Timer, ULP ADC, ULP Comparator, ULP UART) are currently supported for the PS1 state in the Power Manager. | None | None |
|
| N/A | Peripheral clock sources are currently fixed and cannot be configured by the user. | None | None |
|
| N/A | GPDMA driver currently supports only memory-to-memory transfers. | None | None |
|