MQTT Client broker information structure.

This structure holds the information required to connect to an MQTT broker, that includes the broker's IP address, port number, connection encryption status, connection timeout, keep-alive interval, and keep-alive retries.

Public Attributes#

sl_ip_address_t

IP address of the broker.

uint16_t

Port number of the broker.

bool

Indicates if the connection is encrypted. This field would be deprecated in future releases. You are recommended to use tls_flags in sl_mqtt_client_configuration_t.

uint16_t

MQTT connection timeout in milliseconds.

uint16_t

Keep-alive interval of the MQTT connection in seconds.

uint16_t

Number of MQTT ping retries.

Public Attribute Documentation#

ip#

sl_ip_address_t sl_mqtt_broker_t::ip

IP address of the broker.


port#

uint16_t sl_mqtt_broker_t::port

Port number of the broker.


is_connection_encrypted#

bool sl_mqtt_broker_t::is_connection_encrypted

Indicates if the connection is encrypted. This field would be deprecated in future releases. You are recommended to use tls_flags in sl_mqtt_client_configuration_t.


connect_timeout#

uint16_t sl_mqtt_broker_t::connect_timeout

MQTT connection timeout in milliseconds.


keep_alive_interval#

uint16_t sl_mqtt_broker_t::keep_alive_interval

Keep-alive interval of the MQTT connection in seconds.


keep_alive_retries#

uint16_t sl_mqtt_broker_t::keep_alive_retries

Number of MQTT ping retries.