Network Wi-Fi client profile.

This structure holds the configuration for a Wi-Fi client profile, including the Wi-Fi client settings and the network IP configuration.

Public Attributes#

sl_wifi_client_configuration_t

Wi-Fi client configuration of type sl_wifi_client_configuration_t

Network IP configuration of type sl_net_ip_configuration_t.

uint8_t

Priority for auto-join (0 = highest, 255 = lowest)

Public Attribute Documentation#

config#

sl_wifi_client_configuration_t sl_net_wifi_client_profile_t::config

Wi-Fi client configuration of type sl_wifi_client_configuration_t


ip#

sl_net_ip_configuration_t sl_net_wifi_client_profile_t::ip

Network IP configuration of type sl_net_ip_configuration_t.


priority#

uint8_t sl_net_wifi_client_profile_t::priority

Priority for auto-join (0 = highest, 255 = lowest)