Structure to hold the parameters of Analog comparator configurations.
Public Attributes#
Comparator number, sl_analog_comparator_number_t for possible values.
Comparator non-inverting input, sl_analog_comparator_inputs_t for possible values.
Comparator inverting input, sl_analog_comparator_inputs_t for possible values.
Comparator hysteresis control value, sl_analog_comparator_hystersis_values_t.
True to enable and false to disable filter for comparator.
Public Attribute Documentation#
comparator_number#
uint8_t sl_analog_comparator_config_t::comparator_number
Comparator number, sl_analog_comparator_number_t for possible values.
non_inverting_input#
uint8_t sl_analog_comparator_config_t::non_inverting_input
Comparator non-inverting input, sl_analog_comparator_inputs_t for possible values.
inverting_input#
uint8_t sl_analog_comparator_config_t::inverting_input
Comparator inverting input, sl_analog_comparator_inputs_t for possible values.
hystersis_value#
uint8_t sl_analog_comparator_config_t::hystersis_value
Comparator hysteresis control value, sl_analog_comparator_hystersis_values_t.
is_filter_enabled#
boolean_t sl_analog_comparator_config_t::is_filter_enabled
True to enable and false to disable filter for comparator.