Socket Address Family#
Macros#
Unspecified address family.
Local to host (UNIX domain) address family. This domain is not supported in the current release.
POSIX compatibility alias for AF_UNIX. This domain is not supported in the current release.
Internet IP Protocol address family.
ARPANET IMP address family. This domain is not supported in the current release.
PUP protocols (for example, BSP) address family. This domain is not supported in the current release.
MIT CHAOS protocols address family. This domain is not supported in the current release.
XEROX NS protocols address family. This domain is not supported in the current release.
ISO protocols address family. This domain is not supported in the current release.
OSI protocol family. This domain is not supported in the current release.
European Computer Manufacturers Association (ECMA) protocols address family. This domain is not supported in the current release.
Datakit protocols address family. This domain is not supported in the current release.
CCITT protocols (for example, X.25) address family. This domain is not supported in the current release.
IBM SNA address family. This domain is not supported in the current release.
DECnet address family. This domain is not supported in the current release.
DEC Direct data link interface address family. This domain is not supported in the current release.
LAT address family. This domain is not supported in the current release.
NSC Hyperchannel address family. This domain is not supported in the current release.
AppleTalk address family. This domain is not supported in the current release.
Internal Routing Protocol address family. This domain is not supported in the current release.
Link layer interface address family. This domain is not supported in the current release.
eXpress Transfer Protocol (no AF). This domain is not supported in the current release.
Connection-oriented IP, aka ST II address family. This domain is not supported in the current release.
Computer Network Technology address family. This domain is not supported in the current release.
Identifier for RTIP packets. This domain is not supported in the current release.
Novell Internet Protocol address family. This domain is not supported in the current release.
IPv6 address family.
Identifier for PIP packets. This domain is not supported in the current release.
Integrated Services Digital Network address family. This domain is not supported in the current release.
CCITT E.164 recommendation address family. This domain is not supported in the current release.
Native ATM access address family. This domain is not supported in the current release.
Encapsulation address family. This domain is not supported in the current release.
Simple Internet Protocol address family. This domain is not supported in the current release.
Key management protocol address family (originally developed for usage with IPsec).
Used by BPF to not rewrite headers in interface output routine. This domain is not supported in the current release.
Bluetooth address family. This domain is not supported in the current release.
MPLS address family. This domain is not supported in the current release.
Identifier for pflow packets. This domain is not supported in the current release.
Identifier for PIPEX packets. This domain is not supported in the current release.
Maximum address family value. This domain is not supported in the current release.